|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::application::monitor::AbstractDeviceMonitor.
Public Member Functions | |
| DeviceMonitor (DSPortAdapter adapter) | |
| Create a simple monitor that does not search branches. | |
| void | setAdapter (DSPortAdapter adapter) |
| Sets this monitor to search a new DSPortAdapter. | |
| OWPath | getDevicePath (Long address) |
| Returns the OWPath of the device with the given address. | |
| void | setDoAlarmSearch (boolean findAlarmingParts) |
| Sets this monitor to search for alarming parts. | |
| boolean | getDoAlarmSearch () |
| See if Gets this monitor to search for alarming parts. | |
| void | search (Vector arrivals, Vector departures) throws OneWireException, OneWireIOException |
| Performs a search of the 1-Wire network without searching branches. | |
Class DeviceMonitor represents the monitor that searches the 1-Wire net for new arrivals. This monitor performs a simple search, meaning that no branches are explicitly traversed. If a branch is activated/deactivated between search cycles, this monitor will see the arrival/departure of new devices without reference to the branch which they lie on.
| DeviceMonitor | ( | DSPortAdapter | adapter | ) |
Create a simple monitor that does not search branches.
| the | DSPortAdapter this monitor should search |
| OWPath getDevicePath | ( | Long | address | ) | [virtual] |
Returns the OWPath of the device with the given address.
| address | a Long object representing the address of the device |
Implements AbstractDeviceMonitor.
| boolean getDoAlarmSearch | ( | ) |
See if Gets this monitor to search for alarming parts.
| the | DSPortAdapter this monitor should search |
| void search | ( | Vector | arrivals, |
| Vector | departures | ||
| ) | throws OneWireException, OneWireIOException [virtual] |
Performs a search of the 1-Wire network without searching branches.
| arrivals | A vector of Long objects, represent new arrival addresses. |
| departures | A vector of Long objects, represent departed addresses. |
Implements AbstractDeviceMonitor.
| void setAdapter | ( | DSPortAdapter | adapter | ) | [virtual] |
Sets this monitor to search a new DSPortAdapter.
| the | DSPortAdapter this monitor should search |
Implements AbstractDeviceMonitor.
| void setDoAlarmSearch | ( | boolean | findAlarmingParts | ) |
Sets this monitor to search for alarming parts.
| the | DSPortAdapter this monitor should search |
1.7.3