This is the complete list of members for
DeviceMonitor, including all inherited members.
| adapter | AbstractDeviceMonitor | [protected] |
| addDeviceMonitorEventListener(DeviceMonitorEventListener dmel) | AbstractDeviceMonitor | |
| cleanUpStaleContainerReferences() | AbstractDeviceMonitor | |
| cleanUpStalePathReferences() | AbstractDeviceMonitor | |
| deviceAddressHash | AbstractDeviceMonitor | [protected] |
| deviceContainerHash | AbstractDeviceMonitor | [protected, static] |
| DeviceMonitor(DSPortAdapter adapter) | DeviceMonitor | |
| fireArrivalEvent(DSPortAdapter adapter, Vector address) | AbstractDeviceMonitor | [protected] |
| fireDepartureEvent(DSPortAdapter adapter, Vector address) | AbstractDeviceMonitor | [protected] |
| getAdapter() | AbstractDeviceMonitor | |
| getAllAddresses() | AbstractDeviceMonitor | |
| getDeviceContainer(DSPortAdapter adapter, byte[] address) | AbstractDeviceMonitor | [static] |
| getDeviceContainer(DSPortAdapter adapter, String address) | AbstractDeviceMonitor | [static] |
| getDeviceContainer(DSPortAdapter adapter, long address) | AbstractDeviceMonitor | [static] |
| getDeviceContainer(DSPortAdapter adapter, Long longAddress) | AbstractDeviceMonitor | [static] |
| getDevicePath(Long address) | DeviceMonitor | [virtual] |
| com::dalsemi::onewire::application::monitor::AbstractDeviceMonitor.getDevicePath(byte[] address) | AbstractDeviceMonitor | |
| com::dalsemi::onewire::application::monitor::AbstractDeviceMonitor.getDevicePath(String address) | AbstractDeviceMonitor | |
| com::dalsemi::onewire::application::monitor::AbstractDeviceMonitor.getDevicePath(long address) | AbstractDeviceMonitor | |
| getDoAlarmSearch() | DeviceMonitor | |
| getMaxErrorCount() | AbstractDeviceMonitor | |
| getMaxStateCount() | AbstractDeviceMonitor | |
| isMonitorRunning() | AbstractDeviceMonitor | |
| isRunning | AbstractDeviceMonitor | [protected] |
| keepRunning | AbstractDeviceMonitor | [protected] |
| killMonitor() | AbstractDeviceMonitor | |
| listeners | AbstractDeviceMonitor | [protected] |
| max_error_count | AbstractDeviceMonitor | [protected] |
| max_state_count | AbstractDeviceMonitor | [protected] |
| msSleep(long msTime) | AbstractDeviceMonitor | [protected] |
| pauseMonitor(boolean blocking) | AbstractDeviceMonitor | |
| putDeviceContainer(byte[] address, OneWireContainer owc) | AbstractDeviceMonitor | [static] |
| putDeviceContainer(String address, OneWireContainer owc) | AbstractDeviceMonitor | [static] |
| putDeviceContainer(long address, OneWireContainer owc) | AbstractDeviceMonitor | [static] |
| putDeviceContainer(Long longAddress, OneWireContainer owc) | AbstractDeviceMonitor | [static] |
| resetSearch() | AbstractDeviceMonitor | |
| resumeMonitor(boolean blocking) | AbstractDeviceMonitor | |
| run() | AbstractDeviceMonitor | |
| search(Vector arrivals, Vector departures) | DeviceMonitor | [virtual] |
| setAdapter(DSPortAdapter adapter) | DeviceMonitor | [virtual] |
| setDoAlarmSearch(boolean findAlarmingParts) | DeviceMonitor | |
| setMaxErrorCount(int errorCnt) | AbstractDeviceMonitor | |
| setMaxStateCount(int stateCnt) | AbstractDeviceMonitor | |
| startRunning | AbstractDeviceMonitor | [protected] |
| sync_flag | AbstractDeviceMonitor | [protected] |