|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::application::monitor::AbstractDeviceMonitor.
Public Member Functions | |
| ChainMonitor (DSPortAdapter adapter) | |
| Create a simple monitor that does not search branches. | |
| void | setAdapter (DSPortAdapter adapter) |
| Sets this monitor to search a new DSPortAdapter. | |
| OWPath | getDevicePath (Long address) |
| Returns the OWPath of the device with the given address. | |
| boolean | chainOn () throws OneWireException, OneWireIOException |
| chainOn sends the chain mode "ON" command sequence to all chain devices. | |
| boolean | chainConditionalReadRom (byte[] chainDeviceAddress) throws OneWireException, OneWireIOException |
| chainConditionalReadRom sends the chain mode "DONE" command sequence to current chain device. | |
| boolean | chainDone () throws OneWireException, OneWireIOException |
| chainDone sends the chain mode "DONE" command sequence to current chain device. | |
| boolean | chainOff () throws OneWireException, OneWireIOException |
| chainOff sends the chain mode "OFF" command sequence to all chain devices. | |
| void | search (Vector arrivals, Vector departures) throws OneWireException, OneWireIOException |
| Performs a search of the 1-Wire network without searching branches. | |
| Vector | toContainerVector (Vector arrivals) throws OneWireException, OneWireIOException |
| A helper method that takes the arrivals Vector from the search method and returns a Vector of OneWireContainers. | |
Class ChainMonitor represents the monitor that searches the 1-Wire net for Chain Mode devices, otherwise known as "Sequence Detect". Chain Mode devices have two PIO pins (PIOA and PIOB). You can chain multiple devices together by connecting PIOA of one part to PIOB of the next device. The first device in the chain has its PIOB grounded.
This monitor performs a simple search. If a branch is activated/deactivated between search cycles, this monitor will see the arrival/departure of new devices without reference to the branch which they lie on.
| ChainMonitor | ( | DSPortAdapter | adapter | ) |
Create a simple monitor that does not search branches.
| the | DSPortAdapter this monitor should search |
| boolean chainConditionalReadRom | ( | byte[] | chainDeviceAddress | ) | throws OneWireException, OneWireIOException |
chainConditionalReadRom sends the chain mode "DONE" command sequence to current chain device.
| 8-byte | array for chain 1-Wire net address |
| boolean chainDone | ( | ) | throws OneWireException, OneWireIOException |
chainDone sends the chain mode "DONE" command sequence to current chain device.
| none |
| boolean chainOff | ( | ) | throws OneWireException, OneWireIOException |
chainOff sends the chain mode "OFF" command sequence to all chain devices.
| none |
| boolean chainOn | ( | ) | throws OneWireException, OneWireIOException |
chainOn sends the chain mode "ON" command sequence to all chain devices.
| none |
| OWPath getDevicePath | ( | Long | address | ) | [virtual] |
Returns the OWPath of the device with the given address.
| address | a Long object representing the address of the device |
Implements AbstractDeviceMonitor.
| void search | ( | Vector | arrivals, |
| Vector | departures | ||
| ) | throws OneWireException, OneWireIOException [virtual] |
Performs a search of the 1-Wire network without searching branches.
| arrivals | A vector of Long objects, represent new arrival addresses. |
| departures | A vector of Long objects, represent departed addresses. |
Implements AbstractDeviceMonitor.
| void setAdapter | ( | DSPortAdapter | adapter | ) | [virtual] |
Sets this monitor to search a new DSPortAdapter.
| the | DSPortAdapter this monitor should search |
Implements AbstractDeviceMonitor.
| Vector toContainerVector | ( | Vector | arrivals | ) | throws OneWireException, OneWireIOException |
A helper method that takes the arrivals Vector from the search method and returns a Vector of OneWireContainers.
| arrivals | A vector of Long objects, represent new arrival addresses. |
1.7.3