|
1-Wire API for .NET Version 4.00
|
Inherited by ChainMonitor, DeviceMonitor, and NetworkDeviceMonitor.
Public Member Functions | |
| void | cleanUpStaleContainerReferences () |
| The device monitor will internally cache OneWireContainer objects for each 1-Wire device. | |
| void | cleanUpStalePathReferences () |
| The device monitor will internally cache OWPath objects for each 1-Wire device. | |
| void | resetSearch () |
| Resets this device monitor. | |
| int | getMaxStateCount () |
| The number of searches that a button should be "missing" before it is removed. | |
| void | setMaxStateCount (int stateCnt) |
| The number of searches that a button should be "missing" before it is removed. | |
| int | getMaxErrorCount () |
| Number of searches that an error occurs before listener's are notified. | |
| void | setMaxErrorCount (int errorCnt) |
| Number of searches that an error occurs before listener's are notified. | |
| DSPortAdapter | getAdapter () |
| Returns the DSPortAdapter this device is searching. | |
| abstract void | setAdapter (DSPortAdapter adapter) |
| Sets this monitor to search a new DSPortAdapter. | |
| abstract void | search (Vector arrivals, Vector departures) throws OneWireException, OneWireIOException |
| Performs a search of the 1-Wire network. | |
| boolean | pauseMonitor (boolean blocking) |
| Pause this monitor. | |
| boolean | resumeMonitor (boolean blocking) |
| Resume this monitor. | |
| boolean | isMonitorRunning () |
| Check if this monitor is running. | |
| void | killMonitor () |
| Kill this monitor. | |
| void | run () |
| Monitor run method that performs a periodic search of the entire 1-Wire network. | |
| void | addDeviceMonitorEventListener (DeviceMonitorEventListener dmel) |
| Add a listener, to be notified of arrivals, departures, and exceptions. | |
| OWPath | getDevicePath (byte[] address) |
| Returns the OWPath of the device with the given address. | |
| OWPath | getDevicePath (String address) |
| Returns the OWPath of the device with the given address. | |
| OWPath | getDevicePath (long address) |
| Returns the OWPath of the device with the given address. | |
| abstract OWPath | getDevicePath (Long address) |
| Returns the OWPath of the device with the given address. | |
| Enumeration | getAllAddresses () |
| Returns all addresses known by this monitor as an Enumeration of Long objects. | |
Static Public Member Functions | |
| static OneWireContainer | getDeviceContainer (DSPortAdapter adapter, byte[] address) |
| Returns the OneWireContainer object of the device with the given address. | |
| static OneWireContainer | getDeviceContainer (DSPortAdapter adapter, String address) |
| Returns the OneWireContainer object of the device with the given address. | |
| static OneWireContainer | getDeviceContainer (DSPortAdapter adapter, long address) |
| Returns the OneWireContainer object of the device with the given address. | |
| static OneWireContainer | getDeviceContainer (DSPortAdapter adapter, Long longAddress) |
| Returns the OneWireContainer object of the device with the given address. | |
| static void | putDeviceContainer (byte[] address, OneWireContainer owc) |
| Sets the OneWireContainer object of the device with the given address. | |
| static void | putDeviceContainer (String address, OneWireContainer owc) |
| Sets the OneWireContainer object of the device with the given address. | |
| static void | putDeviceContainer (long address, OneWireContainer owc) |
| Sets the OneWireContainer object of the device with the given address. | |
| static void | putDeviceContainer (Long longAddress, OneWireContainer owc) |
| Sets the OneWireContainer object of the device with the given address. | |
Protected Member Functions | |
| void | msSleep (long msTime) |
| Sleep for the specified number of milliseconds. | |
| void | fireArrivalEvent (DSPortAdapter adapter, Vector address) |
| Notify the listeners of the arrival event. | |
| void | fireDepartureEvent (DSPortAdapter adapter, Vector address) |
| Notify the listeners of the departure event. | |
Protected Attributes | |
| final Object | sync_flag = new Object() |
| object used for synchronization | |
| final Hashtable | deviceAddressHash = new Hashtable() |
| Addresses of all current devices, mapped to their state count. | |
| final Vector | listeners = new Vector() |
| Listeners who receive notification of events generated by this device Monitor. | |
| int | max_state_count = 3 |
| Number of searches that a button should be "missing" before it is removed. | |
| int | max_error_count = 6 |
| Number of searches that an error occurs before a dialog is displayed. | |
| volatile boolean | keepRunning = true |
| Flag for overall thread running state. | |
| volatile boolean | startRunning = true |
| Flag to indicate thread has begin to run. | |
| volatile boolean | isRunning = false |
| Flag to indicate thread is running now. | |
| DSPortAdapter | adapter = null |
| the adapter to search for devices | |
Static Protected Attributes | |
| static final Hashtable | deviceContainerHash = new Hashtable() |
| hashtable for holding device containers, static to keep only a single instance of each OneWireContainer. | |
Abstract super-class for 1-Wire Monitors, a optionally-threadable object for searching 1-Wire networks. If this object is not run in it's own thread, it is possible to perform single-step searches by calling the NewLine method directly.
In a touch-contact environment, it is not suitable to say that a device has "departed" because it was missing for one cycle of searching. In the time it takes to get an iButton into a blue-dot receptor, the monitor could have generated a handful of arrival and departure events. To circumvent this problem, the device monitor keeps a "missing state count" for each device on the network. Each search cycle that passes where the device is missing causes it's "missing state count" to be incremented. Once the device's "missing state count" is equal to the "max state count", a departure event is generated for the device.
Similarly, the reporting of exceptions could be spurious in a touch-contact environment. Instead of reporting the exception on each failed search attempt, the monitor will default to retrying the search a handful of times before finally reporting the exception.
To receive events, an object must implement the DeviceMonitorEventListener interface.
| void addDeviceMonitorEventListener | ( | DeviceMonitorEventListener | dmel | ) |
Add a listener, to be notified of arrivals, departures, and exceptions.
| dmel | Listener of monitor events. |
| void cleanUpStaleContainerReferences | ( | ) |
The device monitor will internally cache OneWireContainer objects for each 1-Wire device.
Use this method to clean up all stale container objects. A stale container object is a OneWireContainer object which references a 1-Wire device address which has not been seen by a recent search. This will be essential in a touch-contact environment which could run for some time and needs to conserve memory.
| void cleanUpStalePathReferences | ( | ) |
The device monitor will internally cache OWPath objects for each 1-Wire device.
Use this method to clean up all stale OWPath objects. A stale path object is a OWPath which references a branching path to a 1-Wire device address which has not been seen by a recent search. This will be essential in a touch-contact environment which could run for some time and needs to conserve memory.
Reimplemented in NetworkDeviceMonitor.
| void fireArrivalEvent | ( | DSPortAdapter | adapter, |
| Vector | address | ||
| ) | [protected] |
Notify the listeners of the arrival event.
| address | Vector of Long objects representing the address of new arrivals. |
| void fireDepartureEvent | ( | DSPortAdapter | adapter, |
| Vector | address | ||
| ) | [protected] |
Notify the listeners of the departure event.
| address | Vector of Long objects representing the address of departed devices. |
| DSPortAdapter getAdapter | ( | ) |
Returns the DSPortAdapter this device is searching.
| the | DSPortAdapter this monitor is searching |
| Enumeration getAllAddresses | ( | ) |
Returns all addresses known by this monitor as an Enumeration of Long objects.
| static OneWireContainer getDeviceContainer | ( | DSPortAdapter | adapter, |
| long | address | ||
| ) | [static] |
Returns the OneWireContainer object of the device with the given address.
| adapter | The DSPortAdapter that the device is connected to. |
| address | a long representing the address of the device |
| static OneWireContainer getDeviceContainer | ( | DSPortAdapter | adapter, |
| byte[] | address | ||
| ) | [static] |
Returns the OneWireContainer object of the device with the given address.
| adapter | The DSPortAdapter that the device is connected to. |
| address | a byte array representing the address of the device |
| static OneWireContainer getDeviceContainer | ( | DSPortAdapter | adapter, |
| String | address | ||
| ) | [static] |
Returns the OneWireContainer object of the device with the given address.
| adapter | The DSPortAdapter that the device is connected to. |
| address | a String representing the address of the device |
| static OneWireContainer getDeviceContainer | ( | DSPortAdapter | adapter, |
| Long | longAddress | ||
| ) | [static] |
Returns the OneWireContainer object of the device with the given address.
| adapter | The DSPortAdapter that the device is connected to. |
| address | a Long object representing the address of the device |
| OWPath getDevicePath | ( | byte[] | address | ) |
Returns the OWPath of the device with the given address.
| address | a byte array representing the address of the device |
| OWPath getDevicePath | ( | String | address | ) |
Returns the OWPath of the device with the given address.
| address | a string representing the address of the device |
| OWPath getDevicePath | ( | long | address | ) |
Returns the OWPath of the device with the given address.
| address | a long representing the address of the device |
| abstract OWPath getDevicePath | ( | Long | address | ) | [pure virtual] |
Returns the OWPath of the device with the given address.
| address | a Long object representing the address of the device |
Implemented in ChainMonitor, DeviceMonitor, and NetworkDeviceMonitor.
| int getMaxErrorCount | ( | ) |
Number of searches that an error occurs before listener's are notified.
| int getMaxStateCount | ( | ) |
The number of searches that a button should be "missing" before it is removed.
| boolean isMonitorRunning | ( | ) |
Check if this monitor is running.
true if monitor is running | void killMonitor | ( | ) |
Kill this monitor.
Wait util this thread is no longer alive (with timeout).
| void msSleep | ( | long | msTime | ) | [protected] |
Sleep for the specified number of milliseconds.
| msTime | number of milliseconds to sleep |
| boolean pauseMonitor | ( | boolean | blocking | ) |
Pause this monitor.
| blocking | if true, this method will block until the monitor is paused. |
| static void putDeviceContainer | ( | byte[] | address, |
| OneWireContainer | owc | ||
| ) | [static] |
Sets the OneWireContainer object of the device with the given address.
| address | a byte array object representing the address of the device |
| owc | The specific OneWireContainer object of the device |
| static void putDeviceContainer | ( | long | address, |
| OneWireContainer | owc | ||
| ) | [static] |
Sets the OneWireContainer object of the device with the given address.
| address | a long object representing the address of the device |
| owc | The specific OneWireContainer object of the device |
| static void putDeviceContainer | ( | Long | longAddress, |
| OneWireContainer | owc | ||
| ) | [static] |
Sets the OneWireContainer object of the device with the given address.
| address | a Long object representing the address of the device |
| owc | The specific OneWireContainer object of the device |
| static void putDeviceContainer | ( | String | address, |
| OneWireContainer | owc | ||
| ) | [static] |
Sets the OneWireContainer object of the device with the given address.
| address | a String object representing the address of the device |
| owc | The specific OneWireContainer object of the device |
| void resetSearch | ( | ) |
Resets this device monitor.
All known devices will be marked as "departed" and departure events will be fired.
| boolean resumeMonitor | ( | boolean | blocking | ) |
Resume this monitor.
| blocking | if true, this method will block until the monitor is resumed. |
| void run | ( | ) |
Monitor run method that performs a periodic search of the entire 1-Wire network.
Listeners that have registered are notified when changes in the network are detected.
| abstract void search | ( | Vector | arrivals, |
| Vector | departures | ||
| ) | throws OneWireException, OneWireIOException [pure virtual] |
Performs a search of the 1-Wire network.
| arrivals | A vector of Long objects, represent new arrival addresses. |
| departures | A vector of Long objects, represent departed addresses. |
Implemented in ChainMonitor, DeviceMonitor, and NetworkDeviceMonitor.
| abstract void setAdapter | ( | DSPortAdapter | adapter | ) | [pure virtual] |
Sets this monitor to search a new DSPortAdapter.
| the | DSPortAdapter this monitor should search |
Implemented in ChainMonitor, DeviceMonitor, and NetworkDeviceMonitor.
| void setMaxErrorCount | ( | int | errorCnt | ) |
Number of searches that an error occurs before listener's are notified.
| errorCnt | Number of searches that an error occurs before listener's are notified |
| void setMaxStateCount | ( | int | stateCnt | ) |
The number of searches that a button should be "missing" before it is removed.
| stateCnt | The number of searches that a button should be "missing" before it is removed. |
1.7.3