|
1-Wire API for .NET Version 4.00
|
A 1-Wire file output stream is an output stream for writing data to a OWFile or to a OWFileDescriptor.
More...
Inherits java::io::OutputStream.
Public Member Functions | |
| OWFileOutputStream (OneWireContainer owd, String name) throws OWFileNotFoundException | |
| Creates an output file stream to write to the file with the specified name. | |
| OWFileOutputStream (OneWireContainer[] owd, String name) throws OWFileNotFoundException | |
| Creates an output file stream to write to the file with the specified name. | |
| OWFileOutputStream (OneWireContainer owd, String name, boolean append) throws OWFileNotFoundException | |
Creates an output file stream to write to the file with the specified name. | |
| OWFileOutputStream (OneWireContainer[] owd, String name, boolean append) throws OWFileNotFoundException | |
Creates an output file stream to write to the file with the specified name. | |
| OWFileOutputStream (OWFile file) throws OWFileNotFoundException | |
Creates a file output stream to write to the file represented by the specified File object. | |
| OWFileOutputStream (OWFileDescriptor fdObj) | |
| Creates an output file stream to write to the specified file descriptor, which represents an existing connection to an actual file in the Filesystem. | |
| void | write (int b) throws IOException |
| Writes the specified byte to this file output stream. | |
| void | write (byte b[]) throws IOException |
Writes b.length bytes from the specified byte array to this file output stream. | |
| void | write (byte b[], int off, int len) throws IOException |
Writes len bytes from the specified byte array starting at offset off to this file output stream. | |
| void | close () throws IOException |
| Closes this file output stream and releases any system resources associated with this stream. | |
| OWFileDescriptor | getFD () throws IOException |
| Returns the file descriptor associated with this stream. | |
| void | finalize () throws IOException |
Cleans up the connection to the file, and ensures that the close method of this file output stream is called when there are no more references to this stream. | |
A 1-Wire file output stream is an output stream for writing data to a OWFile or to a OWFileDescriptor.
Whether or not a file is available or may be created depends upon the underlying platform. This platform allows a file to be opened for writing by only one OWFileOutputStream (or other file-writing object) at a time. In such situations the constructors in this class will fail if the file involved is already open. The 1-Wire File system must be formatted before use. Use OWFile:format to prepare a device or group of devices.
The 1-Wire device will only be written in the following situations
getFD() and call the sync() method of the OWFileDescriptor until a SyncFailedException is NOT thrown IOException is thrown close() finalize() WARNING could deadlock if device not synced and inside beginExclusive/endExclusive block. Note that the 1-Wire File system can reside across multiple 1-Wire devices. In this case only one of the devices need be supplied to the constructor. Each device in a multi-device file system contains information to reacquire the entire list.
File and directory name limitations
Write to a 1-Wire file on device 'owd':
// create a 1-Wire file at root
OWFileOutputStream outstream = new OWFileOutputStream(owd, "DEMO.0"); // write the data (in a byte array data[])
outstream.write(data); // get 1-Wire File descriptor to flush to device
OWFileDescriptor owfd = owfile.getFD(); // loop until sync is successful
do
{
try
{
owfd.sync();
done = true;
}
catch (SyncFailedException e)
{
// do something
...
done = false;
}
}
while (!done) // close the stream to release system resources
outstream.close();
| OWFileOutputStream | ( | OneWireContainer | owd, |
| String | name | ||
| ) | throws OWFileNotFoundException |
Creates an output file stream to write to the file with the specified name.
A new OWFileDescriptor object is created to represent this file connection.
First, if there is a security manager, its checkWrite method is called with name as its argument.
If the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason then a FileNotFoundException is thrown.
| owd | OneWireContainer that this Filesystem resides on |
| name | the system-dependent filename |
| FileNotFoundException | if the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason |
| SecurityException | if a security manager exists and its checkWrite method denies write access to the file. |
| OWFileOutputStream | ( | OneWireContainer[] | owd, |
| String | name | ||
| ) | throws OWFileNotFoundException |
Creates an output file stream to write to the file with the specified name.
A new OWFileDescriptor object is created to represent this file connection.
First, if there is a security manager, its checkWrite method is called with name as its argument.
If the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason then a FileNotFoundException is thrown.
| owd | array of OneWireContainers that this Filesystem resides on |
| name | the system-dependent filename |
| FileNotFoundException | if the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason |
| SecurityException | if a security manager exists and its checkWrite method denies write access to the file. |
| OWFileOutputStream | ( | OneWireContainer | owd, |
| String | name, | ||
| boolean | append | ||
| ) | throws OWFileNotFoundException |
Creates an output file stream to write to the file with the specified name.
If the second argument is true, then bytes will be written to the end of the file rather than the beginning. A new OWFileDescriptor object is created to represent this file connection.
First, if there is a security manager, its checkWrite method is called with name as its argument.
If the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason then a FileNotFoundException is thrown.
| owd | OneWireContainer that this Filesystem resides on |
| name | the system-dependent file name |
| append | if true, then bytes will be written to the end of the file rather than the beginning |
| FileNotFoundException | if the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason. |
| SecurityException | if a security manager exists and its checkWrite method denies write access to the file. |
| OWFileOutputStream | ( | OneWireContainer[] | owd, |
| String | name, | ||
| boolean | append | ||
| ) | throws OWFileNotFoundException |
Creates an output file stream to write to the file with the specified name.
If the second argument is true, then bytes will be written to the end of the file rather than the beginning. A new OWFileDescriptor object is created to represent this file connection.
First, if there is a security manager, its checkWrite method is called with name as its argument.
If the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason then a FileNotFoundException is thrown.
| owd | array of OneWireContainers that this Filesystem resides on |
| name | the system-dependent file name |
| append | if true, then bytes will be written to the end of the file rather than the beginning |
| FileNotFoundException | if the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason. |
| SecurityException | if a security manager exists and its checkWrite method denies write access to the file. |
| OWFileOutputStream | ( | OWFile | file | ) | throws OWFileNotFoundException |
Creates a file output stream to write to the file represented by the specified File object.
A new OWFileDescriptor object is created to represent this file connection.
First, if there is a security manager, its checkWrite method is called with the path represented by the file argument as its argument.
If the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason then a FileNotFoundException is thrown.
| file | the file to be opened for writing. |
| FileNotFoundException | if the file exists but is a directory rather than a regular file, does not exist but cannot be created, or cannot be opened for any other reason |
| SecurityException | if a security manager exists and its checkWrite method denies write access to the file. |
| OWFileOutputStream | ( | OWFileDescriptor | fdObj | ) |
Creates an output file stream to write to the specified file descriptor, which represents an existing connection to an actual file in the Filesystem.
First, if there is a security manager, its checkWrite method is called with the file descriptor fdObj argument as its argument.
| fdObj | the file descriptor to be opened for writing. |
| SecurityException | if a security manager exists and its checkWrite method denies write access to the file descriptor. |
| void close | ( | ) | throws IOException |
Closes this file output stream and releases any system resources associated with this stream.
This file output stream may no longer be used for writing bytes.
| IOException | if an I/O error occurs. |
| void finalize | ( | ) | throws IOException |
Cleans up the connection to the file, and ensures that the close method of this file output stream is called when there are no more references to this stream.
| IOException | if an I/O error occurs. |
| OWFileDescriptor getFD | ( | ) | throws IOException |
Returns the file descriptor associated with this stream.
OWFileDescriptor object that represents the connection to the file in the Filesystem being used by this FileOutputStream object.| IOException | if an I/O error occurs. |
| void write | ( | byte | b[] | ) | throws IOException |
Writes b.length bytes from the specified byte array to this file output stream.
| b | the data. |
| IOException | if an I/O error occurs. |
| void write | ( | byte | b[], |
| int | off, | ||
| int | len | ||
| ) | throws IOException |
Writes len bytes from the specified byte array starting at offset off to this file output stream.
| b | the data. |
| off | the start offset in the data. |
| len | the number of bytes to write. |
| IOException | if an I/O error occurs. |
| void write | ( | int | b | ) | throws IOException |
Writes the specified byte to this file output stream.
Implements the write method of OutputStream.
| b | the byte to be written. |
| IOException | if an I/O error occurs. |
1.7.3