|
1-Wire API for .NET Version 4.00
|
A OWFileInputStream obtains input bytes from a file in a 1-Wire Filesystem.
More...
Inherits java::io::InputStream.
Public Member Functions | |
| OWFileInputStream (OneWireContainer owd, String name) throws OWFileNotFoundException | |
Creates a FileInputStream by opening a connection to an actual file, the file named by the path name name in the Filesystem. | |
| OWFileInputStream (OneWireContainer[] owd, String name) throws OWFileNotFoundException | |
Creates a FileInputStream by opening a connection to an actual file, the file named by the path name name in the Filesystem. | |
| OWFileInputStream (OWFile file) throws OWFileNotFoundException | |
Creates a OWFileInputStream by opening a connection to an actual file, the file named by the File object file in the Filesystem. | |
| OWFileInputStream (OWFileDescriptor fdObj) | |
Creates a OWFileInputStream by using the file descriptor fdObj, which represents an existing connection to an actual file in the Filesystem. | |
| int | read () throws IOException |
| Reads a byte of data from this input stream. | |
| int | read (byte b[]) throws IOException |
Reads up to b.length bytes of data from this input stream into an array of bytes. | |
| int | read (byte b[], int off, int len) throws IOException |
Reads up to len bytes of data from this input stream into an array of bytes. | |
| long | skip (long n) throws IOException |
Skips over and discards n bytes of data from the input stream. | |
| int | available () throws IOException |
| Returns the number of bytes that can be read from this file input stream without blocking. | |
| void | close () throws IOException |
| Closes this file input stream and releases any system resources associated with the stream. | |
| final OWFileDescriptor | getFD () throws IOException |
Returns the OWFileDescriptor object that represents the connection to the actual file in the Filesystem being used by this FileInputStream. | |
| void | finalize () throws IOException |
Ensures that the close method of this file input stream is called when there are no more references to it. | |
| void | mark (int readlimit) |
| Marks the current position in this input stream. | |
| void | reset () throws IOException |
Repositions this stream to the position at the time the mark method was last called on this input stream. | |
| boolean | markSupported () |
Tests if this input stream supports the mark and reset methods. | |
A OWFileInputStream obtains input bytes from a file in a 1-Wire Filesystem.
What files are available depends on the 1-Wire device.
Note that the 1-Wire File system can reside across multiple 1-Wire devices. In this case only one of the devices need be supplied to the constructor. Each device in a multi-device file system contains information to reacquire the entire list.
File and directory name limitations
Read from a 1-Wire file on device 'owd':
// get an input stream to the 1-Wire file
OWFileInputStream instream = new OWFileInputStream(owd, "DEMO.0"); // read some data
byte[] data = new byte[2000];
int len = instream.read(data); // close the stream to release system resources
instream.close();
| OWFileInputStream | ( | OneWireContainer | owd, |
| String | name | ||
| ) | throws OWFileNotFoundException |
Creates a FileInputStream by opening a connection to an actual file, the file named by the path name name in the Filesystem.
A new OWFileDescriptor object is created to represent this file connection.
First, if there is a security manager, its checkRead method is called with the name argument as its argument.
If the named file does not exist, is a directory rather than a regular file, or for some other reason cannot be opened for reading then a FileNotFoundException is thrown.
| owd | OneWireContainer that this Filesystem resides on |
| name | the system-dependent file name. |
| FileNotFoundException | if the file does not exist, is a directory rather than a regular file, or for some other reason cannot be opened for reading. |
| OWFileInputStream | ( | OneWireContainer[] | owd, |
| String | name | ||
| ) | throws OWFileNotFoundException |
Creates a FileInputStream by opening a connection to an actual file, the file named by the path name name in the Filesystem.
A new OWFileDescriptor object is created to represent this file connection.
First, if there is a security manager, its checkRead method is called with the name argument as its argument.
If the named file does not exist, is a directory rather than a regular file, or for some other reason cannot be opened for reading then a FileNotFoundException is thrown.
| owd | array of OneWireContainers that this Filesystem resides on |
| name | the system-dependent file name. |
| FileNotFoundException | if the file does not exist, is a directory rather than a regular file, or for some other reason cannot be opened for reading. |
| OWFileInputStream | ( | OWFile | file | ) | throws OWFileNotFoundException |
Creates a OWFileInputStream by opening a connection to an actual file, the file named by the File object file in the Filesystem.
A new OWFileDescriptor object is created to represent this file connection.
If the named file does not exist, is a directory rather than a regular file, or for some other reason cannot be opened for reading then a FileNotFoundException is thrown.
| file | the file to be opened for reading. |
| FileNotFoundException | if the file does not exist, is a directory rather than a regular file, or for some other reason cannot be opened for reading. |
| OWFileInputStream | ( | OWFileDescriptor | fdObj | ) |
Creates a OWFileInputStream by using the file descriptor fdObj, which represents an existing connection to an actual file in the Filesystem.
If fdObj is null then a NullPointerException is thrown.
| fdObj | the file descriptor to be opened for reading. |
| int available | ( | ) | throws IOException |
Returns the number of bytes that can be read from this file input stream without blocking.
| IOException | if an I/O error occurs. |
| void close | ( | ) | throws IOException |
Closes this file input stream and releases any system resources associated with the stream.
| IOException | if an I/O error occurs. |
| void finalize | ( | ) | throws IOException |
Ensures that the close method of this file input stream is called when there are no more references to it.
| IOException | if an I/O error occurs. |
| final OWFileDescriptor getFD | ( | ) | throws IOException |
Returns the OWFileDescriptor object that represents the connection to the actual file in the Filesystem being used by this FileInputStream.
| IOException | if an I/O error occurs. |
| void mark | ( | int | readlimit | ) |
Marks the current position in this input stream.
A subsequent call to the reset method repositions this stream at the last marked position so that subsequent reads re-read the same bytes.
The readlimit arguments tells this input stream to allow that many bytes to be read before the mark position gets invalidated.
The general contract of mark is that, if the method markSupported returns true, the stream somehow remembers all the bytes read after the call to mark and stands ready to supply those same bytes again if and whenever the method reset is called. However, the stream is not required to remember any data at all if more than readlimit bytes are read from the stream before reset is called.
The mark method of InputStream does nothing.
| readlimit | the maximum limit of bytes that can be read before the mark position becomes invalid. |
| boolean markSupported | ( | ) |
Tests if this input stream supports the mark and reset methods.
The markSupported method of InputStream returns false.
true if this true type supports the mark and reset method; false otherwise. | int read | ( | byte | b[] | ) | throws IOException |
Reads up to b.length bytes of data from this input stream into an array of bytes.
This method blocks until some input is available.
| b | the buffer into which the data is read. |
-1 if there is no more data because the end of the file has been reached. | IOException | if an I/O error occurs. |
| int read | ( | ) | throws IOException |
Reads a byte of data from this input stream.
This method blocks if no input is yet available.
-1 if the end of the file is reached. | IOException | if an I/O error occurs. |
| int read | ( | byte | b[], |
| int | off, | ||
| int | len | ||
| ) | throws IOException |
Reads up to len bytes of data from this input stream into an array of bytes.
This method blocks until some input is available.
| b | the buffer into which the data is read. |
| off | the start offset of the data. |
| len | the maximum number of bytes read. |
-1 if there is no more data because the end of the file has been reached. | IOException | if an I/O error occurs. |
| void reset | ( | ) | throws IOException |
Repositions this stream to the position at the time the mark method was last called on this input stream.
The general contract of reset is:
If the method markSupported returns true, then:
If the method mark has not been called since the stream was created, or the number of bytes read from the stream since mark was last called is larger than the argument to mark at that last call, then an IOException might be thrown.
IOException is not thrown, then the stream is reset to a state such that all the bytes read since the most recent call to mark (or since the start of the file, if mark has not been called) will be resupplied to subsequent callers of the read method, followed by any bytes that otherwise would have been the next input data as of the time of the call to reset. If the method markSupported returns false, then:
The call to reset may throw an IOException.
IOException is not thrown, then the stream is reset to a fixed state that depends on the particular type of the input stream and how it was created. The bytes that will be supplied to subsequent callers of the read method depend on the particular type of the input stream. The method reset for class InputStream does nothing and always throws an IOException.
| IOException | if this stream has not been marked or if the mark has been invalidated. |
| long skip | ( | long | n | ) | throws IOException |
Skips over and discards n bytes of data from the input stream.
The skip method may, for a variety of reasons, end up skipping over some smaller number of bytes, possibly 0. The actual number of bytes skipped is returned.
| n | the number of bytes to be skipped. |
| IOException | if an I/O error occurs. |
1.7.3