|
1-Wire API for .NET Version 4.00
|
An abstract representation of file and directory pathnames on 1-Wire devices. More...
Public Member Functions | |
| OWFile (OneWireContainer owd, String pathname) | |
Creates a new OWFile instance by converting the given pathname string into an abstract pathname. | |
| OWFile (OneWireContainer[] owd, String pathname) | |
Creates a new OWFile instance by converting the given pathname string into an abstract pathname. | |
| OWFile (OneWireContainer owd, String parent, String child) | |
Creates a new OWFile instance from a parent pathname string and a child pathname string. | |
| OWFile (OWFile parent, String child) | |
Creates a new OWFile instance from a parent abstract pathname and a child pathname string. | |
| String | getName () |
| Returns the name of the file or directory denoted by this abstract pathname. | |
| String | getParent () |
Returns the pathname string of this abstract pathname's parent, or null if this pathname does not name a parent directory. | |
| OWFile | getParentFile () |
Returns the abstract pathname of this abstract pathname's parent, or null if this pathname does not name a parent directory. | |
| String | getPath () |
| Converts this abstract pathname into a pathname string. | |
| boolean | isAbsolute () |
| Tests whether this abstract pathname is absolute. | |
| String | getAbsolutePath () |
| Returns the absolute pathname string of this abstract pathname. | |
| OWFile | getAbsoluteFile () |
| Returns the absolute form of this abstract pathname. | |
| String | getCanonicalPath () throws IOException |
| Returns the canonical pathname string of this abstract pathname. | |
| OWFile | getCanonicalFile () throws IOException |
| Returns the canonical form of this abstract pathname. | |
| boolean | canRead () |
| Tests whether the application can read the file denoted by this abstract pathname. | |
| boolean | canWrite () |
| Tests whether the application can modify to the file denoted by this abstract pathname. | |
| boolean | exists () |
| Tests whether the file denoted by this abstract pathname exists. | |
| boolean | isDirectory () |
| Tests whether the file denoted by this abstract pathname is a directory. | |
| boolean | isFile () |
| Tests whether the file denoted by this abstract pathname is a normal file. | |
| boolean | isHidden () |
| Tests whether the file named by this abstract pathname is a hidden file. | |
| long | lastModified () |
| Returns the time that the file denoted by this abstract pathname was last modified. | |
| long | length () |
| Returns the length of the file denoted by this abstract pathname. | |
| boolean | createNewFile () throws IOException |
| Atomically creates a new, empty file named by this abstract pathname if and only if a file with this name does not yet exist. | |
| boolean | delete () |
| Deletes the file or directory denoted by this abstract pathname. | |
| String[] | list () |
| Returns an array of strings naming the files and directories in the directory denoted by this abstract pathname. | |
| OWFile[] | listFiles () |
| Returns an array of abstract pathnames denoting the files in the directory denoted by this abstract pathname. | |
| boolean | mkdir () |
| Creates the directory named by this abstract pathname. | |
| boolean | mkdirs () |
| Creates the directory named by this abstract pathname, including any necessary but nonexistent parent directories. | |
| boolean | renameTo (OWFile dest) |
| Renames the file denoted by this abstract pathname. | |
| boolean | setLastModified (long time) |
| Sets the last-modified time of the file or directory named by this abstract pathname. | |
| boolean | setReadOnly () |
| Marks the file or directory named by this abstract pathname so that only read operations are allowed. | |
| int | compareTo (OWFile pathname) |
| Compares two abstract pathnames lexicographically. | |
| int | compareTo (Object o) |
| Compares this abstract pathname to another object. | |
| boolean | equals (Object obj) |
| Tests this abstract pathname for equality with the given object. | |
| int | hashCode () |
| Computes a hash code for this abstract pathname. | |
| String | toString () |
| Returns the pathname string of this abstract pathname. | |
| OWFileDescriptor | getFD () throws IOException |
Returns the OWFileDescriptor object that represents the connection to the actual file in the Filesystem being used by this OWFileInputStream. | |
| OneWireContainer | getOneWireContainer () |
| Gets the OneWireContainer that this File resides on. | |
| OneWireContainer[] | getOneWireContainers () |
| Gets the OneWireContainer(s) that this File resides on. | |
| void | format () throws IOException |
| Format the Filesystem on the 1-Wire device provided in the constructor. | |
| int | getFreeMemory () throws IOException |
| Gets the number of bytes available on this device for file and directory information. | |
| void | close () throws IOException |
| Closes this file and releases any system resources associated with this stream. | |
| int[] | getPageList () throws IOException |
| Get's an array of integers that represents the page list of the file or directory represented by this OWFile. | |
| int | getStartPage () throws IOException |
| Returns an integer which represents the starting memory page of the file or directory represented by this OWFile. | |
| PagedMemoryBank | getMemoryBankForPage (int page) |
| Get's the memory bank object for the specified page. | |
| int | getLocalPage (int page) |
| Get's the local page number on the memory bank object for the specified page. | |
Static Public Member Functions | |
| static OWFile[] | listRoots (OneWireContainer owc) |
| List the available filesystem roots. | |
Static Public Attributes | |
| static final String | separator = "/" |
| Field separator. | |
| static final char | separatorChar = '/' |
| Field separatorChar. | |
| static final String | pathSeparator = ":" |
| Field pathSeparator. | |
| static final char | pathSeparatorChar = ':' |
| Field pathSeparatorChar. | |
Protected Member Functions | |
| void | finalize () throws IOException |
Cleans up the connection to the file, and ensures that the close method of this file output stream is called when there are no more references to this stream. | |
An abstract representation of file and directory pathnames on 1-Wire devices.
User interfaces and operating systems use system-dependent pathname strings to name files and directories. This class presents an abstract, system-independent view of hierarchical pathnames. An abstract pathname has two components:
"/" for the UNIX root directory, or "\\" for a Win32 UNC pathname, and Each name in an abstract pathname except for the last denotes a directory; the last name may denote either a directory or a file. The empty abstract pathname has no prefix and an empty name sequence.
The conversion of a pathname string to or from an abstract pathname is inherently system-dependent. When an abstract pathname is converted into a pathname string, each name is separated from the next by a single copy of the default separator character. The default name-separator character is defined by the system property OWFile.separator, and is made available in the public static fields separator and separatorChar of this class. When a pathname string is converted into an abstract pathname, the names within it may be separated by the default name-separator character or by any other name-separator character that is supported by the underlying system.
A pathname, whether abstract or in string form, may be either absolute or relative. An absolute pathname is complete in that no other information is required in order to locate the file that it denotes. A relative pathname, in contrast, must be interpreted in terms of information taken from some other pathname. By default the classes in the java.io package always resolve relative pathnames against the current user directory. This directory is named by the system property user.dir, and is typically the directory in which the Java virtual machine was invoked. The pathname provided to this OWFile however is always absolute.
The prefix concept is used to handle root directories on UNIX platforms, and drive specifiers, root directories and UNC pathnames on Win32 platforms, as follows:
For 1-Wire the Filesystem , the prefix of an absolute pathname is always "/". The abstract pathname denoting the root directory has the prefix "/" and an empty name sequence.
Instances of the OWFile class are immutable; that is, once created, the abstract pathname represented by a OWFile object will never change.
The methods in the class are the same as in the java.io.File version 1.2 with the following exceptions
Methods provided but of limited functionallity
Methods not provided or supported:
Extra Methods (not usually in 1.2 java.io.File)
File and directory name limitations
OWFile instance is closed with the close() method or the sync() method from the OWFileDescriptor sync() method for flushing the changes to the Filesystem is preferred since it can be called multiple times if there is a connection problem format() method in order for files or directories to be added or changed. format() method is used to link these devices then only the 'root' need be used in future constuctors of this class or the 1-Wire file stream classes. getFreeMemory() method to get an estimate of free memory available. close() method to release system resources allocated when done with the OWFile instance Format the Filesystem of the 1-Wire device 'owd':
// create a 1-Wire file at root
OWFile owfile = new OWFile(owd, ""); // format Filesystem
owfile.format(); // get 1-Wire File descriptor to flush to device
OWFileDescriptor owfd = owfile.getFD();
// loop until sync is successful
do
{
try
{
owfd.sync();
done = true;
}
catch (SyncFailedException e)
{
// do something
...
done = false;
}
}
while (!done) // close the 1-Wire file to release system resources
owfile.close();
Make a multi-level directory structure on the 1-Wire device 'owd':
OWFile owfile = new OWFile(owd, "/doc/text/temp"); // make the directories
if (owfile.mkdirs())
System.out.println("Success!");
else
System.out.println("Out of memory or invalid file/directory"); // get 1-Wire File descriptor to flush to device
...
http://pdfserv.maxim-ic.com/arpdf/AppNotes/app114.pdf
| OWFile | ( | OneWireContainer | owd, |
| String | pathname | ||
| ) |
Creates a new OWFile instance by converting the given pathname string into an abstract pathname.
If the given string is the empty string, then the result is the empty abstract pathname.
| owd | OneWireContainer that this Filesystem resides on |
| pathname | A pathname string |
| NullPointerException | If the pathname argument is null |
| OWFile | ( | OneWireContainer[] | owd, |
| String | pathname | ||
| ) |
Creates a new OWFile instance by converting the given pathname string into an abstract pathname.
If the given string is the empty string, then the result is the empty abstract pathname.
| owd | ordered array of OneWireContainers that this Filesystem resides on |
| pathname | A pathname string |
| NullPointerException | If the pathname argument is null |
Change the OWFileDescriptor to accept only an array of containers Change the local ref to be an array Create a single array in constructors with single passed owc
| OWFile | ( | OneWireContainer | owd, |
| String | parent, | ||
| String | child | ||
| ) |
Creates a new OWFile instance from a parent pathname string and a child pathname string.
If parent is null then the new OWFile instance is created as if by invoking the single-argument OWFile constructor on the given child pathname string.
Otherwise the parent pathname string is taken to denote a directory, and the child pathname string is taken to denote either a directory or a file. If the child pathname string is absolute then it is converted into a relative pathname in a system-dependent way. If parent is the empty string then the new OWFile instance is created by converting child into an abstract pathname and resolving the result against a system-dependent default directory. Otherwise each pathname string is converted into an abstract pathname and the child abstract pathname is resolved against the parent.
| owd | OneWireContainer that this Filesystem resides on |
| parent | The parent pathname string |
| child | The child pathname string |
| NullPointerException | If child is null |
Creates a new OWFile instance from a parent abstract pathname and a child pathname string.
If parent is null then the new OWFile instance is created as if by invoking the single-argument OWFile constructor on the given child pathname string.
Otherwise the parent abstract pathname is taken to denote a directory, and the child pathname string is taken to denote either a directory or a file. If the child pathname string is absolute then it is converted into a relative pathname in a system-dependent way. If parent is the empty abstract pathname then the new OWFile instance is created by converting child into an abstract pathname and resolving the result against a system-dependent default directory. Otherwise each pathname string is converted into an abstract pathname and the child abstract pathname is resolved against the parent.
| owd | OneWireContainer that this Filesystem resides on |
| parent | The parent abstract pathname |
| child | The child pathname string |
| NullPointerException | If child is null |
| boolean canRead | ( | ) |
Tests whether the application can read the file denoted by this abstract pathname.
true if and only if the file specified by this abstract pathname exists and can be read by the application; false otherwise | boolean canWrite | ( | ) |
Tests whether the application can modify to the file denoted by this abstract pathname.
true if and only if the Filesystem actually contains a file denoted by this abstract pathname and the application is allowed to write to the file; false otherwise. | void close | ( | ) | throws IOException |
Closes this file and releases any system resources associated with this stream.
This file may no longer be used after this operation.
| IOException | if an I/O error occurs. |
| int compareTo | ( | OWFile | pathname | ) |
Compares two abstract pathnames lexicographically.
The ordering defined by this method depends upon the underlying system. On UNIX systems, alphabetic case is significant in comparing pathnames; on Win32 systems it is not.
| pathname | The abstract pathname to be compared to this abstract pathname |
| int compareTo | ( | Object | o | ) |
Compares this abstract pathname to another object.
If the other object is an abstract pathname, then this function behaves like compareTo(OWFile). Otherwise, it throws a ClassCastException, since abstract pathnames can only be compared to abstract pathnames.
| o | The Object to be compared to this abstract pathname |
| <code>ClassCastException</code> | if the argument is not an abstract pathname |
| boolean createNewFile | ( | ) | throws IOException |
Atomically creates a new, empty file named by this abstract pathname if and only if a file with this name does not yet exist.
The check for the existence of the file and the creation of the file if it does not exist are a single operation that is atomic with respect to all other filesystem activities that might affect the file.
true if the named file does not exist and was successfully created; false if the named file already exists| IOException | If an I/O error occurred |
| boolean delete | ( | ) |
Deletes the file or directory denoted by this abstract pathname.
If this pathname denotes a directory, then the directory must be empty in order to be deleted.
true if and only if the file or directory is successfully deleted; false otherwise | boolean equals | ( | Object | obj | ) |
Tests this abstract pathname for equality with the given object.
Returns true if and only if the argument is not null and is an abstract pathname that denotes the same file or directory as this abstract pathname. Whether or not two abstract pathnames are equal depends upon the underlying system. On UNIX systems, alphabetic case is significant in comparing pathnames; on Win32 systems it is not.
| obj | The object to be compared with this abstract pathname |
true if and only if the objects are the same; false otherwise | boolean exists | ( | ) |
Tests whether the file denoted by this abstract pathname exists.
true if and only if the file denoted by this abstract pathname exists; false otherwise | void finalize | ( | ) | throws IOException [protected] |
Cleans up the connection to the file, and ensures that the close method of this file output stream is called when there are no more references to this stream.
| IOException | if an I/O error occurs. |
| void format | ( | ) | throws IOException |
Format the Filesystem on the 1-Wire device provided in the constructor.
This operation is required before any file IO is possible.
WARNING this will remove any files/directories.
| IOException | if an I/O error occurs. |
| OWFile getAbsoluteFile | ( | ) |
Returns the absolute form of this abstract pathname.
Equivalent to new File(this.getAbsolutePath()).
| String getAbsolutePath | ( | ) |
Returns the absolute pathname string of this abstract pathname.
If this abstract pathname is already absolute, then the pathname string is simply returned as if by the getPath method. If this abstract pathname is the empty abstract pathname then the pathname string of the current user directory, which is named by the system property user.dir, is returned. Otherwise this pathname is resolved in a system-dependent way. On UNIX systems, a relative pathname is made absolute by resolving it against the current user directory. On Win32 systems, a relative pathname is made absolute by resolving it against the current directory of the drive named by the pathname, if any; if not, it is resolved against the current user directory.
| OWFile getCanonicalFile | ( | ) | throws IOException |
Returns the canonical form of this abstract pathname.
Equivalent to new File(this.getCanonicalPath()).
| IOException | If an I/O error occurs, which is possible because the construction of the canonical pathname may require filesystem queries |
| String getCanonicalPath | ( | ) | throws IOException |
Returns the canonical pathname string of this abstract pathname.
The precise definition of canonical form is system-dependent, but canonical forms are always absolute. Thus if this abstract pathname is relative it will be converted to absolute form as if by the getAbsoluteFile method.
Every pathname that denotes an existing file or directory has a unique canonical form. Every pathname that denotes a nonexistent file or directory also has a unique canonical form. The canonical form of the pathname of a nonexistent file or directory may be different from the canonical form of the same pathname after the file or directory is created. Similarly, the canonical form of the pathname of an existing file or directory may be different from the canonical form of the same pathname after the file or directory is deleted.
| IOException | If an I/O error occurs, which is possible because the construction of the canonical pathname may require filesystem queries |
| OWFileDescriptor getFD | ( | ) | throws IOException |
Returns the OWFileDescriptor object that represents the connection to the actual file in the Filesystem being used by this OWFileInputStream.
| IOException | if an I/O error occurs. |
| int getFreeMemory | ( | ) | throws IOException |
Gets the number of bytes available on this device for file and directory information.
| IOException | if an I/O error occurs |
| int getLocalPage | ( | int | page | ) |
Get's the local page number on the memory bank object for the specified page.
This is significant if the Filesystem spans memory banks on the same or different devices.
| PagedMemoryBank getMemoryBankForPage | ( | int | page | ) |
Get's the memory bank object for the specified page.
This is significant if the Filesystem spans memory banks on the same or different devices.
| String getName | ( | ) |
Returns the name of the file or directory denoted by this abstract pathname.
This is just the last name in the pathname's name sequence. If the pathname's name sequence is empty, then the empty string is returned.
| OneWireContainer getOneWireContainer | ( | ) |
Gets the OneWireContainer that this File resides on.
This is where the 'filesystem' resides. If this Filesystem spans multiple devices then this method returns the 'MASTER' device.
| OneWireContainer [] getOneWireContainers | ( | ) |
Gets the OneWireContainer(s) that this File resides on.
This is where the 'filesystem' resides. The first device is the 'MASTER' device and the other devices are 'SATELLITE' devices.
| int [] getPageList | ( | ) | throws IOException |
Get's an array of integers that represents the page list of the file or directory represented by this OWFile.
| IOException | if an I/O error occurs. |
| String getParent | ( | ) |
Returns the pathname string of this abstract pathname's parent, or null if this pathname does not name a parent directory.
The parent of an abstract pathname consists of the pathname's prefix, if any, and each name in the pathname's name sequence except for the last. If the name sequence is empty then the pathname does not name a parent directory.
null if this pathname does not name a parent | OWFile getParentFile | ( | ) |
Returns the abstract pathname of this abstract pathname's parent, or null if this pathname does not name a parent directory.
The parent of an abstract pathname consists of the pathname's prefix, if any, and each name in the pathname's name sequence except for the last. If the name sequence is empty then the pathname does not name a parent directory.
null if this pathname does not name a parent | String getPath | ( | ) |
Converts this abstract pathname into a pathname string.
The resulting string uses the default name-separator character to separate the names in the name sequence.
| int getStartPage | ( | ) | throws IOException |
Returns an integer which represents the starting memory page of the file or directory represented by this OWFile.
| IOException | if the file doesn't exist |
| int hashCode | ( | ) |
Computes a hash code for this abstract pathname.
Because equality of abstract pathnames is inherently system-dependent, so is the computation of their hash codes. On UNIX systems, the hash code of an abstract pathname is equal to the exclusive or of its pathname string and the decimal value 1234321. On Win32 systems, the hash code is equal to the exclusive or of its pathname string, convered to lower case, and the decimal value 1234321.
| boolean isAbsolute | ( | ) |
Tests whether this abstract pathname is absolute.
The definition of absolute pathname is system dependent. On UNIX systems, a pathname is absolute if its prefix is "/". On Win32 systems, a pathname is absolute if its prefix is a drive specifier followed by "\\", or if its prefix is "\\".
true if this abstract pathname is absolute, false otherwise | boolean isDirectory | ( | ) |
Tests whether the file denoted by this abstract pathname is a directory.
true if and only if the file denoted by this abstract pathname exists and is a directory; false otherwise | boolean isFile | ( | ) |
Tests whether the file denoted by this abstract pathname is a normal file.
A file is normal if it is not a directory and, in addition, satisfies other system-dependent criteria. Any non-directory file created by a Java application is guaranteed to be a normal file.
true if and only if the file denoted by this abstract pathname exists and is a normal file; false otherwise | boolean isHidden | ( | ) |
Tests whether the file named by this abstract pathname is a hidden file.
The exact definition of hidden is system-dependent. On UNIX systems, a file is considered to be hidden if its name begins with a period character ('.'). On Win32 systems, a file is considered to be hidden if it has been marked as such in the filesystem.
true if and only if the file denoted by this abstract pathname is hidden according to the conventions of the underlying platform | long lastModified | ( | ) |
Returns the time that the file denoted by this abstract pathname was last modified.
long value representing the time the file was last modified, measured in milliseconds since the epoch (00:00:00 GMT, January 1, 1970), or 0L if the file does not exist or if an I/O error occurs | long length | ( | ) |
Returns the length of the file denoted by this abstract pathname.
0L if the file does not exist | String [] list | ( | ) |
Returns an array of strings naming the files and directories in the directory denoted by this abstract pathname.
If this abstract pathname does not denote a directory, then this method returns null. Otherwise an array of strings is returned, one for each file or directory in the directory. Names denoting the directory itself and the directory's parent directory are not included in the result. Each string is a file name rather than a complete path.
There is no guarantee that the name strings in the resulting array will appear in any specific order; they are not, in particular, guaranteed to appear in alphabetical order.
null if this abstract pathname does not denote a directory, or if an I/O error occurs. | OWFile [] listFiles | ( | ) |
Returns an array of abstract pathnames denoting the files in the directory denoted by this abstract pathname.
If this abstract pathname does not denote a directory, then this method returns null. Otherwise an array of OWFile objects is returned, one for each file or directory in the directory. Pathnames denoting the directory itself and the directory's parent directory are not included in the result. Each resulting abstract pathname is constructed from this abstract pathname using the OWFile(OWFile, String) constructor. Therefore if this pathname is absolute then each resulting pathname is absolute; if this pathname is relative then each resulting pathname will be relative to the same directory.
There is no guarantee that the name strings in the resulting array will appear in any specific order; they are not, in particular, guaranteed to appear in alphabetical order.
null if this abstract pathname does not denote a directory, or if an I/O error occurs. | static OWFile [] listRoots | ( | OneWireContainer | owc | ) | [static] |
List the available filesystem roots.
A particular Java platform may support zero or more hierarchically-organized Filesystems. Each Filesystem has a root directory from which all other files in that file system can be reached. Windows platforms, for example, have a root directory for each active drive; UNIX platforms have a single root directory, namely "/". The set of available filesystem roots is affected by various system-level operations such the insertion or ejection of removable media and the disconnecting or unmounting of physical or virtual disk drives.
This method returns an array of OWFile objects that denote the root directories of the available filesystem roots. It is guaranteed that the canonical pathname of any file physically present on the local machine will begin with one of the roots returned by this method.
The canonical pathname of a file that resides on some other machine and is accessed via a remote-filesystem protocol such as SMB or NFS may or may not begin with one of the roots returned by this method. If the pathname of a remote file is syntactically indistinguishable from the pathname of a local file then it will begin with one of the roots returned by this method. Thus, for example, OWFile objects denoting the root directories of the mapped network drives of a Windows platform will be returned by this method, while OWFile objects containing UNC pathnames will not be returned by this method.
| owc | OneWireContainer that this Filesystem resides on |
OWFile objects denoting the available filesystem roots, or null if the set of roots could not be determined. The array will be empty if there are no filesystem roots. | boolean mkdir | ( | ) |
Creates the directory named by this abstract pathname.
true if and only if the directory was created; false otherwise | boolean mkdirs | ( | ) |
Creates the directory named by this abstract pathname, including any necessary but nonexistent parent directories.
Note that if this operation fails it may have succeeded in creating some of the necessary parent directories.
true if and only if the directory was created, along with all necessary parent directories; false otherwise | boolean renameTo | ( | OWFile | dest | ) |
Renames the file denoted by this abstract pathname.
| dest | The new abstract pathname for the named file |
true if and only if the renaming succeeded; false otherwise| NullPointerException | If parameter dest is null |
| boolean setLastModified | ( | long | time | ) |
Sets the last-modified time of the file or directory named by this abstract pathname.
All platforms support file-modification times to the nearest second, but some provide more precision. The argument will be truncated to fit the supported precision. If the operation succeeds and no intervening operations on the file take place, then the next invocation of the lastModified method will return the (possibly truncated) time argument that was passed to this method.
| time | The new last-modified time, measured in milliseconds since the epoch (00:00:00 GMT, January 1, 1970) |
true if and only if the operation succeeded; false otherwise| IllegalArgumentException | If the argument is negative |
| boolean setReadOnly | ( | ) |
Marks the file or directory named by this abstract pathname so that only read operations are allowed.
After invoking this method the file or directory is guaranteed not to change until it is either deleted or marked to allow write access. Whether or not a read-only file or directory may be deleted depends upon the underlying system.
true if and only if the operation succeeded; false otherwise | String toString | ( | ) |
Returns the pathname string of this abstract pathname.
This is just the string returned by the getPath method.
1.7.3