|
1-Wire API for .NET Version 4.00
|
Inherits com::dalsemi::onewire::adapter::DSPortAdapter, and com::dalsemi::onewire::adapter::NetAdapterConstants.
Public Member Functions | |
| NetAdapter () | |
| Creates an instance of NetAdapter that isn't connected. | |
| void | setSecret (String secret) |
| Sets the shared secret for authenticating this NetAdapter with a NetAdapterHost. | |
| void | resetSecret () |
| Resets the secret to be the default stored in the onewire.properties file (if there is one), or the default as defined by NetAdapterConstants. | |
| void | pingHost () throws OneWireException, OneWireIOException |
| Sends a ping to the host, just to keep the connection alive. | |
| boolean | adapterDetected () throws OneWireIOException, OneWireException |
| Detects adapter presence on the selected port. | |
| String | getAdapterName () |
| Retrieves the name of the port adapter as a string. | |
| String | getPortTypeDescription () |
| Retrieves a description of the port required by this port adapter. | |
| String | getClassVersion () |
| Retrieves a version string for this class. | |
| Enumeration | getPortNames () |
| Retrieves a list of the platform appropriate port names for this adapter. | |
| boolean | selectPort (String portName) throws OneWireIOException, OneWireException |
| Specifies a platform appropriate port name for this adapter. | |
| boolean | selectPort (Socket sock) throws OneWireIOException, OneWireException |
| New method, unique to NetAdapter. | |
| void | freePort () throws OneWireException |
| Frees ownership of the selected port, if it is currently owned, back to the system. | |
| String | getPortName () throws OneWireException |
Retrieves the name of the selected port as a String. | |
| boolean | canOverdrive () throws OneWireIOException, OneWireException |
| Returns whether adapter can physically support overdrive mode. | |
| boolean | canHyperdrive () throws OneWireIOException, OneWireException |
| Returns whether the adapter can physically support hyperdrive mode. | |
| boolean | canFlex () throws OneWireIOException, OneWireException |
| Returns whether the adapter can physically support flex speed mode. | |
| boolean | canProgram () throws OneWireIOException, OneWireException |
| Returns whether adapter can physically support 12 volt power mode. | |
| boolean | canDeliverPower () throws OneWireIOException, OneWireException |
| Returns whether the adapter can physically support strong 5 volt power mode. | |
| boolean | canDeliverSmartPower () throws OneWireIOException, OneWireException |
| Returns whether the adapter can physically support "smart" strong 5 volt power mode. | |
| boolean | canBreak () throws OneWireIOException, OneWireException |
| Returns whether adapter can physically support 0 volt 'break' mode. | |
| boolean | findFirstDevice () throws OneWireIOException, OneWireException |
Returns true if the first iButton or 1-Wire device is found on the 1-Wire Network. | |
| boolean | findNextDevice () throws OneWireIOException, OneWireException |
Returns true if the next iButton or 1-Wire device is found. | |
| void | getAddress (byte[] address) |
| Copies the 'current' 1-Wire device address being used by the adapter into the array. | |
| void | setSearchOnlyAlarmingDevices () |
| Sets the 1-Wire Network search to find only iButtons and 1-Wire devices that are in an 'Alarm' state that signals a need for attention. | |
| void | setNoResetSearch () |
| Sets the 1-Wire Network search to not perform a 1-Wire reset before a search. | |
| void | setSearchAllDevices () |
| Sets the 1-Wire Network search to find all iButtons and 1-Wire devices whether they are in an 'Alarm' state or not and restores the default setting of providing a 1-Wire reset command before each search. | |
| void | targetAllFamilies () |
| Removes any selectivity during a search for iButtons or 1-Wire devices by family type. | |
| void | targetFamily (int family) |
| Takes an integer to selectively search for this desired family type. | |
| void | targetFamily (byte family[]) |
| Takes an array of bytes to use for selectively searching for acceptable family codes. | |
| void | excludeFamily (int family) |
| Takes an integer family code to avoid when searching for iButtons. | |
| void | excludeFamily (byte family[]) |
| Takes an array of bytes containing family codes to avoid when finding iButtons or 1-Wire devices. | |
| boolean | beginExclusive (boolean blocking) throws OneWireException |
| Gets exclusive use of the 1-Wire to communicate with an iButton or 1-Wire Device. | |
| void | endExclusive () |
| Relinquishes exclusive control of the 1-Wire Network. | |
| int | reset () throws OneWireIOException, OneWireException |
| Sends a Reset to the 1-Wire Network. | |
| void | putBit (boolean bitValue) throws OneWireIOException, OneWireException |
| Sends a bit to the 1-Wire Network. | |
| boolean | getBit () throws OneWireIOException, OneWireException |
| Gets a bit from the 1-Wire Network. | |
| void | putByte (int byteValue) throws OneWireIOException, OneWireException |
| Sends a byte to the 1-Wire Network. | |
| int | getByte () throws OneWireIOException, OneWireException |
| Gets a byte from the 1-Wire Network. | |
| byte[] | getBlock (int len) throws OneWireIOException, OneWireException |
| Gets a block of data from the 1-Wire Network. | |
| void | getBlock (byte[] arr, int len) throws OneWireIOException, OneWireException |
| Gets a block of data from the 1-Wire Network and write it into the provided array. | |
| void | getBlock (byte[] arr, int off, int len) throws OneWireIOException, OneWireException |
| Gets a block of data from the 1-Wire Network and write it into the provided array. | |
| void | dataBlock (byte[] dataBlock, int off, int len) throws OneWireIOException, OneWireException |
| Sends a block of data and returns the data received in the same array. | |
| void | setPowerDuration (int timeFactor) throws OneWireIOException, OneWireException |
| Sets the duration to supply power to the 1-Wire Network. | |
| boolean | startPowerDelivery (int changeCondition) throws OneWireIOException, OneWireException |
| Sets the 1-Wire Network voltage to supply power to a 1-Wire device. | |
| void | setProgramPulseDuration (int timeFactor) throws OneWireIOException, OneWireException |
| Sets the duration for providing a program pulse on the 1-Wire Network. | |
| boolean | startProgramPulse (int changeCondition) throws OneWireIOException, OneWireException |
| Sets the 1-Wire Network voltage to eprom programming level. | |
| void | startBreak () throws OneWireIOException, OneWireException |
| Sets the 1-Wire Network voltage to 0 volts. | |
| void | setPowerNormal () throws OneWireIOException, OneWireException |
| Sets the 1-Wire Network voltage to normal level. | |
| void | setSpeed (int speed) throws OneWireIOException, OneWireException |
| Sets the new speed of data transfer on the 1-Wire Network. | |
| int | getSpeed () |
| Returns the current data transfer speed on the 1-Wire Network. | |
Protected Attributes | |
| Integer | currentThreadHash = NOT_OWNED |
| Keeps hash of current thread for exclusive lock. | |
| Connection | conn = EMPTY_CONNECTION |
| instance for current connection, defaults to EMPTY | |
| String | portNameForReconnect = null |
| portName For Reconnecting to Host | |
| byte[] | netAdapterSecret = null |
| secret for authentication with the server | |
| boolean | useCustomSecret = false |
| if true, the user used a custom secret | |
| Boolean | multicastEnabled = null |
| indicates whether or not mulicast is enabled | |
| String | multicastGroup = null |
| The multicast group to use for NetAdapter Datagram packets. | |
| int | datagramPort = -1 |
| The port to use for NetAdapter Datagram packets. | |
Static Protected Attributes | |
| static final String | UNSPECIFIED_ERROR = "An unspecified error occurred." |
| Error message when neither RET_SUCCESS or RET_FAILURE are returned. | |
| static final String | COMM_FAILED = "IO Error: " |
| Error message when I/O failure occurs. | |
| static final Integer | NOT_OWNED = new Integer(0) |
| constant for no exclusive lock | |
NetAdapter is a network-based DSPortAdapter. It allows for the use of an actual DSPortAdapter which isn't on the local machine, but rather is connected to another device which is reachable via a TCP/IP network connection.
The syntax for the selectPort(String) command is the hostname of the computer which hosts the actual DSPortAdapter and the TCP/IP port that the host is listening on. If the port number is not specified, a default value of 6161 is used. Here are a few examples to illustrate the syntax:
<P?The use of the NetAdapter is virtually identical to the use of any other DSPortAdapter. The only significant changes are the necessity of the 'host' component (see NetAdapterHost) and the discovery of hosts on your network. There are currently two techniques used for discovering all of the hosts: The look-up of each host from the onewire.properties file and the use of multicast sockets for automatic discovery.
In the onewire.properties file, you can add a host to your list of valid hosts by making a NetAdapter.host with an integer to distinguish the hosts. There is no limit on the number of hosts which can appear in this list, but the first one must be numbered '0'. These hosts will then be returned in the list of valid 'ports' from the selectPortNames() method. Note that there do not have to be any servers returned from selectPortNames() for the NetAdapter to be able to connect to them (so it isn't necessary to add these entries for it to function), but applications which allow a user to automatically select an appropriate adapter and a port from a given list will not function properly without it. For example:
The multicast socket technique allows you to automatically discover hosts on your subnet which are listening for multicast packets. By default, the multicast discovery of NetAdapter hosts is disabled. When enabled, the NetAdapter creates a multicast socket and looks for servers every time you call selectPortNames(). This will add a 1 second delay (due to the socket timeout) on calling the method. If you'd like to enable this feature, add the following line to your onewire.properties file:
The port used and the multicast group used for multicast sockets can also be changed. The group however, must fall withing a valid range. For more information about multicast sockets in Java, see the Java tutorial on networking at http://java.sun.com/docs/books/tutorial/. Change the defaults in the onewire.properties file with the following entries:
Once the NetAdapter is connected with a host, a version check is performed followed by a simple authentication step. The authentication is dependent upon a secret shared between the NetAdapter and the host. Both will use a default value, that each will agree with if you don't provide a secret of your own. To set the secret, add the following line to your onewire.properties file:
Optionally, the secret can be specified on a per-host basis by simply adding the secret after the port number followed by a colon. If no port number is specified, a double-colon is required. Here are examples:
All of the above mentioned properties can be set on the command-line as well as being set in the onewire.properties file. To set the properties on the command-line, use the -D option: java -DNetAdapter.Secret="custom secret" myApplication
The following is a list of all parameters that can be set for the NetAdapter, followed by default values where applicable.
If you wanted added security on the communication channel, an SSL socket (or similar custom socket implementation) can be used by circumventing the standard DSPortAdapter's selectPort(String) and using the NetAdapter-specific selectPort(Socket). For example:
NetAdapter na = new NetAdapter();Socket secureSocket = // insert fancy secure socket implementation here
na.selectPort(secureSocket);
For information on setting up the host component, see the JavaDocs for theNetAdapterHost
| NetAdapter | ( | ) |
Creates an instance of NetAdapter that isn't connected.
Must call selectPort(String); or selectPort(Socket);
| boolean adapterDetected | ( | ) | throws OneWireIOException, OneWireException [virtual] |
Detects adapter presence on the selected port.
true if the adapter is confirmed to be connected to the selected port, false if the adapter is not connected.| OneWireIOException | |
| OneWireException |
Implements DSPortAdapter.
| boolean beginExclusive | ( | boolean | blocking | ) | throws OneWireException [virtual] |
Gets exclusive use of the 1-Wire to communicate with an iButton or 1-Wire Device.
This method should be used for critical sections of code where a sequence of commands must not be interrupted by communication of threads with other iButtons, and it is permissible to sustain a delay in the special case that another thread has already been granted exclusive access and this access has not yet been relinquished.
It can be called through the OneWireContainer class by the end application if they want to ensure exclusive use. If it is not called around several methods then it will be called inside each method.
| blocking | true if want to block waiting for an excluse access to the adapter |
true if blocking was false and a exclusive session with the adapter was aquired| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| boolean canBreak | ( | ) | throws OneWireIOException, OneWireException |
Returns whether adapter can physically support 0 volt 'break' mode.
true if this port adapter can do break, false otherwise.| OneWireIOException | on a 1-Wire communication error with the adapter |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| boolean canDeliverPower | ( | ) | throws OneWireIOException, OneWireException |
Returns whether the adapter can physically support strong 5 volt power mode.
true if this port adapter can do strong 5 volt mode, false otherwise.| OneWireIOException | on a 1-Wire communication error with the adapter |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| boolean canDeliverSmartPower | ( | ) | throws OneWireIOException, OneWireException |
Returns whether the adapter can physically support "smart" strong 5 volt power mode.
"smart" power delivery is the ability to deliver power until it is no longer needed. The current drop it detected and power delivery is stopped.
true if this port adapter can do "smart" strong 5 volt mode, false otherwise.| OneWireIOException | on a 1-Wire communication error with the adapter |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| boolean canFlex | ( | ) | throws OneWireIOException, OneWireException |
Returns whether the adapter can physically support flex speed mode.
true if this port adapter can do flex speed, false otherwise.| OneWireIOException | on a 1-Wire communication error with the adapter |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| boolean canHyperdrive | ( | ) | throws OneWireIOException, OneWireException |
Returns whether the adapter can physically support hyperdrive mode.
true if this port adapter can do HyperDrive, false otherwise.| OneWireIOException | on a 1-Wire communication error with the adapter |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| boolean canOverdrive | ( | ) | throws OneWireIOException, OneWireException |
Returns whether adapter can physically support overdrive mode.
true if this port adapter can do OverDrive, false otherwise.| OneWireIOException | on a 1-Wire communication error with the adapter |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| boolean canProgram | ( | ) | throws OneWireIOException, OneWireException |
Returns whether adapter can physically support 12 volt power mode.
true if this port adapter can do Program voltage, false otherwise.| OneWireIOException | on a 1-Wire communication error with the adapter |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| void dataBlock | ( | byte[] | dataBlock, |
| int | off, | ||
| int | len | ||
| ) | throws OneWireIOException, OneWireException [virtual] |
Sends a block of data and returns the data received in the same array.
This method is used when sending a block that contains reads and writes. The 'read' portions of the data block need to be pre-loaded with 0xFF's. It starts sending data from the index at offset 'off' for length 'len'.
| dataBlock | array of data to transfer to and from the 1-Wire Network. |
| off | offset into the array of data to start |
| len | length of data to send / receive starting at 'off' |
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| void endExclusive | ( | ) | [virtual] |
Relinquishes exclusive control of the 1-Wire Network.
This command dynamically marks the end of a critical section and should be used when exclusive control is no longer needed.
Implements DSPortAdapter.
| void excludeFamily | ( | int | family | ) |
Takes an integer family code to avoid when searching for iButtons.
or 1-Wire devices. If this method is used, then no devices of this family will be found by any of the search methods.
| family | the code of the family type NOT to target in searches |
Reimplemented from DSPortAdapter.
| void excludeFamily | ( | byte | family[] | ) |
Takes an array of bytes containing family codes to avoid when finding iButtons or 1-Wire devices.
If used, then no devices with family codes in this array will be found by any of the search methods.
| family | array of family cods NOT to target for searches |
Reimplemented from DSPortAdapter.
| boolean findFirstDevice | ( | ) | throws OneWireIOException, OneWireException [virtual] |
Returns true if the first iButton or 1-Wire device is found on the 1-Wire Network.
If no devices are found, then false will be returned.
true if an iButton or 1-Wire device is found.| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| boolean findNextDevice | ( | ) | throws OneWireIOException, OneWireException [virtual] |
Returns true if the next iButton or 1-Wire device is found.
The previous 1-Wire device found is used as a starting point in the search. If no more devices are found then false will be returned.
true if an iButton or 1-Wire device is found.| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| void freePort | ( | ) | throws OneWireException [virtual] |
Frees ownership of the selected port, if it is currently owned, back to the system.
This should only be called if the recently selected port does not have an adapter, or at the end of your application's use of the port.
| OneWireException | If port does not exist |
Implements DSPortAdapter.
| String getAdapterName | ( | ) | [virtual] |
Retrieves the name of the port adapter as a string.
The 'Adapter' is a device that connects to a 'port' that allows one to communicate with an iButton or other 1-Wire device. As example of this is 'DS9097U'.
String representation of the port adapter. Implements DSPortAdapter.
| void getAddress | ( | byte[] | address | ) | [virtual] |
Copies the 'current' 1-Wire device address being used by the adapter into the array.
This address is the last iButton or 1-Wire device found in a search (findNextDevice()...). This method copies into a user generated array to allow the reuse of the buffer. When searching many iButtons on the one wire network, this will reduce the memory burn rate.
| address | An array to be filled with the current iButton address. |
Implements DSPortAdapter.
| boolean getBit | ( | ) | throws OneWireIOException, OneWireException [virtual] |
Gets a bit from the 1-Wire Network.
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| byte [] getBlock | ( | int | len | ) | throws OneWireIOException, OneWireException [virtual] |
Gets a block of data from the 1-Wire Network.
| len | length of data bytes to receive |
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| void getBlock | ( | byte[] | arr, |
| int | len | ||
| ) | throws OneWireIOException, OneWireException [virtual] |
Gets a block of data from the 1-Wire Network and write it into the provided array.
| arr | array in which to write the received bytes |
| len | length of data bytes to receive |
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| void getBlock | ( | byte[] | arr, |
| int | off, | ||
| int | len | ||
| ) | throws OneWireIOException, OneWireException [virtual] |
Gets a block of data from the 1-Wire Network and write it into the provided array.
| arr | array in which to write the received bytes |
| off | offset into the array to start |
| len | length of data bytes to receive |
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| int getByte | ( | ) | throws OneWireIOException, OneWireException [virtual] |
Gets a byte from the 1-Wire Network.
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| String getClassVersion | ( | ) | [virtual] |
| String getPortName | ( | ) | throws OneWireException [virtual] |
Retrieves the name of the selected port as a String.
String of selected port| OneWireException | if valid port not yet selected |
Implements DSPortAdapter.
| Enumeration getPortNames | ( | ) | [virtual] |
Retrieves a list of the platform appropriate port names for this adapter.
A port must be selected with the method 'selectPort' before any other communication methods can be used. Using a communcation method before 'selectPort' will result in a OneWireException exception.
Enumeration of type String that contains the port names Implements DSPortAdapter.
| String getPortTypeDescription | ( | ) | [virtual] |
Retrieves a description of the port required by this port adapter.
An example of a 'Port' would 'serial communication port'.
String description of the port type required. Implements DSPortAdapter.
| int getSpeed | ( | ) |
Returns the current data transfer speed on the 1-Wire Network.
int representing the current 1-Wire speed Reimplemented from DSPortAdapter.
| void pingHost | ( | ) | throws OneWireException, OneWireIOException |
Sends a ping to the host, just to keep the connection alive.
Although it currently is not implemented on the standard NetAdapterHost, this command is used as a signal to the NetAdapterSim to simulate some amount of time that has run.
| void putBit | ( | boolean | bitValue | ) | throws OneWireIOException, OneWireException [virtual] |
Sends a bit to the 1-Wire Network.
| bitValue | the bit value to send to the 1-Wire Network. |
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| void putByte | ( | int | byteValue | ) | throws OneWireIOException, OneWireException [virtual] |
Sends a byte to the 1-Wire Network.
| byteValue | the byte value to send to the 1-Wire Network. |
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| int reset | ( | ) | throws OneWireIOException, OneWireException [virtual] |
Sends a Reset to the 1-Wire Network.
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Implements DSPortAdapter.
| boolean selectPort | ( | Socket | sock | ) | throws OneWireIOException, OneWireException |
New method, unique to NetAdapter.
Sets the "port", i.e. the connection to the server via an already established socket connection.
| sock | Socket connection to NetAdapterHost |
true if connection to host was successful| OneWireIOException | If port does not exist, or unable to communicate with port. |
| OneWireException | If port does not exist |
| boolean selectPort | ( | String | portName | ) | throws OneWireIOException, OneWireException [virtual] |
Specifies a platform appropriate port name for this adapter.
Note that even though the port has been selected, it's ownership may be relinquished if it is not currently held in a 'exclusive' block. This class will then try to re-aquire the port when needed. If the port cannot be re-aquired ehen the exception PortInUseException will be thrown.
| portName | Address to connect this NetAdapter to, in the form of "hostname:port". For example, "shughes.dalsemi.com:6161", where 6161 is the port number to connect to. The use of NetAdapter.DEFAULT_PORT is recommended. |
true if the port was aquired, false if the port is not available.| OneWireIOException | If port does not exist, or unable to communicate with port. |
| OneWireException | If port does not exist |
Implements DSPortAdapter.
| void setNoResetSearch | ( | ) | [virtual] |
Sets the 1-Wire Network search to not perform a 1-Wire reset before a search.
This feature is chiefly used with the DS2409 1-Wire coupler. The normal reset before each search can be restored with the 'setSearchAllDevices()' method.
Implements DSPortAdapter.
| void setPowerDuration | ( | int | timeFactor | ) | throws OneWireIOException, OneWireException |
Sets the duration to supply power to the 1-Wire Network.
This method takes a time parameter that indicates the program pulse length when the method startPowerDelivery().
Note: to avoid getting an exception, use the canDeliverPower() and canDeliverSmartPower() method to check it's availability.
| timeFactor |
|
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| void setPowerNormal | ( | ) | throws OneWireIOException, OneWireException |
Sets the 1-Wire Network voltage to normal level.
This method is used to disable 1-Wire conditions created by startPowerDelivery and startProgramPulse. This method will automatically be called if a communication method is called while an outstanding power command is taking place.
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter or the adapter does not support this operation |
Reimplemented from DSPortAdapter.
| void setProgramPulseDuration | ( | int | timeFactor | ) | throws OneWireIOException, OneWireException |
Sets the duration for providing a program pulse on the 1-Wire Network.
This method takes a time parameter that indicates the program pulse length when the method startProgramPulse().
Note: to avoid getting an exception, use the canDeliverPower() method to check it's availability.
| timeFactor |
|
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| void setSearchAllDevices | ( | ) | [virtual] |
Sets the 1-Wire Network search to find all iButtons and 1-Wire devices whether they are in an 'Alarm' state or not and restores the default setting of providing a 1-Wire reset command before each search.
(see setNoResetSearch() method).
Implements DSPortAdapter.
| void setSearchOnlyAlarmingDevices | ( | ) | [virtual] |
Sets the 1-Wire Network search to find only iButtons and 1-Wire devices that are in an 'Alarm' state that signals a need for attention.
Not all iButton types have this feature. Some that do: DS1994, DS1920, DS2407. This selective searching can be canceled with the 'setSearchAllDevices()' method.
Implements DSPortAdapter.
| void setSecret | ( | String | secret | ) |
Sets the shared secret for authenticating this NetAdapter with a NetAdapterHost.
| secret | the new secret for authenticating this client. |
| void setSpeed | ( | int | speed | ) | throws OneWireIOException, OneWireException |
Sets the new speed of data transfer on the 1-Wire Network.
| speed |
|
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter or the adapter does not support this operation |
Reimplemented from DSPortAdapter.
| void startBreak | ( | ) | throws OneWireIOException, OneWireException |
Sets the 1-Wire Network voltage to 0 volts.
This method is used rob all 1-Wire Network devices of parasite power delivery to force them into a hard reset.
| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter or the adapter does not support this operation |
Reimplemented from DSPortAdapter.
| boolean startPowerDelivery | ( | int | changeCondition | ) | throws OneWireIOException, OneWireException |
Sets the 1-Wire Network voltage to supply power to a 1-Wire device.
This method takes a time parameter that indicates whether the power delivery should be done immediately, or after certain conditions have been met.
Note: to avoid getting an exception, use the canDeliverPower() and canDeliverSmartPower() method to check it's availability.
| changeCondition |
|
true if the voltage change was successful, false otherwise.| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter |
Reimplemented from DSPortAdapter.
| boolean startProgramPulse | ( | int | changeCondition | ) | throws OneWireIOException, OneWireException |
Sets the 1-Wire Network voltage to eprom programming level.
This method takes a time parameter that indicates whether the power delivery should be done immediately, or after certain conditions have been met.
Note: to avoid getting an exception, use the canProgram() method to check it's availability.
| changeCondition |
|
true if the voltage change was successful, false otherwise.| OneWireIOException | on a 1-Wire communication error |
| OneWireException | on a setup error with the 1-Wire adapter or the adapter does not support this operation |
Reimplemented from DSPortAdapter.
| void targetAllFamilies | ( | ) |
Removes any selectivity during a search for iButtons or 1-Wire devices by family type.
The unique address for each iButton and 1-Wire device contains a family descriptor that indicates the capabilities of the device.
Reimplemented from DSPortAdapter.
| void targetFamily | ( | byte | family[] | ) |
Takes an array of bytes to use for selectively searching for acceptable family codes.
If used, only devices with family codes in this array will be found by any of the search methods.
| family | array of the family types to target for searches |
Reimplemented from DSPortAdapter.
| void targetFamily | ( | int | family | ) |
Takes an integer to selectively search for this desired family type.
If this method is used, then no devices of other families will be found by any of the search methods.
| family | the code of the family type to target for searches |
Reimplemented from DSPortAdapter.
1.7.3