|
1-Wire API for .NET Version 4.00
|
| AbstractDeviceMonitor | |
| ADContainer | |
| Address | Utilities to translate and verify the 1-Wire Network address |
| Bit | Utilities for bit operations on an array |
| ChainMonitor | |
| ClockContainer | |
| Contact | This class provides a default object for the Contact type of a tagged 1-Wire device |
| Convert | Utilities for conversion between miscellaneous datatypes |
| CRC16 | CRC16 is a class containing an implementation of the Cyclic-Redundency-Check (CRC) CRC16 |
| CRC8 | CRC8 is a class to contain an implementation of the Cyclic-Redundency-Check CRC8 for the iButton |
| D2A | This class provides a default object for the D2A type of a tagged 1-Wire device |
| Debug | |
| DeviceMonitor | |
| DeviceMonitorEvent | Represents a group of 1-Wire addresses that have either arrived to or departed from the 1-Wire network |
| DeviceMonitorEventListener | Interface for classes which will listen to device monitor events such as arrivals, departures, and network exceptions |
| DeviceMonitorException | Represents an encapsulated exception from a particular Device Monitor |
| DotNetAdapterx64 | The DSPortAdapter class for all DotNet native adapters for x64 Windows |
| DotNetAdapterx86 | The DSPortAdapterx86 class for all DotNet native adapters (Win32) |
| DSPortAdapter | The abstract base class for all 1-Wire port adapter objects |
| DumbAdapter | |
| Event | This class provides a default object for the Event type of a tagged 1-Wire device |
| Humidity | This class provides a default object for the Humidity type of a tagged 1-Wire device |
| HumidityContainer | 1-Wire Humidity interface class for basic Humidity measuring operations |
| IOHelper | Generic IO routines |
| Level | This class provides a default object for the Level type of a tagged 1-Wire device |
| MemoryBank | |
| MemoryBankAD | Memory bank class for the DS2450 |
| MemoryBankAppReg | Memory bank class for the EPROM section of iButtons and 1-Wire devices |
| MemoryBankEE | Memory bank class for the DS1971/DS2430 |
| MemoryBankEEPROM | Memory bank class for the EEPROM section of iButtons and 1-Wire devices on the DS2431 |
| MemoryBankEEPROMblock | Memory bank class for the EEPROM section of iButtons and 1-Wire devices on the DS2408 |
| MemoryBankEEPROMstatus | Memory bank class for the EEPROM section of iButtons and 1-Wire devices on the DS2408 |
| MemoryBankEPROM | Memory bank class for the EPROM section of iButtons and 1-Wire devices |
| MemoryBankNV | Memory bank class for the NVRAM section of iButtons and 1-Wire devices |
| MemoryBankNVCRC | Memory bank class for the NVRAM with build in CRC section of iButtons and 1-Wire devices |
| MemoryBankNVCRCPW | Memory bank class for the NVRAM with built-in CRC generation and Password protected memory read/write iButtons and 1-Wire Devices |
| MemoryBankSBM | Memory bank class for the DS2438 |
| MemoryBankScratch | Memory bank class for the Scratchpad section of NVRAM iButtons and 1-Wire devices |
| MemoryBankScratchCRC | Memory bank class for the Scratchpad section of NVRAM iButtons and 1-Wire devices |
| MemoryBankScratchCRCPW | Memory bank class for the Scratchpad section of NVRAM iButtons and 1-Wire devices with password protected memory pages |
| MemoryBankScratchEE | Memory bank class for the Scratchpad section of EEPROM iButtons and 1-Wire devices |
| MemoryBankScratchEx | Memory bank class for the Scratchpad section of NVRAM iButtons and 1-Wire devices |
| MemoryBankScratchSHA | Memory bank class for the Scratchpad section of SHA iButtons and 1-Wire devices |
| MemoryBankScratchSHAEE | Memory bank class for the Scratchpad section of SHA EEPROM iButtons and 1-Wire devices with SHA write-protected memory pages |
| MemoryBankScratchTemp | Memory bank class for the DS28EA00 |
| MemoryBankSHAEE | Memory bank class for the DS1961S/DS2432 |
| MemoryCache | Class to provide read/write cache services to a 1-Wire memory device |
| MissionContainer | |
| MulticastListener | Generic Mulitcast broadcast listener |
| NetAdapter | |
| NetAdapterConstants | Interface for holding all constants related to Network Adapter communications |
| NetAdapterHost | |
| NetAdapterSim | |
| NetworkDeviceMonitor | Class NetworkDeviceMonitor represents the monitor that searches the 1-Wire net, including the traversal of branches, looing for new arrivals and departures |
| OneWireAccessProvider | Manages the Maxim adapter class derivatives of DSPortAdapter |
| OneWireContainer | A OneWireContainer encapsulates the DSPortAdapter, the 1-Wire® network address, and methods to manipulate a specific 1-Wire device |
| OneWireContainer01 | |
| OneWireContainer02 | |
| OneWireContainer04 | |
| OneWireContainer05 | |
| OneWireContainer06 | |
| OneWireContainer08 | |
| OneWireContainer09 | |
| OneWireContainer0A | |
| OneWireContainer0B | |
| OneWireContainer0C | |
| OneWireContainer0F | |
| OneWireContainer10 | |
| OneWireContainer12 | |
| OneWireContainer13 | |
| OneWireContainer14 | |
| OneWireContainer18 | |
| OneWireContainer1A | |
| OneWireContainer1C | |
| OneWireContainer1D | |
| OneWireContainer1F | |
| OneWireContainer20 | |
| OneWireContainer21 | |
| OneWireContainer22 | |
| OneWireContainer23 | |
| OneWireContainer24 | |
| OneWireContainer27 | |
| OneWireContainer28 | |
| OneWireContainer29 | |
| OneWireContainer2C | |
| OneWireContainer2D | |
| OneWireContainer30 | |
| OneWireContainer33 | |
| OneWireContainer37 | |
| OneWireContainer3A | |
| OneWireContainer41 | |
| OneWireContainer42 | |
| OneWireContainer43 | |
| OneWireException | This is the general exception thrown by the iButton and 1-Wire operations |
| OneWireIOException | This exception is thrown when there is an IO error communicating on on the 1-Wire Network |
| OneWireSensor | |
| OTPMemoryBank | |
| OWFile | An abstract representation of file and directory pathnames on 1-Wire devices |
| OWFileDescriptor | Instances of the 1-Wire file descriptor class serve as an opaque handle to the underlying machine-specific structure representing an open file, an open socket, or another source or sink of bytes |
| OWFileInputStream | A OWFileInputStream obtains input bytes from a file in a 1-Wire Filesystem |
| OWFileNotFoundException | |
| OWFileOutputStream | A 1-Wire file output stream is an output stream for writing data to a OWFile or to a OWFileDescriptor |
| OWPath | 1-Wire® Network path |
| OWPathElement | 1-Wire® Network path element |
| OWSyncFailedException | Represents a failed 1-Wire memory sync operation |
| PagedMemoryBank | |
| PasswordContainer | Public interface for all devices which implement some form of password protection |
| PotentiometerContainer | 1-Wire® Potentiometer interface class for basic potentiometer operations |
| SAXParser | |
| ScratchPad | Scratchpad interface for Memory banks that require it |
| SHA | Utility methods for performing SHA calculations |
| SHADebit | |
| SHADebitUnsigned | |
| SHAiButtonCopr | |
| SHAiButtonCoprVM | |
| SHAiButtonUser | |
| SHAiButtonUser18 | |
| SHAiButtonUser33 | |
| SHASoftAuth | |
| SHATransaction | |
| Switch | This class provides a default object for the Switch type of a tagged 1-Wire device |
| SwitchContainer | |
| TaggedDevice | This class provides a default object for a tagged 1-Wire device |
| TAGHandler | SAX parser handler that handles XML 1-wire tags |
| TAGParser | The tag parser parses tagging information |
| TemperatureContainer | 1-Wire temperature interface class for basic temperature measuring operations |
| Thermal | This class provides a default object for the Thermal type of a tagged 1-Wire device |
| XML | XML services |
1.7.3