|
1-Wire API for Compact.NET Version 4.00
|
The OVERLAPPED structure contains information used in asynchronous I/O. More...
Public Attributes | |
| internal UIntPtr | internalLow |
| Reserved for operating system use. | |
| internal UIntPtr | internalHigh |
| Reserved for operating system use. | |
| internal UInt32 | offset |
| Specifies a file position at which to start the transfer. | |
| internal UInt32 | offsetHigh |
| Specifies the high word of the byte offset at which to start the transfer. | |
| internal IntPtr | hEvent |
| Handle to an event set to the signaled state when the operation has been completed. | |
The OVERLAPPED structure contains information used in asynchronous I/O.
| internal IntPtr hEvent |
Handle to an event set to the signaled state when the operation has been completed.
The calling process must set this member either to zero or a valid event handle before calling any overlapped functions. To create an event object, use the CreateEvent function. Functions such as WriteFile set the event to the nonsignaled state before they begin an I/O operation.
| internal UInt32 offset |
Specifies a file position at which to start the transfer.
The file position is a byte offset from the start of the file. The calling process sets this member before calling the ReadFile or WriteFile function. This member is ignored when reading from or writing to named pipes and communications devices and should be zero.
| internal UInt32 offsetHigh |
Specifies the high word of the byte offset at which to start the transfer.
This member is ignored when reading from or writing to named pipes and communications devices and should be zero.
1.7.3