|
1-Wire API for Compact.NET Version 4.00
|
UParameterSettings contains the parameter settings state for one speed on the DS2480 based iButton COM port adapter. More...
Public Member Functions | |
| UParameterSettings (SlewRate sr, ProgramPulseTime12 ppt12, ProgramPulseTime5 ppt5, WriteOneLowTime wolt, SampleOffsetTime sot) | |
| Parameter Settings constructor. | |
Public Attributes | |
| SlewRate | pullDownSlewRate |
| The pull down slew rate for this mode. | |
| ProgramPulseTime12 | pulse12VoltTime |
| 12 Volt programming pulse time expressed in micro-seconds. | |
| ProgramPulseTime5 | pulse5VoltTime |
| 5 Volt programming pulse time expressed in milli-seconds. | |
| WriteOneLowTime | write1LowTime |
| Write 1 low time expressed in micro-seconds. | |
| SampleOffsetTime | sampleOffsetTime |
| Data sample offset and write 0 recovery time expressed in micro-seconds. | |
UParameterSettings contains the parameter settings state for one speed on the DS2480 based iButton COM port adapter.
<version>0.00</version> <author>DS, SH</author>
| UParameterSettings | ( | SlewRate | sr, |
| ProgramPulseTime12 | ppt12, | ||
| ProgramPulseTime5 | ppt5, | ||
| WriteOneLowTime | wolt, | ||
| SampleOffsetTime | sot | ||
| ) |
Parameter Settings constructor.
| SlewRate pullDownSlewRate |
The pull down slew rate for this mode.
| ProgramPulseTime12 pulse12VoltTime |
12 Volt programming pulse time expressed in micro-seconds.
| ProgramPulseTime5 pulse5VoltTime |
5 Volt programming pulse time expressed in milli-seconds.
| SampleOffsetTime sampleOffsetTime |
Data sample offset and write 0 recovery time expressed in micro-seconds.
| WriteOneLowTime write1LowTime |
Write 1 low time expressed in micro-seconds.
1.7.3