|
1-Wire API for Compact.NET Version 4.00
|
UAdapterState contains the communication state of the DS2480 based COM port adapter. More...
Public Member Functions | |
| UAdapterState (OneWireState newOneWireState) | |
| Construct the state of the U brick with the defaults. | |
Public Attributes | |
| const byte | USPEED_REGULAR = (byte)(0x00) |
| DS9097U speed mode, regular speed. | |
| const byte | USPEED_FLEX = (byte)(0x04) |
| DS9097U speed mode, flexible speed for long lines. | |
| const byte | USPEED_OVERDRIVE = (byte)(0x08) |
| DS9097U speed mode, overdrive speed. | |
| const byte | USPEED_PULSE = (byte)(0x0C) |
| DS9097U speed mode, pulse, for program and power delivery. | |
| const byte | MODE_DATA = (byte)(0x00E1) |
| DS9097U data mode. | |
| const byte | MODE_COMMAND = (byte)(0x00E3) |
| DS9097U command mode. | |
| const byte | MODE_STOP_PULSE = (byte)(0x00F1) |
| DS9097U pulse mode. | |
| const byte | MODE_SPECIAL = (byte)(0x00F3) |
| DS9097U special mode (in revision 1 silicon only) | |
| const byte | CHIP_VERSION1 = (byte)(0x04) |
| DS9097U chip revision 1. | |
| const byte | CHIP_VERSION_MASK = (byte)(0x1C) |
| DS9097U chip revision mask. | |
| const byte | PROGRAM_VOLTAGE_MASK = (byte)(0x20) |
| DS9097U program voltage available mask. | |
| const int | MAX_ALARM_COUNT = 3000 |
| Maximum number of alarms. | |
| UParameterSettings[] | uParameters |
| Parameter settings for the three logical modes. | |
| OneWireState | oneWireState |
| The OneWire State object reference. | |
| bool | streamBits |
| Flag true if can stream bits. | |
| bool | streamBytes |
| Flag true if can stream bytes. | |
| bool | streamSearches |
| Flag true if can stream Search. | |
| bool | streamResets |
| Flag true if can stream resets. | |
| AdapterBaud | ubaud |
| Current baud rate that we are communicating with the DS9097U expressed for the DS2480 ichip. | |
| byte | uSpeedMode |
| This is the current 'real' speed that the OneWire is operating at. | |
| bool | programVoltageAvailable |
| This is the current state of the DS2480 adapter on program voltage availablity. | |
| bool | inCommandMode |
| True when DS2480 is currently in command mode. | |
| byte | revision |
| The DS2480 revision number. The current value values are 1 and 2. | |
Protected Attributes | |
| internal bool | longAlarmCheck |
| Flag to indicate need to Search for long alarm check. | |
| internal int | lastAlarmCount |
| Count of how many resets have been seen without Alarms. | |
UAdapterState contains the communication state of the DS2480 based COM port adapter.
\//\ This class is very preliminary and not all functionality is complete or debugged. This class is subject to change. //\//\
<version>0.00</version> <author>DS, SH</author>
| UAdapterState | ( | OneWireState | newOneWireState | ) |
Construct the state of the U brick with the defaults.
| const byte CHIP_VERSION1 = (byte)(0x04) |
DS9097U chip revision 1.
| const byte CHIP_VERSION_MASK = (byte)(0x1C) |
DS9097U chip revision mask.
| bool inCommandMode |
True when DS2480 is currently in command mode.
False when it is in data mode.
internal int lastAlarmCount [protected] |
Count of how many resets have been seen without Alarms.
internal bool longAlarmCheck [protected] |
Flag to indicate need to Search for long alarm check.
| const int MAX_ALARM_COUNT = 3000 |
Maximum number of alarms.
| const byte MODE_COMMAND = (byte)(0x00E3) |
DS9097U command mode.
| const byte MODE_DATA = (byte)(0x00E1) |
DS9097U data mode.
| const byte MODE_SPECIAL = (byte)(0x00F3) |
DS9097U special mode (in revision 1 silicon only)
| const byte MODE_STOP_PULSE = (byte)(0x00F1) |
DS9097U pulse mode.
The OneWire State object reference.
| const byte PROGRAM_VOLTAGE_MASK = (byte)(0x20) |
DS9097U program voltage available mask.
This is the current state of the DS2480 adapter on program voltage availablity.
'true' if available.
| byte revision |
The DS2480 revision number. The current value values are 1 and 2.
| bool streamBits |
Flag true if can stream bits.
| bool streamBytes |
Flag true if can stream bytes.
| bool streamResets |
Flag true if can stream resets.
| bool streamSearches |
Flag true if can stream Search.
| AdapterBaud ubaud |
Current baud rate that we are communicating with the DS9097U expressed for the DS2480 ichip.
Valid values can be:
Parameter settings for the three logical modes.
| const byte USPEED_FLEX = (byte)(0x04) |
DS9097U speed mode, flexible speed for long lines.
| const byte USPEED_OVERDRIVE = (byte)(0x08) |
DS9097U speed mode, overdrive speed.
| const byte USPEED_PULSE = (byte)(0x0C) |
DS9097U speed mode, pulse, for program and power delivery.
| const byte USPEED_REGULAR = (byte)(0x00) |
DS9097U speed mode, regular speed.
| byte uSpeedMode |
This is the current 'real' speed that the OneWire is operating at.
This is used to represent the actual mode that the DS2480 is operting in. For example the logical speed might be USPEED_REGULAR but for RF emission reasons we may put the actual DS2480 in OWSpeed.SPEED_FLEX.
The valid values for this are:
1.7.3