This file gives details on setting up help for the Elves application.

Start the Elves application and then push the Setup button. 
In the resulting window  enter the full path, name and extension 
of the browser you wish to use. Most browsers should work.

Enter the Help Path to where the help files are to be found. 
If you do not know where they are then try searching for the file 
AO_P.html and use its path.  Alternatively the help files may be in a 
folder ElvesHelp.exe as a compressed self-extracting file and its 
path may be selected.  In this case the extraction process will be 
started automatically when the Help button is pushed the first time. 
This file may include help files for other ADuC7xxx applications. 

The help files might be in the current folder and this path will be
chosen by default.  When specifying paths include a trailing backslash.

Ensure the Details radio button is checked to get the selected help 
instead of this file.

Exit Setup by clicking on the OK button