| Functions |
Context
|
The following lists the presently defined function abbreviations.
| Bsy | Check for busy |
|---|---|
| Cfg | Configure |
| Clr | Clear |
| Get | Get a result which was started previously |
| Go | Start an action |
| Idl | Check for idle |
| Rd | Read |
| Set | Set |
| Sta | Status |
| Wr | Write |
For function names the leading character must be capital and the other characters lower case. File names should use the same cases although Windows messes this up. MMR names use all 3 characters upper case.
Further abbreviations will need to be defined as required, but do not invent new ones if one from the list is appropriate.