![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2983: Multi-Sensor High Accuracy Digital Temperature Measurement System. More...
LTC2983: Multi-Sensor High Accuracy Digital Temperature Measurement System.
support_functions_LTC2983.h: This file contains all the support function prototypes used in the main program.
http://www.linear.com/product/LTC2983
http://www.linear.com/product/LTC2983#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2983: Multi-Sensor High Accuracy Digital Temperature Measurement System
Definition in file support_functions_LTC2983.h.
Go to the source code of this file.
Functions | |
| void | print_title () |
| Prints the title block when program first starts. More... | |
| void | assign_channel (uint8_t chip_select, uint8_t channel_number, uint32_t channel_assignment_data) |
| void | write_custom_table (uint8_t chip_select, struct table_coeffs coefficients[64], uint16_t start_address, uint8_t table_length) |
| void | write_custom_steinhart_hart (uint8_t chip_select, uint32_t steinhart_hart_coeffs[6], uint16_t start_address) |
| void | measure_channel (uint8_t chip_select, uint8_t channel_number, uint8_t channel_output) |
| void | convert_channel (uint8_t chip_select, uint8_t channel_number) |
| void | wait_for_process_to_finish (uint8_t chip_select) |
| void | get_result (uint8_t chip_select, uint8_t channel_number, uint8_t channel_output) |
| void | print_conversion_result (uint32_t raw_conversion_result, uint8_t channel_output) |
| void | read_voltage_or_resistance_results (uint8_t chip_select, uint8_t channel_number) |
| void | print_fault_data (uint8_t fault_byte) |
| uint32_t | transfer_four_bytes (uint8_t chip_select, uint8_t read_or_write, uint16_t start_address, uint32_t input_data) |
| uint8_t | transfer_byte (uint8_t chip_select, uint8_t read_or_write, uint16_t start_address, uint8_t input_data) |
| uint16_t | get_start_address (uint16_t base_address, uint8_t channel_number) |
| bool | is_number_in_array (uint8_t number, uint8_t *array, uint8_t array_length) |
| void assign_channel | ( | uint8_t | chip_select, |
| uint8_t | channel_number, | ||
| uint32_t | channel_assignment_data | ||
| ) |
Definition at line 90 of file support_functions_LTC2983.cpp.
| void convert_channel | ( | uint8_t | chip_select, |
| uint8_t | channel_number | ||
| ) |
Definition at line 159 of file support_functions_LTC2983.cpp.
| void get_result | ( | uint8_t | chip_select, |
| uint8_t | channel_number, | ||
| uint8_t | channel_output | ||
| ) |
Definition at line 183 of file support_functions_LTC2983.cpp.
| uint16_t get_start_address | ( | uint16_t | base_address, |
| uint8_t | channel_number | ||
| ) |
Definition at line 324 of file support_functions_LTC2983.cpp.
| bool is_number_in_array | ( | uint8_t | number, |
| uint8_t * | array, | ||
| uint8_t | array_length | ||
| ) |
Definition at line 330 of file support_functions_LTC2983.cpp.
| void measure_channel | ( | uint8_t | chip_select, |
| uint8_t | channel_number, | ||
| uint8_t | channel_output | ||
| ) |
Definition at line 152 of file support_functions_LTC2983.cpp.
| void print_conversion_result | ( | uint32_t | raw_conversion_result, |
| uint8_t | channel_output | ||
| ) |
Definition at line 211 of file support_functions_LTC2983.cpp.
| void print_fault_data | ( | uint8_t | fault_byte | ) |
Definition at line 251 of file support_functions_LTC2983.cpp.
| void print_title | ( | void | ) |
Prints the title block when program first starts.
Print the title block.
Prints the title block.
Prints the title block when the program first starts.
Definition at line 75 of file support_functions_LTC2983.cpp.
| void read_voltage_or_resistance_results | ( | uint8_t | chip_select, |
| uint8_t | channel_number | ||
| ) |
Definition at line 237 of file support_functions_LTC2983.cpp.
| uint8_t transfer_byte | ( | uint8_t | chip_select, |
| uint8_t | read_or_write, | ||
| uint16_t | start_address, | ||
| uint8_t | input_data | ||
| ) |
Definition at line 308 of file support_functions_LTC2983.cpp.
| uint32_t transfer_four_bytes | ( | uint8_t | chip_select, |
| uint8_t | read_or_write, | ||
| uint16_t | start_address, | ||
| uint32_t | input_data | ||
| ) |
Definition at line 284 of file support_functions_LTC2983.cpp.
| void wait_for_process_to_finish | ( | uint8_t | chip_select | ) |
Definition at line 168 of file support_functions_LTC2983.cpp.
| void write_custom_steinhart_hart | ( | uint8_t | chip_select, |
| uint32_t | steinhart_hart_coeffs[6], | ||
| uint16_t | start_address | ||
| ) |
Definition at line 124 of file support_functions_LTC2983.cpp.
| void write_custom_table | ( | uint8_t | chip_select, |
| struct table_coeffs | coefficients[64], | ||
| uint16_t | start_address, | ||
| uint8_t | table_length | ||
| ) |
Definition at line 97 of file support_functions_LTC2983.cpp.