Register configuration structure.
More...
Register configuration structure.
Definition at line 159 of file LTC681x.h.
◆ aux_channels
| uint8_t register_cfg::aux_channels |
Number of Aux channels.
Definition at line 163 of file LTC681x.h.
◆ cell_channels
| uint8_t register_cfg::cell_channels |
Number of Cell channels.
Definition at line 161 of file LTC681x.h.
◆ num_cv_reg
| uint8_t register_cfg::num_cv_reg |
Number of Cell voltage register.
Definition at line 164 of file LTC681x.h.
◆ num_gpio_reg
| uint8_t register_cfg::num_gpio_reg |
Number of Aux register.
Definition at line 165 of file LTC681x.h.
◆ num_stat_reg
| uint8_t register_cfg::num_stat_reg |
Number of Status register.
Definition at line 166 of file LTC681x.h.
◆ stat_channels
| uint8_t register_cfg::stat_channels |
Number of Stat channels.
Definition at line 162 of file LTC681x.h.
The documentation for this struct was generated from the following file: