PEC error counter structure.
More...
PEC error counter structure.
Definition at line 149 of file LTC681x.h.
◆ aux_pec
| uint16_t pec_counter::aux_pec[4] |
Aux register data PEC error count.
Definition at line 154 of file LTC681x.h.
◆ cell_pec
| uint16_t pec_counter::cell_pec[6] |
Cell voltage register data PEC error count.
Definition at line 153 of file LTC681x.h.
◆ cfgr_pec
| uint16_t pec_counter::cfgr_pec |
Configuration register data PEC error count.
Definition at line 152 of file LTC681x.h.
◆ pec_count
| uint16_t pec_counter::pec_count |
Overall PEC error count.
Definition at line 151 of file LTC681x.h.
◆ stat_pec
| uint16_t pec_counter::stat_pec[2] |
Status register data PEC error count.
Definition at line 155 of file LTC681x.h.
The documentation for this struct was generated from the following file: