This struct holds all of the calibration data, i.e. offset integers, LSB floats, etc. The eeprom_data_union contains a byte_array that is used to write and read this data to/from the EEPROM.
More...
This struct holds all of the calibration data, i.e. offset integers, LSB floats, etc. The eeprom_data_union contains a byte_array that is used to write and read this data to/from the EEPROM.
Definition at line 294 of file EasySMU.h.
◆ cal_key
| int16_t EasySMU::eeprom_data_union::data_struct_type::cal_key |
If this is set to the proper value, it indicates that a calibration has been performed.
(If not, this EasySMU has never been calibrated.)
Definition at line 296 of file EasySMU.h.
◆ current_measure_LSB
| float EasySMU::eeprom_data_union::data_struct_type::current_measure_LSB |
the current of one LSB in amps from the current ADC
Definition at line 306 of file EasySMU.h.
◆ current_measure_offset
| int32_t EasySMU::eeprom_data_union::data_struct_type::current_measure_offset |
the code from the current ADC that corresponds to 0A at the output
Definition at line 308 of file EasySMU.h.
◆ current_measure_output_resistance
| float EasySMU::eeprom_data_union::data_struct_type::current_measure_output_resistance |
This value is used to modify the output current measurement result based on output voltage.
This compensates for the current that flows through the feedback network, etc.
Definition at line 307 of file EasySMU.h.
◆ current_source_pulldown_LSB
| float EasySMU::eeprom_data_union::data_struct_type::current_source_pulldown_LSB |
the current of one LSB in amps from the current pulldown DAC channel
Definition at line 303 of file EasySMU.h.
◆ current_source_pulldown_offset
| int16_t EasySMU::eeprom_data_union::data_struct_type::current_source_pulldown_offset |
current DAC code that ideally would result in 0A at output, if the output current could be configured below 0.5mA
Definition at line 302 of file EasySMU.h.
◆ current_source_pullup_LSB
| float EasySMU::eeprom_data_union::data_struct_type::current_source_pullup_LSB |
the current of one LSB in amps from the current pullup DAC channel
Definition at line 301 of file EasySMU.h.
◆ current_source_pullup_offset
| int16_t EasySMU::eeprom_data_union::data_struct_type::current_source_pullup_offset |
current DAC code that ideally would result in 0A at output, if the output current could be configured below 0.5mA
Definition at line 300 of file EasySMU.h.
◆ temperature_Iadc_code
| int32_t EasySMU::eeprom_data_union::data_struct_type::temperature_Iadc_code |
This is the temperature code read from the current ADC during calibration.
(It is probably 25C, but an actual measurement/calibration is not performed.)
Definition at line 310 of file EasySMU.h.
◆ temperature_Vadc_code
| int32_t EasySMU::eeprom_data_union::data_struct_type::temperature_Vadc_code |
This is the temperature code read from the voltage ADC during calibration.
(It is probably 25C, but an actual measurement/calibration is not performed.)
Definition at line 309 of file EasySMU.h.
◆ voltage_measure_LSB
| float EasySMU::eeprom_data_union::data_struct_type::voltage_measure_LSB |
the voltage of one LSB in volts from the voltage ADC
Definition at line 305 of file EasySMU.h.
◆ voltage_measure_offset
| int32_t EasySMU::eeprom_data_union::data_struct_type::voltage_measure_offset |
the voltage ADC code that corresponds to 0V at the output
Definition at line 304 of file EasySMU.h.
◆ voltage_source_LSB
| float EasySMU::eeprom_data_union::data_struct_type::voltage_source_LSB |
the voltage of one LSB in volts (from the voltage channel of the DAC)
Definition at line 299 of file EasySMU.h.
◆ voltage_source_offset
| int16_t EasySMU::eeprom_data_union::data_struct_type::voltage_source_offset |
The output voltage is 0V when this code is stored in the voltage channel of the DAC.
Definition at line 298 of file EasySMU.h.
The documentation for this struct was generated from the following file: