![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Go to the source code of this file.
Functions | |
| static void | drawFrame () |
| static void | redBtn () |
| static void | greenBtn () |
| static void | setup (void) |
| static void | loop () |
Macros | |
| #define | YP A3 |
| #define | XM A2 |
| #define | YM 5 |
| #define | XP 4 |
| #define | TS_MINX 150 |
| #define | TS_MINY 120 |
| #define | TS_MAXX 920 |
| #define | TS_MAXY 940 |
| #define | MINPRESSURE 10 |
| #define | MAXPRESSURE 1000 |
| #define | TFT_CS 10 |
| #define | TFT_DC 9 |
| #define | FRAME_X 210 |
| #define | FRAME_Y 180 |
| #define | FRAME_W 100 |
| #define | FRAME_H 50 |
| #define | REDBUTTON_X FRAME_X |
| #define | REDBUTTON_Y FRAME_Y |
| #define | REDBUTTON_W (FRAME_W/2) |
| #define | REDBUTTON_H FRAME_H |
| #define | GREENBUTTON_X (REDBUTTON_X + REDBUTTON_W) |
| #define | GREENBUTTON_Y FRAME_Y |
| #define | GREENBUTTON_W (FRAME_W/2) |
| #define | GREENBUTTON_H FRAME_H |
Variables | |
| TouchScreen | ts = TouchScreen(XP, YP, XM, YM, 300) |
| Adafruit_ILI9341 | tft = Adafruit_ILI9341(TFT_CS, TFT_DC) |
| boolean | RecordOn = false |
|
static |
Definition at line 54 of file onoffbutton_breakout.ino.
|
static |
Definition at line 71 of file onoffbutton_breakout.ino.
|
static |
Definition at line 94 of file onoffbutton_breakout.ino.
|
static |
Definition at line 59 of file onoffbutton_breakout.ino.
|
static |
Definition at line 83 of file onoffbutton_breakout.ino.
| #define FRAME_H 50 |
Definition at line 42 of file onoffbutton_breakout.ino.
| #define FRAME_W 100 |
Definition at line 41 of file onoffbutton_breakout.ino.
| #define FRAME_X 210 |
Definition at line 39 of file onoffbutton_breakout.ino.
| #define FRAME_Y 180 |
Definition at line 40 of file onoffbutton_breakout.ino.
| #define GREENBUTTON_H FRAME_H |
Definition at line 52 of file onoffbutton_breakout.ino.
| #define GREENBUTTON_W (FRAME_W/2) |
Definition at line 51 of file onoffbutton_breakout.ino.
| #define GREENBUTTON_X (REDBUTTON_X + REDBUTTON_W) |
Definition at line 49 of file onoffbutton_breakout.ino.
| #define GREENBUTTON_Y FRAME_Y |
Definition at line 50 of file onoffbutton_breakout.ino.
| #define MAXPRESSURE 1000 |
Definition at line 25 of file onoffbutton_breakout.ino.
| #define MINPRESSURE 10 |
Definition at line 24 of file onoffbutton_breakout.ino.
| #define REDBUTTON_H FRAME_H |
Definition at line 47 of file onoffbutton_breakout.ino.
| #define REDBUTTON_W (FRAME_W/2) |
Definition at line 46 of file onoffbutton_breakout.ino.
| #define REDBUTTON_X FRAME_X |
Definition at line 44 of file onoffbutton_breakout.ino.
| #define REDBUTTON_Y FRAME_Y |
Definition at line 45 of file onoffbutton_breakout.ino.
| #define TFT_CS 10 |
Definition at line 33 of file onoffbutton_breakout.ino.
| #define TFT_DC 9 |
Definition at line 34 of file onoffbutton_breakout.ino.
| #define TS_MAXX 920 |
Definition at line 21 of file onoffbutton_breakout.ino.
| #define TS_MAXY 940 |
Definition at line 22 of file onoffbutton_breakout.ino.
| #define TS_MINX 150 |
Definition at line 19 of file onoffbutton_breakout.ino.
| #define TS_MINY 120 |
Definition at line 20 of file onoffbutton_breakout.ino.
| #define XM A2 |
Definition at line 14 of file onoffbutton_breakout.ino.
| #define XP 4 |
Definition at line 16 of file onoffbutton_breakout.ino.
| #define YM 5 |
Definition at line 15 of file onoffbutton_breakout.ino.
| #define YP A3 |
Definition at line 13 of file onoffbutton_breakout.ino.
| boolean RecordOn = false |
Definition at line 37 of file onoffbutton_breakout.ino.
| Adafruit_ILI9341 tft = Adafruit_ILI9341(TFT_CS, TFT_DC) |
Definition at line 35 of file onoffbutton_breakout.ino.
| TouchScreen ts = TouchScreen(XP, YP, XM, YM, 300) |
Definition at line 30 of file onoffbutton_breakout.ino.