![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library File. More...
Library File.
Definition in file nvm.cpp.
Go to the source code of this file.
Functions | |
| uint8_t | get_hex_data (void) |
| uint8_t | get_filtered_hex_data (void) |
| uint8_t | get_record_data (void) |
| pRecordHeaderLengthAndType | get_record (void) |
Macros | |
| #define | DEBUG_FLASH 0 |
Variables | |
| const unsigned char * | icpFile |
| uint32_t | flashLocation = 0 |
| LT_SMBusNoPec * | smbusNoPec__ |
| LT_SMBusPec * | smbusPec__ |
| pRecordHeaderLengthAndType get_record | ( | void | ) |
| LT_SMBusNoPec* smbusNoPec__ |
| LT_SMBusPec* smbusPec__ |