![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Copyright 2018(c) Analog Devices, Inc. More...
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Library File
Definition in file main_record_processor.cpp.
Go to the source code of this file.
Macros | |
| #define | DEBUG_SILENT 0 |
| #define | DEBUG_PROCESSING 0 |
| #define | DEBUG_PRINT 0 |
Variables | |
| static bool | verification_in_progress = false |
| VARIABLES. More... | |
| static bool | ignore_records = false |
| uint8_t processRecordsOnDemand | ( | pRecordHeaderLengthAndType(*)(void) | getRecord | ) |
Definition at line 91 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x01___processWriteByteOptionalPEC | ( | t_RECORD_PMBUS_WRITE_BYTE * | pRecord | ) |
PRIVATE PROTOTYPES RELATING TO RECORD TYPE PARSING.
Definition at line 367 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x02___processWriteWordOptionalPEC | ( | t_RECORD_PMBUS_WRITE_WORD * | pRecord | ) |
Definition at line 412 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x04___processReadByteExpectOptionalPEC | ( | t_RECORD_PMBUS_READ_BYTE_EXPECT * | pRecord | ) |
Definition at line 455 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x05___processReadWordExpectOptionalPEC | ( | t_RECORD_PMBUS_READ_WORD_EXPECT * | pRecord | ) |
Definition at line 500 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x09___bufferNVMData | ( | t_RECORD_NVM_DATA * | pRecord | ) |
Definition at line 545 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x0A___processReadByteLoopMaskOptionalPEC | ( | t_RECORD_PMBUS_READ_BYTE_LOOP_MASK * | pRecord | ) |
Definition at line 587 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x0B___processReadWordLoopMaskOptionalPEC | ( | t_RECORD_PMBUS_READ_WORD_LOOP_MASK * | pRecord | ) |
Definition at line 646 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x0C___processPollReadByteUntilAckNoPEC | ( | t_RECORD_PMBUS_POLL_READ_BYTE_UNTIL_ACK * | pRecord | ) |
Definition at line 703 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x0D___processDelayMs | ( | t_RECORD_DELAY_MS * | pRecord | ) |
Definition at line 743 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x0E___processSendByteOptionalPEC | ( | t_RECORD_PMBUS_SEND_BYTE * | pRecord | ) |
Definition at line 782 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x0F___processWriteByteNoPEC | ( | t_RECORD_PMBUS_WRITE_BYTE_NOPEC * | pRecord | ) |
Definition at line 819 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x10___processWriteWordNoPEC | ( | t_RECORD_PMBUS_WRITE_WORD_NOPEC * | pRecord | ) |
Definition at line 857 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x12___processReadByteExpectNoPEC | ( | t_RECORD_PMBUS_READ_BYTE_EXPECT_NOPEC * | pRecord | ) |
Definition at line 895 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x13___processReadWordExpectNoPEC | ( | t_RECORD_PMBUS_READ_WORD_EXPECT_NOPEC * | pRecord | ) |
Definition at line 934 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x15___processReadByteLoopMaskNoPEC | ( | t_RECORD_PMBUS_READ_BYTE_LOOP_MASK_NOPEC * | pRecord | ) |
Definition at line 974 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x16___processReadWordLoopMaskNoPEC | ( | t_RECORD_PMBUS_READ_WORD_LOOP_MASK_NOPEC * | pRecord | ) |
Definition at line 1027 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x17___processSendByteNoPEC | ( | t_RECORD_PMBUS_SEND_BYTE_NOPEC * | pRecord | ) |
Definition at line 1081 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x18___processEvent | ( | t_RECORD_EVENT * | pRecord | ) |
Definition at line 1114 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x19___processReadByteExpectMaskNoPEC | ( | t_RECORD_PMBUS_READ_BYTE_EXPECT_MASK_NOPEC * | pRecord | ) |
Definition at line 1209 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x1A___processReadWordExpectMaskNoPEC | ( | t_RECORD_PMBUS_READ_WORD_EXPECT_MASK_NOPEC * | pRecord | ) |
Definition at line 1256 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x1B___processVariableMetaData | ( | t_RECORD_VARIABLE_META_DATA * | pRecord | ) |
Definition at line 1310 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x1C___modifyWordNoPEC | ( | t_RECORD_PMBUS_MODIFY_WORD_NO_PEC * | pRecord | ) |
Definition at line 1395 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x1D___modifyByteNoPEC | ( | t_RECORD_PMBUS_MODIFY_BYTE_NO_PEC * | pRecord | ) |
Definition at line 1439 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x1E___writeNvmData | ( | t_RECORD_NVM_DATA * | pRecord | ) |
Definition at line 1483 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x1F___read_then_verifyNvmData | ( | t_RECORD_NVM_DATA * | pRecord | ) |
Definition at line 1509 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x20___modifyByteOptionalPEC | ( | t_RECORD_PMBUS_MODIFY_BYTE * | pRecord | ) |
Definition at line 1535 of file main_record_processor.cpp.
| uint8_t recordProcessor___0x21___modifyWordOptionalPEC | ( | t_RECORD_PMBUS_MODIFY_WORD * | pRecord | ) |
Definition at line 1588 of file main_record_processor.cpp.
| uint8_t verifyRecordsOnDemand | ( | pRecordHeaderLengthAndType(*)(void) | getRecord | ) |
Definition at line 224 of file main_record_processor.cpp.
| #define DEBUG_PRINT 0 |
Definition at line 46 of file main_record_processor.cpp.
| #define DEBUG_PROCESSING 0 |
Definition at line 45 of file main_record_processor.cpp.
| #define DEBUG_SILENT 0 |
Definition at line 44 of file main_record_processor.cpp.
|
static |
Definition at line 79 of file main_record_processor.cpp.
|
static |
VARIABLES.
Definition at line 78 of file main_record_processor.cpp.