![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology LTC3887 Telemetry LTC3887: Power Management Solution for Application Processors. More...
Linear Technology LTC3887 Telemetry LTC3887: Power Management Solution for Application Processors.
Demonstrates Fast Telemetry NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator.
http://www.linear.com/product/LTC3887
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file fast_telemetry.ino.
Go to the source code of this file.
Functions | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
Macros | |
| #define | LTC3887_I2C_ADDRESS 0x4E |
| #define | MFR_ADC_CONTROL 0xD8 |
| #define | ADC_MFR_TELEMETRY_STATUS 0xDA |
| #define | MFR_REAL_TIME 0xFB |
| #define | NUM_MEAS 10 |
Variables | |
| static uint8_t | ltc3887_i2c_address |
| static LT_SMBus * | smbus = new LT_SMBusNoPec() |
| static LT_PMBus * | pmbus = new LT_PMBus(smbus) |
|
static |
|
static |
|
static |
Prints the title block when program first starts.
Definition at line 348 of file fast_telemetry.ino.
|
static |
| #define ADC_MFR_TELEMETRY_STATUS 0xDA |
Definition at line 67 of file fast_telemetry.ino.
| #define LTC3887_I2C_ADDRESS 0x4E |
Definition at line 65 of file fast_telemetry.ino.
| #define MFR_ADC_CONTROL 0xD8 |
Definition at line 66 of file fast_telemetry.ino.
| #define MFR_REAL_TIME 0xFB |
Definition at line 68 of file fast_telemetry.ino.
| #define NUM_MEAS 10 |
Definition at line 69 of file fast_telemetry.ino.
|
static |
Definition at line 71 of file fast_telemetry.ino.
Definition at line 73 of file fast_telemetry.ino.
|
static |
Definition at line 72 of file fast_telemetry.ino.