![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Definition at line 60 of file LT_SMBusGroup.h.
Public Member Functions | |
| LT_SMBusGroup (LT_SMBus *) | |
| LT_SMBusGroup (LT_SMBus *, uint32_t speed) | |
| virtual | ~LT_SMBusGroup () |
| void | writeByte (uint8_t address, uint8_t command, uint8_t data) |
| SMBus write byte command. More... | |
| void | writeBytes (uint8_t *addresses, uint8_t *commands, uint8_t *data, uint8_t no_addresses) |
| SMBus write byte command for a list of addresses. More... | |
| uint8_t | readByte (uint8_t address, uint8_t command) |
| SMBus read byte command. More... | |
| void | writeWord (uint8_t address, uint8_t command, uint16_t data) |
| SMBus write word command. More... | |
| uint16_t | readWord (uint8_t address, uint8_t command) |
| SMBus read word command. More... | |
| void | writeBlock (uint8_t address, uint8_t command, uint8_t *block, uint16_t block_size) |
| SMBus write block command. More... | |
| uint8_t | writeReadBlock (uint8_t address, uint8_t command, uint8_t *block_out, uint16_t block_out_size, uint8_t *block_in, uint16_t block_in_size) |
| SMBus write then read block command. More... | |
| uint8_t | readBlock (uint8_t address, uint8_t command, uint8_t *block, uint16_t block_size) |
| SMBus read block command. More... | |
| void | sendByte (uint8_t address, uint8_t command) |
| SMBus send byte command. More... | |
| void | beginStoring () |
| Group Protocol Begin. More... | |
| void | execute () |
| Group Protocol Execute queued commands. More... | |
Public Member Functions inherited from LT_SMBusBase | |
| LT_I2CBus * | i2cbus (void) |
| void | i2cbus (LT_I2CBus *i2cbus) |
| uint8_t | readAlert (void) |
| Perform ARA. More... | |
| uint8_t | waitForAck (uint8_t address, uint8_t command) |
| Read with the address and command in loop until ack, then issue stop. More... | |
| uint8_t * | probe (uint8_t command) |
| SMBus bus probe. More... | |
| uint8_t * | probeUnique (uint8_t command) |
| SMBus bus probe. More... | |
Public Member Functions inherited from LT_SMBus | |
| virtual | ~LT_SMBus () |
| bool | pecEnabled (void) |
| Check if PEC is enabled. More... | |
| void | pecClear (void) |
| Clear the pec value so it can start a new calculation. More... | |
| void | pecAdd (uint8_t byte_value) |
| Add a byte to the pec calculation. More... | |
| uint8_t | pecGet (void) |
| Get the current pec result. More... | |
| bool | checkCRC (uint8_t *data) |
| Check CRC of block data organized as 31 data bytes plus CRC. More... | |
| uint8_t | getCRC (uint8_t *data) |
| Get CRC of block data organized as 31 bytes pluse CRC. More... | |
| uint8_t | calculate (uint8_t *data, uint8_t begining_value, uint8_t start_index, uint8_t length) |
| Helper function for pec. More... | |
Additional Inherited Members | |
Protected Member Functions inherited from LT_SMBusBase | |
| LT_SMBusBase () | |
| LT_SMBusBase (uint32_t speed) | |
| virtual | ~LT_SMBusBase () |
Protected Member Functions inherited from LT_SMBus | |
| void | constructTable (uint16_t user_polynomial) |
| Initialize the table used to speed up pec calculations. More... | |
| uint8_t | doCalculate (uint8_t data, uint8_t begining_value) |
| Helper function for pec. More... | |
| LT_SMBus () | |
Protected Attributes inherited from LT_SMBusBase | |
| LT_I2CBus * | i2cbus_ |
Protected Attributes inherited from LT_SMBus | |
| bool | pec_enabled_ |
| uint8_t | running_pec_ |
| Temporary pec calc value. More... | |
| unsigned char | poly_ |
| The poly used in the calc. More... | |
| uint16_t | crc_polynomial_ |
| The crc poly used in the calc. More... | |
Static Protected Attributes inherited from LT_SMBusBase | |
| static bool | open_ = false |
| Used to ensure initialisation of i2c once. More... | |
| static uint8_t | found_address_ [] |
| void LT_SMBusGroup::beginStoring | ( | ) |
| void LT_SMBusGroup::execute | ( | ) |
Group Protocol Execute queued commands.
Definition at line 175 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus read block command.
| address | Slave Address |
| command | Command byte |
| block | Memory to receive data |
| block_size | Size of receive data memory |
Reimplemented from LT_SMBusBase.
Definition at line 133 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus read byte command.
| address | Slave Address |
| command | Command byte |
Reimplemented from LT_SMBusBase.
Definition at line 91 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus read word command.
| address | Slave Address |
| command | Command byte |
Reimplemented from LT_SMBusBase.
Definition at line 107 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus send byte command.
| address | Slave Address |
| command | Command byte |
Reimplemented from LT_SMBusBase.
Definition at line 142 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus write block command.
| address | Slave Address |
| command | Command byte |
| block | Data to send |
Reimplemented from LT_SMBusBase.
Definition at line 115 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus write byte command.
| address | Slave address |
| command | Command byte |
| data | Data to send |
Reimplemented from LT_SMBusBase.
Definition at line 75 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus write byte command for a list of addresses.
| addresses | Slave Addresses |
| commands | Command bytes |
| data | Data to send |
Reimplemented from LT_SMBusBase.
Definition at line 83 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus write then read block command.
| address | Slave Address |
| command | Command byte |
| block_out | Data to send |
| block_out_size | Size of data to send |
| block_in | Memory to receive data |
| block_in_size | Size of receive data memory |
Reimplemented from LT_SMBusBase.
Definition at line 124 of file LT_SMBusGroup.cpp.
|
virtual |
SMBus write word command.
| address | Slave Address |
| command | Command byte |
| data | Data to send |
Reimplemented from LT_SMBusBase.
Definition at line 99 of file LT_SMBusGroup.cpp.
| LT_SMBusGroup::LT_SMBusGroup | ( | LT_SMBus * | smbus | ) |
Definition at line 59 of file LT_SMBusGroup.cpp.
| LT_SMBusGroup::LT_SMBusGroup | ( | LT_SMBus * | smbus, |
| uint32_t | speed | ||
| ) |
Definition at line 67 of file LT_SMBusGroup.cpp.
|
virtual |
Definition at line 151 of file LT_SMBusGroup.h.