![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Definition at line 56 of file LT_PMBusDeviceController.h.
Public Member Functions | |
| LT_PMBusDeviceController (LT_PMBus *pmbus, uint8_t address, uint8_t no_pages) | |
| LT_PMBusRail ** | getRails () |
| Return a list of rails if any page is part of a rail. More... | |
Public Member Functions inherited from LT_PMBusDevice | |
| virtual | ~LT_PMBusDevice () |
| LT_PMBus * | pmbus () |
| LT_SMBus * | smbus () |
| void | changePMBus (LT_PMBus *pmbus) |
| Change the pmbus. More... | |
| uint8_t | getAddress () |
| Get the address. More... | |
| virtual char * | getType (void) |
| virtual uint8_t | getNumPages (void)=0 |
| void | setPage (uint8_t page) |
| uint32_t | getMaxSpeed (void) |
| Get the maximum speed the device can communicate with. More... | |
| virtual void | setSpeed (uint32_t speed) |
| Set the speed. If > 100000, enable clock stretching. More... | |
| virtual uint32_t | getCapabilities ()=0 |
| Get the supported capabilities. More... | |
| virtual bool | hasCapability (uint32_t capability)=0 |
| Is/are these capability(s) supported? More... | |
| virtual void | enableFaultLog () |
| Enable the Fault Log. More... | |
| virtual void | disableFaultLog () |
| Disable the Fault Log. More... | |
| virtual bool | hasFaultLog () |
| Is there a fault log? More... | |
| virtual char * | getFaultLog () |
| Get the fault log text (call must free) More... | |
| virtual void | clearFaultLog () |
| Clear the Fault Log. More... | |
| void | setVout (float voltage) |
| float | readVin (bool polling) |
| float | readVout (bool polling) |
| float | readIin (bool polling) |
| float | readIout (bool polling) |
| float | readPin (bool polling) |
| float | readPout (bool polling) |
| float | readExternalTemperature (bool polling) |
| float | readInternalTemperature (bool polling) |
| float | readDutyCycle (bool polling) |
| uint16_t | readStatusWord () |
| uint16_t | readMfrSpecialId () |
| void | clearFaults () |
| void | marginHigh () |
| void | marginLow () |
| void | marginOff () |
Additional Inherited Members | |
Protected Member Functions inherited from LT_PMBusDevice | |
| LT_PMBusDevice (LT_PMBus *pmbus, uint8_t address) | |
| void | probeSpeed () |
Protected Attributes inherited from LT_PMBusDevice | |
| LT_PMBus * | pmbus_ |
| uint8_t | address_ |
| uint32_t | maxSpeed_ |
| uint8_t | model_ [9] |
|
virtual |
Return a list of rails if any page is part of a rail.
Implements LT_PMBusDevice.
Definition at line 65 of file LT_PMBusDeviceController.h.
| LT_PMBusDeviceController::LT_PMBusDeviceController | ( | LT_PMBus * | pmbus, |
| uint8_t | address, | ||
| uint8_t | no_pages | ||
| ) |
Definition at line 63 of file LT_PMBusDeviceController.h.