![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Definition at line 135 of file Adafruit_GFX.h.
Public Member Functions | |
| GFXcanvas1 (uint16_t w, uint16_t h) | |
| ~GFXcanvas1 (void) | |
| void | drawPixel (int16_t x, int16_t y, uint16_t color) |
| void | fillScreen (uint16_t color) |
| uint8_t * | getBuffer (void) |
Public Member Functions inherited from Adafruit_GFX | |
| Adafruit_GFX (int16_t w, int16_t h) | |
| virtual void | drawLine (int16_t x0, int16_t y0, int16_t x1, int16_t y1, uint16_t color) |
| virtual void | drawFastVLine (int16_t x, int16_t y, int16_t h, uint16_t color) |
| virtual void | drawFastHLine (int16_t x, int16_t y, int16_t w, uint16_t color) |
| virtual void | drawRect (int16_t x, int16_t y, int16_t w, int16_t h, uint16_t color) |
| virtual void | fillRect (int16_t x, int16_t y, int16_t w, int16_t h, uint16_t color) |
| virtual void | fillScreen (uint16_t color) |
| virtual void | invertDisplay (boolean i) |
| void | drawCircle (int16_t x0, int16_t y0, int16_t r, uint16_t color) |
| void | drawCircleHelper (int16_t x0, int16_t y0, int16_t r, uint8_t cornername, uint16_t color) |
| void | fillCircle (int16_t x0, int16_t y0, int16_t r, uint16_t color) |
| void | fillCircleHelper (int16_t x0, int16_t y0, int16_t r, uint8_t cornername, int16_t delta, uint16_t color) |
| void | drawTriangle (int16_t x0, int16_t y0, int16_t x1, int16_t y1, int16_t x2, int16_t y2, uint16_t color) |
| void | fillTriangle (int16_t x0, int16_t y0, int16_t x1, int16_t y1, int16_t x2, int16_t y2, uint16_t color) |
| void | drawRoundRect (int16_t x0, int16_t y0, int16_t w, int16_t h, int16_t radius, uint16_t color) |
| void | fillRoundRect (int16_t x0, int16_t y0, int16_t w, int16_t h, int16_t radius, uint16_t color) |
| void | drawBitmap (int16_t x, int16_t y, const uint8_t *bitmap, int16_t w, int16_t h, uint16_t color) |
| void | drawBitmap (int16_t x, int16_t y, const uint8_t *bitmap, int16_t w, int16_t h, uint16_t color, uint16_t bg) |
| void | drawBitmap (int16_t x, int16_t y, uint8_t *bitmap, int16_t w, int16_t h, uint16_t color) |
| void | drawBitmap (int16_t x, int16_t y, uint8_t *bitmap, int16_t w, int16_t h, uint16_t color, uint16_t bg) |
| void | drawXBitmap (int16_t x, int16_t y, const uint8_t *bitmap, int16_t w, int16_t h, uint16_t color) |
| void | drawChar (int16_t x, int16_t y, unsigned char c, uint16_t color, uint16_t bg, uint8_t size) |
| void | setCursor (int16_t x, int16_t y) |
| void | setTextColor (uint16_t c) |
| void | setTextColor (uint16_t c, uint16_t bg) |
| void | setTextSize (uint8_t s) |
| void | setTextWrap (boolean w) |
| void | setRotation (uint8_t r) |
| void | cp437 (boolean x=true) |
| void | setFont (const GFXfont *f=NULL) |
| void | getTextBounds (char *string, int16_t x, int16_t y, int16_t *x1, int16_t *y1, uint16_t *w, uint16_t *h) |
| void | getTextBounds (const __FlashStringHelper *s, int16_t x, int16_t y, int16_t *x1, int16_t *y1, uint16_t *w, uint16_t *h) |
| virtual void | write (uint8_t) |
| int16_t | height (void) const |
| int16_t | width (void) const |
| uint8_t | getRotation (void) const |
| int16_t | getCursorX (void) const |
| int16_t | getCursorY (void) const |
Additional Inherited Members | |
Protected Attributes inherited from Adafruit_GFX | |
| const int16_t | WIDTH |
| const int16_t | HEIGHT |
| int16_t | _width |
| int16_t | _height |
| int16_t | cursor_x |
| int16_t | cursor_y |
| uint16_t | textcolor |
| uint16_t | textbgcolor |
| uint8_t | textsize |
| uint8_t | rotation |
| boolean | wrap |
| boolean | _cp437 |
| GFXfont * | gfxFont |
|
virtual |
Implements Adafruit_GFX.
Definition at line 1149 of file Adafruit_GFX.cpp.
| void GFXcanvas1::fillScreen | ( | uint16_t | color | ) |
Definition at line 1185 of file Adafruit_GFX.cpp.
| uint8_t * GFXcanvas1::getBuffer | ( | void | ) |
Definition at line 1144 of file Adafruit_GFX.cpp.
| GFXcanvas1::GFXcanvas1 | ( | uint16_t | w, |
| uint16_t | h | ||
| ) |
Definition at line 1130 of file Adafruit_GFX.cpp.
| GFXcanvas1::~GFXcanvas1 | ( | void | ) |
Definition at line 1139 of file Adafruit_GFX.cpp.