![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Go to the source code of this file.
Functions | |
| void | printError (int16_t errorNum) |
Macros | |
| #define | _PRINT_ERROR_VOLTAGE_SOURCE_SETTING 0 |
| #define | _PRINT_ERROR_CURRENT_SOURCE_SETTING 1 |
| #define | _PRINT_ERROR_SERIAL_COMMAND 2 |
| #define | _PRINT_ERROR_NO_CALIBRATION_DATA_FOUND 3 |
| #define | _PRINT_ERROR_FACTORY_CALIBRATION_RESTORE_FAILED_CATASTROPHICALLY |
| void printError | ( | int16_t | errorNum | ) |
Definition at line 12 of file PrintError.h.
| #define _PRINT_ERROR_CURRENT_SOURCE_SETTING 1 |
Definition at line 7 of file PrintError.h.
| #define _PRINT_ERROR_FACTORY_CALIBRATION_RESTORE_FAILED_CATASTROPHICALLY |
Definition at line 10 of file PrintError.h.
| #define _PRINT_ERROR_NO_CALIBRATION_DATA_FOUND 3 |
Definition at line 9 of file PrintError.h.
| #define _PRINT_ERROR_SERIAL_COMMAND 2 |
Definition at line 8 of file PrintError.h.
| #define _PRINT_ERROR_VOLTAGE_SOURCE_SETTING 0 |
Definition at line 6 of file PrintError.h.