![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Go to the source code of this file.
Functions | |
| LiquidCrystal | lcd (RS, E, D4, D5, D6, D7) |
| static void | setup () |
| static void | loop () |
| static int8_t | read_switches () |
| static void | init_dac () |
| static void | set_voltage () |
| static void | display_decimal () |
| static void | display_hex () |
| static void | set_voltage_hex () |
Variables | |
| const int16_t | RS = 8 |
| const int16_t | E = 9 |
| const int16_t | D4 = 4 |
| const int16_t | D5 = 5 |
| const int16_t | D6 = 6 |
| const int16_t | D7 = 7 |
| const int16_t | BUTTON_PIN = 0 |
| const int8_t | UP = 1 |
| const int8_t | DOWN = 2 |
| const int8_t | LEFT = 3 |
| const int8_t | RIGHT = 4 |
| const int8_t | SELECT = 5 |
| static int8_t | demo_board_connected |
| static float | LTC2756_lsb = 3.8146972656e-5 |
| static int32_t | LTC2756_offset = 0x20000 |
| static int16_t | pos |
| static int8_t | volts [5] = {0, 0, 0, 0, 0} |
| static int8_t | hex [5] = {0x00, 0x00, 0x00, 0x00,0x02} |
| static uint8_t | HEX_DEC |
| bool | sign = 0 |
|
static |
Definition at line 226 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 318 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 155 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 125 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 136 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 185 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 400 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 82 of file Precision_Voltage_Source.ino.
| const int16_t BUTTON_PIN = 0 |
Definition at line 61 of file Precision_Voltage_Source.ino.
| const int16_t D4 = 4 |
Definition at line 57 of file Precision_Voltage_Source.ino.
| const int16_t D5 = 5 |
Definition at line 58 of file Precision_Voltage_Source.ino.
| const int16_t D6 = 6 |
Definition at line 59 of file Precision_Voltage_Source.ino.
| const int16_t D7 = 7 |
Definition at line 60 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 68 of file Precision_Voltage_Source.ino.
| const int8_t DOWN = 2 |
Definition at line 63 of file Precision_Voltage_Source.ino.
| const int16_t E = 9 |
Definition at line 56 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 75 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 76 of file Precision_Voltage_Source.ino.
| const int8_t LEFT = 3 |
Definition at line 64 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 71 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 72 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 73 of file Precision_Voltage_Source.ino.
| const int8_t RIGHT = 4 |
Definition at line 65 of file Precision_Voltage_Source.ino.
| const int16_t RS = 8 |
Definition at line 55 of file Precision_Voltage_Source.ino.
| const int8_t SELECT = 5 |
Definition at line 66 of file Precision_Voltage_Source.ino.
| bool sign = 0 |
Definition at line 77 of file Precision_Voltage_Source.ino.
| const int8_t UP = 1 |
Definition at line 62 of file Precision_Voltage_Source.ino.
|
static |
Definition at line 74 of file Precision_Voltage_Source.ino.