![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library Header File for LT_2974FaultLog. More...
Library Header File for LT_2974FaultLog.
Definition in file LT_2974FaultLog.cpp.
Go to the source code of this file.
Functions | |
| void | rotate (uint8_t *buf, int start, int len) |
Macros | |
| #define | RAW_EEPROM |
| void rotate | ( | uint8_t * | buf, |
| int | start, | ||
| int | len | ||
| ) |
Definition at line 61 of file LT_2974FaultLog.cpp.
| #define RAW_EEPROM |
Definition at line 59 of file LT_2974FaultLog.cpp.