![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTM9100 Anyside™ High Voltage Isolated Switch Controller with I²C Command and Telemetry. More...
Library for LTM9100 Anyside™ High Voltage Isolated Switch Controller with I²C Command and Telemetry.
Definition in file LTM9100.cpp.
Go to the source code of this file.
Functions | |
| int8_t | LTM9100_register_read (uint8_t i2c_address, uint8_t register_address, uint8_t *register_data) |
| Reads an 8-bit register from the LTM9100 using the standard repeated start format. More... | |
| int8_t | LTM9100_adc_read (uint8_t i2c_address, uint8_t base_address, float *register_data) |
| Read the specified ADC value (SENSE, ADIN, ADIN2) and output in human readable format to the serial console. More... | |
| int8_t | LTM9100_register_write (uint8_t i2c_address, uint8_t register_address, uint8_t register_data) |
| Writes to an 8-bit register inside the LTM9100 using the standard I2C repeated start format. More... | |
| int8_t | LTM9100_bit_set (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number) |
| Sets any bit inside the LTM9100 using the standard I2C repeated start format. More... | |
| int8_t | LTM9100_bit_clear (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number) |
| Clears any bit inside the LTM9100 using the standard I2C repeated start format. More... | |
| int8_t | LTM9100_bit_read (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number, uint8_t *register_data) |
| Read the bit specified by bit_number from the LTM9100. More... | |
| int8_t | LTM9100_alert_read (uint8_t *register_data) |
| Attempts to read a byte from the I2C bus using the alert address (0xC) to ascertain pending alerts on the bus. More... | |
| int8_t | LTM9100_print_all_registers (uint8_t i2c_address) |
| Read all LTM9100 registers and output to the serial console. More... | |
| int8_t | LTM9100_continuous_read_all_registers (uint8_t i2c_address) |
| Read all LTM9100 registers and output to the serial console every second until a key press is detected. More... | |
| boolean | valid_register (uint8_t user_register, uint8_t register_array[], uint8_t array_length) |
| Check if user_register is a valid register for the LTM9100. More... | |
Variables | |
| uint8_t | reg_read_list [10] = {0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09} |
| uint8_t | reg_write_list [9] = {0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09} |
| int8_t LTM9100_adc_read | ( | uint8_t | i2c_address, |
| uint8_t | base_address, | ||
| float * | register_data | ||
| ) |
Read the specified ADC value (SENSE, ADIN, ADIN2) and output in human readable format to the serial console.
Definition at line 80 of file LTM9100.cpp.
| int8_t LTM9100_alert_read | ( | uint8_t * | register_data | ) |
Attempts to read a byte from the I2C bus using the alert address (0xC) to ascertain pending alerts on the bus.
Definition at line 155 of file LTM9100.cpp.
| int8_t LTM9100_bit_clear | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number | ||
| ) |
Clears any bit inside the LTM9100 using the standard I2C repeated start format.
Definition at line 133 of file LTM9100.cpp.
| int8_t LTM9100_bit_read | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number, | ||
| uint8_t * | register_data | ||
| ) |
Read the bit specified by bit_number from the LTM9100.
Definition at line 146 of file LTM9100.cpp.
| int8_t LTM9100_bit_set | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number | ||
| ) |
Sets any bit inside the LTM9100 using the standard I2C repeated start format.
Definition at line 120 of file LTM9100.cpp.
| int8_t LTM9100_continuous_read_all_registers | ( | uint8_t | i2c_address | ) |
Read all LTM9100 registers and output to the serial console every second until a key press is detected.
Definition at line 188 of file LTM9100.cpp.
| int8_t LTM9100_print_all_registers | ( | uint8_t | i2c_address | ) |
Read all LTM9100 registers and output to the serial console.
Definition at line 163 of file LTM9100.cpp.
| int8_t LTM9100_register_read | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t * | register_data | ||
| ) |
Reads an 8-bit register from the LTM9100 using the standard repeated start format.
Definition at line 72 of file LTM9100.cpp.
| int8_t LTM9100_register_write | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | register_data | ||
| ) |
Writes to an 8-bit register inside the LTM9100 using the standard I2C repeated start format.
Definition at line 112 of file LTM9100.cpp.
| boolean valid_register | ( | uint8_t | user_register, |
| uint8_t | register_array[], | ||
| uint8_t | array_length | ||
| ) |
Check if user_register is a valid register for the LTM9100.
Definition at line 212 of file LTM9100.cpp.
| uint8_t reg_read_list[10] = {0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09} |
Definition at line 68 of file LTM9100.cpp.
| uint8_t reg_write_list[9] = {0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09} |
Definition at line 69 of file LTM9100.cpp.