![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC6954: Low Phase Noise, Triple Output Clock Distribution Divider/Driver. More...
Library for LTC6954: Low Phase Noise, Triple Output Clock Distribution Divider/Driver.
Definition in file LTC6954.cpp.
Go to the source code of this file.
Functions | |
| uint8_t | LTC6954_read (uint8_t cs, int8_t address) |
| LTC6954 Read Single Address reads 8 bit Data field to LTC6954. More... | |
| long | LTC6954_read_field (uint8_t cs, uint8_t address, uint8_t MSB_loc, uint8_t numbits) |
| LTC6954 Read Single Field For SPI FIELDS located in 1 or multiple address locations reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| long | get_LTC6954_SPI_FIELD (uint8_t cs, uint8_t f) |
| Gets the LTC6954 SPI field value calls function LTC6954_read_field, which reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| void | LTC6954_write (uint8_t cs, uint8_t address, uint8_t Data) |
| LTC6954 Write Single Address writes 8 bit Data field to LTC6954. More... | |
| uint8_t | LTC6954_write_field (uint8_t cs, long field_data, uint8_t address, uint8_t MSB_loc, uint8_t numbits) |
| LTC6954 Write Single Field For SPI FIELDS in 1 or multiple address locations reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| uint8_t | get_LTC6954_REGSIZE () |
| returns # of addresses in parts register map (array size) More... | |
| uint8_t | get_LTC6954_SPI_FIELD_NUMBITS (uint8_t f) |
| returns the number of bits for a given field name in the SPI map More... | |
| uint8_t | get_LTC6954_SPI_FIELD_RW (uint8_t f) |
| returns if the given field name is (0)read/write or (1)read_only field More... | |
| void | set_LTC6954_SPI_FIELD (uint8_t cs, uint8_t f, long field_data) |
| Sets the LTC6954 SPI field value calls function LTC6954_read_field, which reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| void | set_LTC6954_ALLREGS (uint8_t cs, uint8_t reg00, uint8_t reg01, uint8_t reg02, uint8_t reg03, uint8_t reg04, uint8_t reg05, uint8_t reg06) |
| Writes values to ALL LTC6954 RW address. More... | |
| void | LTC6954_init () |
| Initializes the SPI MAP arrays The values set in initialization are used all the LTC6954 SPI/WRITE and read functions (set_LTC6954_SPI_FIELD, get_LTC6954_SPI_FIELD, LTC6954_read, LTC6954_write, etc, etc) More... | |
Variables | |
| uint8_t | LTC6954_reg [LTC6954_NUM_REGADDR] |
| number of LTC6954 spi addresses More... | |
| uint8_t | LTC6954_spi_map [(LTC6954_NUM_REGFIELD+1)][4] |
| LTC6954 spi map, stores MSB address location, MSB bit location, field length in bits, and R or RW capability. More... | |
| uint8_t get_LTC6954_REGSIZE | ( | ) |
returns # of addresses in parts register map (array size)
Definition at line 239 of file LTC6954.cpp.
| long get_LTC6954_SPI_FIELD | ( | uint8_t | cs, |
| uint8_t | f | ||
| ) |
Gets the LTC6954 SPI field value calls function LTC6954_read_field, which reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| f | SPI field number |
Definition at line 161 of file LTC6954.cpp.
| uint8_t get_LTC6954_SPI_FIELD_NUMBITS | ( | uint8_t | f | ) |
returns the number of bits for a given field name in the SPI map
| f | SPI field number |
Definition at line 249 of file LTC6954.cpp.
| uint8_t get_LTC6954_SPI_FIELD_RW | ( | uint8_t | f | ) |
returns if the given field name is (0)read/write or (1)read_only field
| f | SPI field number |
Definition at line 259 of file LTC6954.cpp.
| void LTC6954_init | ( | ) |
Initializes the SPI MAP arrays The values set in initialization are used all the LTC6954 SPI/WRITE and read functions (set_LTC6954_SPI_FIELD, get_LTC6954_SPI_FIELD, LTC6954_read, LTC6954_write, etc, etc)
Definition at line 304 of file LTC6954.cpp.
| uint8_t LTC6954_read | ( | uint8_t | cs, |
| int8_t | address | ||
| ) |
LTC6954 Read Single Address reads 8 bit Data field to LTC6954.
has to shift data by one bit to account for RW bit
| cs | Chip Select Pin |
| address | Register address for the LTC6954. |
Definition at line 105 of file LTC6954.cpp.
| long LTC6954_read_field | ( | uint8_t | cs, |
| uint8_t | address, | ||
| uint8_t | MSB_loc, | ||
| uint8_t | numbits | ||
| ) |
LTC6954 Read Single Field For SPI FIELDS located in 1 or multiple address locations reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| address | Register address for the LTC6954. |
| MSB_loc | MSB bit location of field |
| numbits | length of field (i.e. number of bits in field) |
Definition at line 125 of file LTC6954.cpp.
| void LTC6954_write | ( | uint8_t | cs, |
| uint8_t | address, | ||
| uint8_t | Data | ||
| ) |
LTC6954 Write Single Address writes 8 bit Data field to LTC6954.
has to shift data by one bit to account for RW bit
| cs | Chip Select Pin |
| address | Register address for the LTC6954. |
| Data | 8-bit data to be written to register |
Definition at line 172 of file LTC6954.cpp.
| uint8_t LTC6954_write_field | ( | uint8_t | cs, |
| long | field_data, | ||
| uint8_t | address, | ||
| uint8_t | MSB_loc, | ||
| uint8_t | numbits | ||
| ) |
LTC6954 Write Single Field For SPI FIELDS in 1 or multiple address locations reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| field_data | Value field value to be set to |
| address | Register address for the LTC6954. |
| MSB_loc | MSB bit location of field |
| numbits | length of field (i.e. number of bits in field) |
Definition at line 188 of file LTC6954.cpp.
| void set_LTC6954_ALLREGS | ( | uint8_t | cs, |
| uint8_t | reg00, | ||
| uint8_t | reg01, | ||
| uint8_t | reg02, | ||
| uint8_t | reg03, | ||
| uint8_t | reg04, | ||
| uint8_t | reg05, | ||
| uint8_t | reg06 | ||
| ) |
Writes values to ALL LTC6954 RW address.
| cs | Chip Select Pin |
| reg00 | LTC6954 register 0 |
| reg01 | LTC6954 register 1 |
| reg02 | LTC6954 register 2 |
| reg03 | LTC6954 register 3 |
| reg04 | LTC6954 register 4 |
| reg05 | LTC6954 register 5 |
| reg06 | LTC6954 register 6 |
Definition at line 282 of file LTC6954.cpp.
| void set_LTC6954_SPI_FIELD | ( | uint8_t | cs, |
| uint8_t | f, | ||
| long | field_data | ||
| ) |
Sets the LTC6954 SPI field value calls function LTC6954_read_field, which reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| f | SPI field number |
| field_data | Value field value to be set to |
Definition at line 272 of file LTC6954.cpp.
| uint8_t LTC6954_reg[LTC6954_NUM_REGADDR] |
number of LTC6954 spi addresses
Definition at line 96 of file LTC6954.cpp.
| uint8_t LTC6954_spi_map[(LTC6954_NUM_REGFIELD+1)][4] |
LTC6954 spi map, stores MSB address location, MSB bit location, field length in bits, and R or RW capability.
Definition at line 97 of file LTC6954.cpp.