![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC6952: Ultralow Jitter, 4.5GHz PLL with 11 Outputs and JESD204B Support. More...
Library for LTC6952: Ultralow Jitter, 4.5GHz PLL with 11 Outputs and JESD204B Support.
Definition in file LTC6952.cpp.
Go to the source code of this file.
Functions | |
| uint8_t | LTC6952_read (uint8_t cs, int8_t address) |
| LTC6952 Read Single Address reads 8 bit Data field to LTC6952. More... | |
| long | LTC6952_read_field (uint8_t cs, uint8_t address, uint8_t MSB_loc, uint8_t numbits) |
| LTC6952 Read Single Field For SPI FIELDS located in 1 or multiple address location reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| long | get_LTC6952_SPI_FIELD (uint8_t cs, uint8_t f) |
| Gets the LTC6952 SPI field value calls function LTC6952_read_field, which reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| void | LTC6952_write (uint8_t cs, uint8_t address, uint8_t Data) |
| LTC6952 Write Single Address writes 8 bit Data field to LTC6952. More... | |
| uint8_t | LTC6952_write_field (uint8_t cs, long field_data, uint8_t address, uint8_t MSB_loc, uint8_t numbits) |
| LTC6952 Write Single Field For SPI FIELDS in 1 or multiple address locations reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| uint8_t | get_LTC6952_REGSIZE () |
| returns # of addresses in parts register map (array size) More... | |
| uint8_t | get_LTC6952_SPI_FIELD_NUMBITS (uint8_t f) |
| returns the number of bits for a given field name in the SPI map More... | |
| uint8_t | get_LTC6952_SPI_FIELD_RW (uint8_t f) |
| returns if the given field name is (0)read/write or (1)read_only field More... | |
| void | set_LTC6952_SPI_FIELD (uint8_t cs, uint8_t f, long field_data) |
| Sets the LTC6952 SPI field value calls function LTC6952_read_field, which reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| void | set_LTC6952_REGS_lkup_tbl (uint8_t lkup_tbl_row) |
| Writes values to ALL LTC6952 RW addresses from a look-up table. More... | |
| void | LTC6952_init () |
| Initializes the SPI MAP arrays The values set in initialization are used for all the LTC6952 SPI/WRITE and read functions (set_LTC6952_SPI_FIELD, get_LTC6952_SPI_FIELD, LTC6952_read, LTC6952_write, etc, etc) More... | |
| int8_t | discover_demo_board_local (char *demo_name) |
| Read the ID string from the EEPROM and determine if any demo board is connected. More... | |
Variables | |
| uint8_t | LTC6952_reg [LTC6952_NUM_REGADDR] |
| number of LTC6952 spi addresses More... | |
| uint16_t | LTC6952_spi_map [(LTC6952_NUM_REGFIELD+1)] |
| LTC6952 spi map, AAAA AAAA RMMM NNNN; A= ADDR LOC, R=R or RW, M = MSB bit location, N = field length. More... | |
| uint8_t | LTC6952_lkup_tbl [2][LTC6952_NUM_REGADDR] |
| created with the LTC6952Wizard tool More... | |
| int8_t discover_demo_board_local | ( | char * | demo_name | ) |
Read the ID string from the EEPROM and determine if any demo board is connected.
Returns 1 if successful, 0 if not successful
Definition at line 493 of file LTC6952.cpp.
| uint8_t get_LTC6952_REGSIZE | ( | ) |
returns # of addresses in parts register map (array size)
Definition at line 244 of file LTC6952.cpp.
| long get_LTC6952_SPI_FIELD | ( | uint8_t | cs, |
| uint8_t | f | ||
| ) |
Gets the LTC6952 SPI field value calls function LTC6952_read_field, which reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| f | SPI field number |
Definition at line 156 of file LTC6952.cpp.
| uint8_t get_LTC6952_SPI_FIELD_NUMBITS | ( | uint8_t | f | ) |
returns the number of bits for a given field name in the SPI map
| f | SPI field number |
Definition at line 254 of file LTC6952.cpp.
| uint8_t get_LTC6952_SPI_FIELD_RW | ( | uint8_t | f | ) |
returns if the given field name is (0)read/write or (1)read_only field
| f | SPI field number |
Definition at line 267 of file LTC6952.cpp.
| void LTC6952_init | ( | ) |
Initializes the SPI MAP arrays The values set in initialization are used for all the LTC6952 SPI/WRITE and read functions (set_LTC6952_SPI_FIELD, get_LTC6952_SPI_FIELD, LTC6952_read, LTC6952_write, etc, etc)
Definition at line 355 of file LTC6952.cpp.
| uint8_t LTC6952_read | ( | uint8_t | cs, |
| int8_t | address | ||
| ) |
LTC6952 Read Single Address reads 8 bit Data field to LTC6952.
has to shift data by one bit to account for RW bit
| cs | Chip Select Pin |
| address | Register address for the LTC6952. |
Definition at line 100 of file LTC6952.cpp.
| long LTC6952_read_field | ( | uint8_t | cs, |
| uint8_t | address, | ||
| uint8_t | MSB_loc, | ||
| uint8_t | numbits | ||
| ) |
LTC6952 Read Single Field For SPI FIELDS located in 1 or multiple address location reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| address | Register address for the LTC6952. |
| MSB_loc | MSB bit location of field |
| numbits | length of field (i.e. number of bits in field) |
Definition at line 120 of file LTC6952.cpp.
| void LTC6952_write | ( | uint8_t | cs, |
| uint8_t | address, | ||
| uint8_t | Data | ||
| ) |
LTC6952 Write Single Address writes 8 bit Data field to LTC6952.
has to shift data by one bit to account for RW bit
| cs | Chip Select Pin |
| address | Register address for the LTC6952. |
| Data | 8-bit data to be written to register |
Definition at line 177 of file LTC6952.cpp.
| uint8_t LTC6952_write_field | ( | uint8_t | cs, |
| long | field_data, | ||
| uint8_t | address, | ||
| uint8_t | MSB_loc, | ||
| uint8_t | numbits | ||
| ) |
LTC6952 Write Single Field For SPI FIELDS in 1 or multiple address locations reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| field_data | Value field value to be set to |
| address | Register address for the LTC6952. |
| MSB_loc | MSB bit location of field |
| numbits | length of field (i.e. number of bits in field) |
Definition at line 193 of file LTC6952.cpp.
| void set_LTC6952_REGS_lkup_tbl | ( | uint8_t | lkup_tbl_row | ) |
Writes values to ALL LTC6952 RW addresses from a look-up table.
| lkup_tbl_row | Any number 0-2, lookup table has 2 options |
Definition at line 305 of file LTC6952.cpp.
| void set_LTC6952_SPI_FIELD | ( | uint8_t | cs, |
| uint8_t | f, | ||
| long | field_data | ||
| ) |
Sets the LTC6952 SPI field value calls function LTC6952_read_field, which reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| f | SPI field number |
| field_data | Value field value to be set to |
Definition at line 283 of file LTC6952.cpp.
| uint8_t LTC6952_lkup_tbl[2][LTC6952_NUM_REGADDR] |
created with the LTC6952Wizard tool
LTC6952 Configuration look-up table
Definition at line 88 of file LTC6952.cpp.
| uint8_t LTC6952_reg[LTC6952_NUM_REGADDR] |
number of LTC6952 spi addresses
Definition at line 85 of file LTC6952.cpp.
| uint16_t LTC6952_spi_map[(LTC6952_NUM_REGFIELD+1)] |
LTC6952 spi map, AAAA AAAA RMMM NNNN; A= ADDR LOC, R=R or RW, M = MSB bit location, N = field length.
Definition at line 86 of file LTC6952.cpp.