![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC6947: Ultralow Noise and Spurious 0.35GHz to 6GHz FracN Synthesizer. More...
Library for LTC6947: Ultralow Noise and Spurious 0.35GHz to 6GHz FracN Synthesizer.
Definition in file LTC6947.cpp.
Go to the source code of this file.
Functions | |
| uint8_t | LTC6947_read (uint8_t cs, int8_t address) |
| LTC6947 Read Single Address reads 8 bit Data field to LTC6947. More... | |
| long | LTC6947_read_field (uint8_t cs, uint8_t address, uint8_t MSB_loc, uint8_t numbits) |
| LTC6947 Read Single Field For SPI FIELDS located in 1 or multiple address location reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| long | get_LTC6947_SPI_FIELD (uint8_t cs, uint8_t f) |
| Gets the LTC6947 SPI field value calls function LTC6947_read_field, which reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| void | LTC6947_write (uint8_t cs, uint8_t address, uint8_t Data) |
| LTC6947 Write Single Address writes 8 bit Data field to LTC6947. More... | |
| uint8_t | LTC6947_write_field (uint8_t cs, long field_data, uint8_t address, uint8_t MSB_loc, uint8_t numbits) |
| LTC6947 Write Single Field For SPI FIELDS in 1 or multiple address locations reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| uint8_t | get_LTC6947_REGSIZE () |
| returns # of addresses in parts register map (array size) More... | |
| uint8_t | get_LTC6947_SPI_FIELD_NUMBITS (uint8_t f) |
| returns the number of bits for a given field name in the SPI map More... | |
| uint8_t | get_LTC6947_SPI_FIELD_RW (uint8_t f) |
| returns if the given field name is (0)read/write or (1)read_only field More... | |
| void | set_LTC6947_SPI_FIELD (uint8_t cs, uint8_t f, long field_data) |
| Sets the LTC6947 SPI field value calls function LTC6947_read_field, which reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address. More... | |
| void | set_LTC6947_ALLREGS (uint8_t cs, uint8_t reg01, uint8_t reg02, uint8_t reg03, uint8_t reg04, uint8_t reg05, uint8_t reg06, uint8_t reg07, uint8_t reg08, uint8_t reg09, uint8_t reg0A, uint8_t reg0B, uint8_t reg0C, uint8_t reg0D) |
| Writes values to ALL LTC6947 RW addresses. More... | |
| void | LTC6947_init () |
| Initializes the SPI MAP arrays The values set in initialization are used for all the LTC6947 SPI/WRITE and read functions (set_LTC6947_SPI_FIELD, get_LTC6947_SPI_FIELD, LTC6947_read, LTC6947_write, etc, etc) More... | |
| void | set_LTC6947_global_fref (unsigned long fref_MHz, unsigned long fref_Hz) |
| sets globals LTC6947_Fref_MHz and LTC6947_Fref_Hz More... | |
| void | set_LTC6947_global_frf (unsigned long frf_MHz, unsigned long frf_Hz) |
| sets globals LTC6947_Frf_MHz and LTC6947_Frf_Hz More... | |
| void | set_LTC6947_global_vcolim (unsigned long fvco_max_MHz, unsigned long fvco_max_Hz, unsigned long fvco_min_MHz, unsigned long fvco_min_Hz) |
| sets globals LTC6947_VCO_Max_Freq_MHz, LTC6947_VCO_Max_Freq_Hz, LTC6947_VCO_Min_Freq_MHz and LTC6947_VCO_Min_Freq_Hz More... | |
| unsigned long | get_LTC6947_global_fref_MHz () |
| returns global LTC6947_Fref_MHz More... | |
| unsigned long | get_LTC6947_global_fref_Hz () |
| returns global LTC6947_Fref_Hz More... | |
| unsigned long | get_LTC6947_global_frf_MHz () |
| returns global LTC6947_Frf_MHz More... | |
| unsigned long | get_LTC6947_global_frf_Hz () |
| returns global LTC6947_Frf_Hz More... | |
| unsigned long | get_LTC6947_global_VCO_MAX_MHz () |
| returns global LTC6947_VCO_Max_Freq_MHz More... | |
| unsigned long | get_LTC6947_global_VCO_MIN_MHz () |
| returns global LTC6947_VCO_Min_Freq_MHz More... | |
| unsigned long | get_LTC6947_global_VCO_MAX_Hz () |
| returns global LTC6947_VCO_Max_Freq_Hz More... | |
| unsigned long | get_LTC6947_global_VCO_MIN_Hz () |
| returns global LTC6947_VCO_Min_Freq_Hz More... | |
| unsigned long | LTC6947_calc_odiv (unsigned long frf[2]) |
| calculates the output divider setting based on the frf and on board VCO frequencies of LTC6947 More... | |
| void | LTC6947_set_frf () |
| FUNCTION: LTC6947_set_frf Calculates the integer (N), fractional (NUM) and output divider (OD) SPI values using self created 64bit math functions. More... | |
| void | prt (unsigned long an[]) |
| Prints HEX representation of 64 bit an. More... | |
| void | init64 (unsigned long an[], unsigned long bigPart, unsigned long littlePart) |
| Creates a equivalent 64 bit number from 2 32 bit numbers. More... | |
| void | HZto64 (unsigned long an[], unsigned long MHzPart, unsigned long HzPart) |
| create a 64 bit Hz number from 32 bit xxxx MHz number and 32 bit yyy yyy Hz number. More... | |
| void | shl64 (unsigned long an[]) |
| Single Bit shift left of equivalent 64 bit number (an[] = an[]<<1) More... | |
| void | shr64 (unsigned long an[]) |
| Single Bit shift right of equivalent 64 bit number (an[] = an[]<<1) More... | |
| void | shl64by (unsigned long an[], uint8_t shiftnum) |
| Multi Bit shift left of equivalent 64 bit number (an[] = an[]<<shiftnum) More... | |
| void | shr64by (unsigned long an[], uint8_t shiftnum) |
| Multi Bit shift right of equivalent 64 bit number (an[] = an[]>>shiftnum) More... | |
| void | add64 (unsigned long an[], unsigned long ann[]) |
| 64 bit Add ann to an (an[] = an[] + ann[]) More... | |
| void | sub64 (unsigned long an[], unsigned long ann[]) |
| 64 bit Subtract ann from an (an[] = an[] - ann[]) More... | |
| boolean | eq64 (unsigned long an[], unsigned long ann[]) |
| 64 bit, if an == ann, then true More... | |
| boolean | lt64 (unsigned long an[], unsigned long ann[]) |
| 64 bit, if an < ann, then true More... | |
| void | div64 (unsigned long num[], unsigned long den[]) |
| 64 bit Divide, num=num/div More... | |
| void | mul64 (unsigned long an[], unsigned long ann[]) |
| 64 bit multiply, an=an*ann More... | |
Variables | |
| uint8_t | LTC6947_reg [LTC6947_NUM_REGADDR] |
| number of LTC6947 spi addresses More... | |
| uint8_t | LTC6947_spi_map [(LTC6947_NUM_REGFIELD+1)][4] |
| LTC6947 spi map, stores MSB address location, MSB bit location, field length in bits, and R or RW capability. More... | |
| unsigned long | LTC6947_Fref_MHz = 100 |
| Default Fref frequency - MHz portion (xxx); Fref = xxx, yyy,yyy. More... | |
| unsigned long | LTC6947_Fref_Hz = 0 |
| Default Fref frequency - Hz portion (yyy,yyy); Fref = x,xxx, yyy,yyy. More... | |
| unsigned long | LTC6947_Frf_MHz = 2415 |
| Default Frf frequency - MHz portion (xxxx); Frf = x,xxx, yyy,yyy. More... | |
| unsigned long | LTC6947_Frf_Hz = 0 |
| Default Frf frequency - Hz portion (yyy,yyy); Frf = x,xxx, yyy,yyy. More... | |
| unsigned long | LTC6947_VCO_Max_Freq_MHz = 2536 |
| Max Vco frequency for default on board VCO - MHz portion (xxxx); Fvco max = xxx, yyy,yyy. More... | |
| unsigned long | LTC6947_VCO_Min_Freq_MHz = 2328 |
| Min Vco frequency for default on board VCO - MHz portion (xxxx); Fvco min = x,xxx, yyy,yyy. More... | |
| unsigned long | LTC6947_VCO_Max_Freq_Hz = 0 |
| Max Vco frequency for default on board VCO - Hz portion (yyy,yyy); Fvco max = x,xxx, yyy,yyy. More... | |
| unsigned long | LTC6947_VCO_Min_Freq_Hz = 0 |
| Min Vco frequency for default on board VCO - Hz portion (yyy,yyy); Fvco min= x,xxx, yyy,yyy. More... | |
| unsigned long | zero64 [] = {0,0} |
| for 64bit math functions More... | |
| void add64 | ( | unsigned long | an[], |
| unsigned long | ann[] | ||
| ) |
64 bit Add ann to an (an[] = an[] + ann[])
| an | 64 bit number, in 1x2 32bit array |
| ann | 64 bit number, in 1x2 32bit array |
Definition at line 879 of file LTC6947.cpp.
| void div64 | ( | unsigned long | num[], |
| unsigned long | den[] | ||
| ) |
64 bit Divide, num=num/div
| num | numerator: 64 bit number, in 1x2 32bit array |
| den | denominator: 64 bit number, in 1x2 32bit array |
Definition at line 928 of file LTC6947.cpp.
| boolean eq64 | ( | unsigned long | an[], |
| unsigned long | ann[] | ||
| ) |
64 bit, if an == ann, then true
| an | 64 bit number, in 1x2 32bit array |
| ann | 64 bit number, in 1x2 32bit array |
Definition at line 907 of file LTC6947.cpp.
| unsigned long get_LTC6947_global_fref_Hz | ( | ) |
| unsigned long get_LTC6947_global_fref_MHz | ( | ) |
| unsigned long get_LTC6947_global_frf_Hz | ( | ) |
| unsigned long get_LTC6947_global_frf_MHz | ( | ) |
| unsigned long get_LTC6947_global_VCO_MAX_Hz | ( | ) |
returns global LTC6947_VCO_Max_Freq_Hz
Definition at line 518 of file LTC6947.cpp.
| unsigned long get_LTC6947_global_VCO_MAX_MHz | ( | ) |
returns global LTC6947_VCO_Max_Freq_MHz
Definition at line 508 of file LTC6947.cpp.
| unsigned long get_LTC6947_global_VCO_MIN_Hz | ( | ) |
returns global LTC6947_VCO_Min_Freq_Hz
Definition at line 523 of file LTC6947.cpp.
| unsigned long get_LTC6947_global_VCO_MIN_MHz | ( | ) |
returns global LTC6947_VCO_Min_Freq_MHz
Definition at line 513 of file LTC6947.cpp.
| uint8_t get_LTC6947_REGSIZE | ( | ) |
returns # of addresses in parts register map (array size)
Definition at line 232 of file LTC6947.cpp.
| long get_LTC6947_SPI_FIELD | ( | uint8_t | cs, |
| uint8_t | f | ||
| ) |
Gets the LTC6947 SPI field value calls function LTC6947_read_field, which reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| f | SPI field number |
Definition at line 154 of file LTC6947.cpp.
| uint8_t get_LTC6947_SPI_FIELD_NUMBITS | ( | uint8_t | f | ) |
returns the number of bits for a given field name in the SPI map
| f | SPI field number |
Definition at line 242 of file LTC6947.cpp.
| uint8_t get_LTC6947_SPI_FIELD_RW | ( | uint8_t | f | ) |
returns if the given field name is (0)read/write or (1)read_only field
| f | SPI field number |
Definition at line 252 of file LTC6947.cpp.
| void HZto64 | ( | unsigned long | an[], |
| unsigned long | MHzPart, | ||
| unsigned long | HzPart | ||
| ) |
create a 64 bit Hz number from 32 bit xxxx MHz number and 32 bit yyy yyy Hz number.
A) if an < 2^32 bits:
B) if an > 2^32 bits (4,294,967,296):
| an | 64 bit number, 1x2 32 bit array |
| MHzPart | integer in MHZ |
| HzPart | integer in Hz |
Definition at line 798 of file LTC6947.cpp.
| void init64 | ( | unsigned long | an[], |
| unsigned long | bigPart, | ||
| unsigned long | littlePart | ||
| ) |
Creates a equivalent 64 bit number from 2 32 bit numbers.
| an | 64 bit number, 1x2 32 bit array |
| bigPart | upper 32 bits |
| littlePart | lower 32 bits |
Definition at line 781 of file LTC6947.cpp.
| boolean lt64 | ( | unsigned long | an[], |
| unsigned long | ann[] | ||
| ) |
64 bit, if an < ann, then true
| an | 64 bit number, in 1x2 32bit array |
| ann | 64 bit number, in 1x2 32bit array |
Definition at line 917 of file LTC6947.cpp.
| unsigned long LTC6947_calc_odiv | ( | unsigned long | frf[2] | ) |
calculates the output divider setting based on the frf and on board VCO frequencies of LTC6947
| frf | output frequency |
Definition at line 534 of file LTC6947.cpp.
| void LTC6947_init | ( | ) |
Initializes the SPI MAP arrays The values set in initialization are used for all the LTC6947 SPI/WRITE and read functions (set_LTC6947_SPI_FIELD, get_LTC6947_SPI_FIELD, LTC6947_read, LTC6947_write, etc, etc)
Definition at line 302 of file LTC6947.cpp.
| uint8_t LTC6947_read | ( | uint8_t | cs, |
| int8_t | address | ||
| ) |
LTC6947 Read Single Address reads 8 bit Data field to LTC6947.
has to shift data by one bit to account for RW bit
| cs | Chip Select Pin |
| address | Register address for the LTC6947. |
Definition at line 98 of file LTC6947.cpp.
| long LTC6947_read_field | ( | uint8_t | cs, |
| uint8_t | address, | ||
| uint8_t | MSB_loc, | ||
| uint8_t | numbits | ||
| ) |
LTC6947 Read Single Field For SPI FIELDS located in 1 or multiple address location reads specific address locations identifies and returns specific field in question can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| address | Register address for the LTC6947. |
| MSB_loc | MSB bit location of field |
| numbits | length of field (i.e. number of bits in field) |
Definition at line 118 of file LTC6947.cpp.
| void LTC6947_set_frf | ( | ) |
FUNCTION: LTC6947_set_frf Calculates the integer (N), fractional (NUM) and output divider (OD) SPI values using self created 64bit math functions.
Datasheet equations:
fpfd = fref/R
can be modified to the following equations:
where:
Linduino One (Arduino Uno) is limited to 32 bit floats/double/long. 32 bit math functions will create rounding errors with the above equations, that can result in frequency errors. Therefore, the following code uses self created 64bit functions for 64bit integer math.
step 1: create 64 bit frf and fref numbers
step 2: calculate O (output divider)
step 3: get current R-divider setting
step 4: calculate frf*O*R max bit count/resolution: 33b+3b+5b= 41b
step 5: calculate N(10b), using value from step 1 N = (int) frf*O*R/fref max bit count/resolution: 41b-23b = 18b
step 6: calculate NUM (18b)
NUM = (int) [2^18 * (frf*O*R/fref -N)]
to get the correct value the above calculation are performed like this
Definition at line 623 of file LTC6947.cpp.
| void LTC6947_write | ( | uint8_t | cs, |
| uint8_t | address, | ||
| uint8_t | Data | ||
| ) |
LTC6947 Write Single Address writes 8 bit Data field to LTC6947.
has to shift data by one bit to account for RW bit
| cs | Chip Select Pin |
| address | Register address for the LTC6947. |
| Data | 8-bit data to be written to register |
Definition at line 165 of file LTC6947.cpp.
| uint8_t LTC6947_write_field | ( | uint8_t | cs, |
| long | field_data, | ||
| uint8_t | address, | ||
| uint8_t | MSB_loc, | ||
| uint8_t | numbits | ||
| ) |
LTC6947 Write Single Field For SPI FIELDS in 1 or multiple address locations reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| field_data | Value field value to be set to |
| address | Register address for the LTC6947. |
| MSB_loc | MSB bit location of field |
| numbits | length of field (i.e. number of bits in field) |
Definition at line 181 of file LTC6947.cpp.
| void mul64 | ( | unsigned long | an[], |
| unsigned long | ann[] | ||
| ) |
64 bit multiply, an=an*ann
| an | 64 bit number, in 1x2 32bit array |
| ann | 64 bit number, in 1x2 32bit array |
Definition at line 975 of file LTC6947.cpp.
| void prt | ( | unsigned long | an[] | ) |
Prints HEX representation of 64 bit an.
| an | 64 bit number, in 1x2 32bit array |
Definition at line 767 of file LTC6947.cpp.
| void set_LTC6947_ALLREGS | ( | uint8_t | cs, |
| uint8_t | reg01, | ||
| uint8_t | reg02, | ||
| uint8_t | reg03, | ||
| uint8_t | reg04, | ||
| uint8_t | reg05, | ||
| uint8_t | reg06, | ||
| uint8_t | reg07, | ||
| uint8_t | reg08, | ||
| uint8_t | reg09, | ||
| uint8_t | reg0A, | ||
| uint8_t | reg0B, | ||
| uint8_t | reg0C, | ||
| uint8_t | reg0D | ||
| ) |
Writes values to ALL LTC6947 RW addresses.
| cs | Chip Select Pin |
| reg01 | LTC6947 register 1 |
| reg02 | LTC6947 register 2 |
| reg03 | LTC6947 register 3 |
| reg04 | LTC6947 register 4 |
| reg05 | LTC6947 register 5 |
| reg06 | LTC6947 register 6 |
| reg07 | LTC6947 register 7 |
| reg08 | LTC6947 register 8 |
| reg09 | LTC6947 register 9 |
| reg0A | LTC6947 register 10 |
| reg0B | LTC6947 register 11 |
| reg0C | LTC6947 register 12 |
| reg0D | LTC6947 register 13 |
Definition at line 275 of file LTC6947.cpp.
| void set_LTC6947_global_fref | ( | unsigned long | fref_MHz, |
| unsigned long | fref_Hz | ||
| ) |
sets globals LTC6947_Fref_MHz and LTC6947_Fref_Hz
Definition at line 466 of file LTC6947.cpp.
| void set_LTC6947_global_frf | ( | unsigned long | frf_MHz, |
| unsigned long | frf_Hz | ||
| ) |
sets globals LTC6947_Frf_MHz and LTC6947_Frf_Hz
Definition at line 472 of file LTC6947.cpp.
| void set_LTC6947_global_vcolim | ( | unsigned long | fvco_max_MHz, |
| unsigned long | fvco_max_Hz, | ||
| unsigned long | fvco_min_MHz, | ||
| unsigned long | fvco_min_Hz | ||
| ) |
sets globals LTC6947_VCO_Max_Freq_MHz, LTC6947_VCO_Max_Freq_Hz, LTC6947_VCO_Min_Freq_MHz and LTC6947_VCO_Min_Freq_Hz
Definition at line 478 of file LTC6947.cpp.
| void set_LTC6947_SPI_FIELD | ( | uint8_t | cs, |
| uint8_t | f, | ||
| long | field_data | ||
| ) |
Sets the LTC6947 SPI field value calls function LTC6947_read_field, which reads specific address/field location then writes to specific field can handle SPI fields in multiple addresses, if MSB bit is in the lower number address.
| cs | Chip Select Pin |
| f | SPI field number |
| field_data | Value field value to be set to |
Definition at line 265 of file LTC6947.cpp.
| void shl64 | ( | unsigned long | an[] | ) |
Single Bit shift left of equivalent 64 bit number (an[] = an[]<<1)
| an | an[] = an[]<<1 |
Definition at line 817 of file LTC6947.cpp.
| void shl64by | ( | unsigned long | an[], |
| uint8_t | shiftnum | ||
| ) |
Multi Bit shift left of equivalent 64 bit number (an[] = an[]<<shiftnum)
| an | an[] = an[]<<shiftnum |
| shiftnum | number of bits to shift left |
Definition at line 843 of file LTC6947.cpp.
| void shr64 | ( | unsigned long | an[] | ) |
Single Bit shift right of equivalent 64 bit number (an[] = an[]<<1)
| an | an[] = an[]>>shiftnum |
Definition at line 830 of file LTC6947.cpp.
| void shr64by | ( | unsigned long | an[], |
| uint8_t | shiftnum | ||
| ) |
Multi Bit shift right of equivalent 64 bit number (an[] = an[]>>shiftnum)
| an | an[] = an[]>>shiftnum |
| shiftnum | number of bits to shift right |
Definition at line 861 of file LTC6947.cpp.
| void sub64 | ( | unsigned long | an[], |
| unsigned long | ann[] | ||
| ) |
64 bit Subtract ann from an (an[] = an[] - ann[])
| an | 64 bit number, in 1x2 32bit array |
| ann | 64 bit number, in 1x2 32bit array |
Definition at line 892 of file LTC6947.cpp.
| unsigned long LTC6947_Fref_Hz = 0 |
Default Fref frequency - Hz portion (yyy,yyy); Fref = x,xxx, yyy,yyy.
Definition at line 83 of file LTC6947.cpp.
| unsigned long LTC6947_Fref_MHz = 100 |
Default Fref frequency - MHz portion (xxx); Fref = xxx, yyy,yyy.
Definition at line 82 of file LTC6947.cpp.
| unsigned long LTC6947_Frf_Hz = 0 |
Default Frf frequency - Hz portion (yyy,yyy); Frf = x,xxx, yyy,yyy.
Definition at line 85 of file LTC6947.cpp.
| unsigned long LTC6947_Frf_MHz = 2415 |
Default Frf frequency - MHz portion (xxxx); Frf = x,xxx, yyy,yyy.
Definition at line 84 of file LTC6947.cpp.
| uint8_t LTC6947_reg[LTC6947_NUM_REGADDR] |
number of LTC6947 spi addresses
Definition at line 79 of file LTC6947.cpp.
| uint8_t LTC6947_spi_map[(LTC6947_NUM_REGFIELD+1)][4] |
LTC6947 spi map, stores MSB address location, MSB bit location, field length in bits, and R or RW capability.
Definition at line 80 of file LTC6947.cpp.
| unsigned long LTC6947_VCO_Max_Freq_Hz = 0 |
Max Vco frequency for default on board VCO - Hz portion (yyy,yyy); Fvco max = x,xxx, yyy,yyy.
Definition at line 88 of file LTC6947.cpp.
| unsigned long LTC6947_VCO_Max_Freq_MHz = 2536 |
Max Vco frequency for default on board VCO - MHz portion (xxxx); Fvco max = xxx, yyy,yyy.
Definition at line 86 of file LTC6947.cpp.
| unsigned long LTC6947_VCO_Min_Freq_Hz = 0 |
Min Vco frequency for default on board VCO - Hz portion (yyy,yyy); Fvco min= x,xxx, yyy,yyy.
Definition at line 89 of file LTC6947.cpp.
| unsigned long LTC6947_VCO_Min_Freq_MHz = 2328 |
Min Vco frequency for default on board VCO - MHz portion (xxxx); Fvco min = x,xxx, yyy,yyy.
Definition at line 87 of file LTC6947.cpp.
| unsigned long zero64[] = {0,0} |
for 64bit math functions
Definition at line 91 of file LTC6947.cpp.