![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC6115 High Voltage High Side Current and Voltage Sense. More...
LTC6115 High Voltage High Side Current and Voltage Sense.
The LTC6115 is a versatile combination of a high voltage, high side current sense amplifier and a voltage sense amplifier.
https://www.analog.com/en/products/ltc6115.html
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
The views and conclusions contained in the software and documentation are those of the authors and should not be interpreted as representing official policies, either expressed or implied, of Analog Devices Inc.
The Analog Devices Linduino is not affiliated with the official Arduino team. However, the Linduino is only possible because of the Arduino team's commitment to the open-source community. Please, visit http://www.arduino.cc and http://store.arduino.cc , and consider a purchase that will help fund their ongoing work.
Copyright 2018 Analog Devices Inc. (ADI)
Header for LTC6115: High-V High Side Current and Voltage Sense.
Definition in file LTC6115.h.
Go to the source code of this file.
Functions | |
| void | LTC6115_initialize () |
| |Function Declarations| More... | |
| float | LTC6115ConvertToVolts (uint32_t val) |
| This function converts ADC code to Voltage. More... | |
| float | LTC6115ConvertToAmps (uint32_t val) |
| This function converts ADC code to Current. More... | |
| void | LTC6115ChangeVGain (float val) |
| This function changes the Voltage gain. More... | |
| void | LTC6115ChangeIGain (float val) |
| This function changes the Current gain. More... | |
| float | LTC6115ToVolts (uint32_t val) |
| This function converts ADC code to Voltage without the converted voltage print statement. More... | |
| float | LTC6115ToAmps (uint32_t val) |
| This function converts ADC code to Current without the converted current print statement. More... | |
| uint32_t | millsToHz (uint32_t val) |
| This function converts milliseconds to frequency (Hz). More... | |
| float | getVGain () |
| This function returns the voltage gain (V/V). More... | |
| float | getIGain () |
| This function returns the current gain (V/A). More... | |
Macros | |
| #define | NUMBITS 10 |
| #define | MAXADCVAL 1023 |
| #define | AREF float(5) |
| #define | LTC6115_VIN 3 |
| Pin Mapping. More... | |
| #define | LTC6115_IIN 0 |
| Maps to DC2026 J7.1, ADC channel 1. More... | |
| float getIGain | ( | ) |
This function returns the current gain (V/A).
Definition at line 109 of file LTC6115.cpp.
| float getVGain | ( | ) |
This function returns the voltage gain (V/V).
Definition at line 100 of file LTC6115.cpp.
| void LTC6115_initialize | ( | ) |
|Function Declarations|
This function will initialize 6115 variables.
|Function Declarations|
Definition at line 92 of file LTC6115.cpp.
| void LTC6115ChangeIGain | ( | float | val | ) |
This function changes the Current gain.
| val | The value to change the Current gain to |
Definition at line 162 of file LTC6115.cpp.
| void LTC6115ChangeVGain | ( | float | val | ) |
This function changes the Voltage gain.
| val | The value to change the Voltage gain to |
Definition at line 155 of file LTC6115.cpp.
| float LTC6115ConvertToAmps | ( | uint32_t | val | ) |
This function converts ADC code to Current.
| val | The ADC code value to convert to Current |
Definition at line 137 of file LTC6115.cpp.
| float LTC6115ConvertToVolts | ( | uint32_t | val | ) |
This function converts ADC code to Voltage.
| val | The ADC code value to convert to Voltage |
Definition at line 118 of file LTC6115.cpp.
| float LTC6115ToAmps | ( | uint32_t | val | ) |
This function converts ADC code to Current without the converted current print statement.
Definition at line 146 of file LTC6115.cpp.
| float LTC6115ToVolts | ( | uint32_t | val | ) |
This function converts ADC code to Voltage without the converted voltage print statement.
Definition at line 128 of file LTC6115.cpp.
| uint32_t millsToHz | ( | uint32_t | val | ) |
This function converts milliseconds to frequency (Hz).
| val | The milliseconds to convert to Hz |
Definition at line 169 of file LTC6115.cpp.
| #define LTC6115_VIN 3 |