![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC6115 High-Voltage High Side Current and Voltage Sense. More...
Library for LTC6115 High-Voltage High Side Current and Voltage Sense.
Definition in file LTC6115.cpp.
Go to the source code of this file.
Functions | |
| void | LTC6115_initialize () |
| This function will initialize 6115 variables. More... | |
| float | getVGain () |
| This function returns the voltage gain (V/V). More... | |
| float | getIGain () |
| This function returns the current gain (V/A). More... | |
| float | LTC6115ConvertToVolts (uint32_t val) |
| This function converts ADC code to Voltage. More... | |
| float | LTC6115ToVolts (uint32_t val) |
| This function converts ADC code to Voltage without the converted voltage print statement. More... | |
| float | LTC6115ConvertToAmps (uint32_t val) |
| This function converts ADC code to Current. More... | |
| float | LTC6115ToAmps (uint32_t val) |
| This function converts ADC code to Current without the converted current print statement. More... | |
| void | LTC6115ChangeVGain (float val) |
| This function changes the Voltage gain. More... | |
| void | LTC6115ChangeIGain (float val) |
| This function changes the Current gain. More... | |
| uint32_t | millsToHz (uint32_t val) |
| This function converts milliseconds to frequency (Hz). More... | |
Variables | |
| float | LTC6115_VGain = 0 |
| 6115 Primary Variables More... | |
| float | LTC6115_IGain = 0 |
| float getIGain | ( | ) |
This function returns the current gain (V/A).
Definition at line 109 of file LTC6115.cpp.
| float getVGain | ( | ) |
This function returns the voltage gain (V/V).
Definition at line 100 of file LTC6115.cpp.
| void LTC6115_initialize | ( | ) |
This function will initialize 6115 variables.
|Function Declarations|
Definition at line 92 of file LTC6115.cpp.
| void LTC6115ChangeIGain | ( | float | val | ) |
This function changes the Current gain.
| val | The value to change the Current gain to |
Definition at line 162 of file LTC6115.cpp.
| void LTC6115ChangeVGain | ( | float | val | ) |
This function changes the Voltage gain.
| val | The value to change the Voltage gain to |
Definition at line 155 of file LTC6115.cpp.
| float LTC6115ConvertToAmps | ( | uint32_t | val | ) |
This function converts ADC code to Current.
| val | The ADC code value to convert to Current |
Definition at line 137 of file LTC6115.cpp.
| float LTC6115ConvertToVolts | ( | uint32_t | val | ) |
This function converts ADC code to Voltage.
| val | The ADC code value to convert to Voltage |
Definition at line 118 of file LTC6115.cpp.
| float LTC6115ToAmps | ( | uint32_t | val | ) |
This function converts ADC code to Current without the converted current print statement.
Definition at line 146 of file LTC6115.cpp.
| float LTC6115ToVolts | ( | uint32_t | val | ) |
This function converts ADC code to Voltage without the converted voltage print statement.
Definition at line 128 of file LTC6115.cpp.
| uint32_t millsToHz | ( | uint32_t | val | ) |
This function converts milliseconds to frequency (Hz).
| val | The milliseconds to convert to Hz |
Definition at line 169 of file LTC6115.cpp.
| float LTC6115_IGain = 0 |
Definition at line 85 of file LTC6115.cpp.
| float LTC6115_VGain = 0 |
6115 Primary Variables
Definition at line 84 of file LTC6115.cpp.