![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC4245 Hot Swap Controller with I2C Compatible Monitoring. More...
Library for LTC4245 Hot Swap Controller with I2C Compatible Monitoring.
Definition in file LTC4245.cpp.
Go to the source code of this file.
Functions | |
| float | LTC4245_code_to_voltage (uint8_t register_code, float full_scale_voltage) |
| Calculates voltage from register code data. More... | |
| int8_t | LTC4245_ARA (uint8_t alert_response_address, uint8_t *i2c_address) |
| SMBus Alert ResponseProtocol: Sends an alert response command and releases /ALERT pin. More... | |
| int8_t | LTC4245_write (uint8_t i2c_address, uint8_t command, uint8_t code) |
| Write an 8-bit code to the LTC4245. More... | |
| int8_t | LTC4245_read (uint8_t i2c_address, uint8_t command, uint8_t *code) |
| Reads an 8-bit adc_code from LTC4245. More... | |
| int8_t LTC4245_ARA | ( | uint8_t | alert_response_address, |
| uint8_t * | i2c_address | ||
| ) |
SMBus Alert ResponseProtocol: Sends an alert response command and releases /ALERT pin.
LTC4245 responds with its address
| alert_response_address | the Alert Response Address on the I2C bus |
| i2c_address | the address of the alert source |
Definition at line 82 of file LTC4245.cpp.
| float LTC4245_code_to_voltage | ( | uint8_t | register_code, |
| float | full_scale_voltage | ||
| ) |
Calculates voltage from register code data.
| full_scale_voltage | Data from registers Full scale voltage |
Definition at line 73 of file LTC4245.cpp.
| int8_t LTC4245_read | ( | uint8_t | i2c_address, |
| uint8_t | command, | ||
| uint8_t * | code | ||
| ) |
Reads an 8-bit adc_code from LTC4245.
| command | LTC4245 I2C ADDRESS |
| code | Register address to read from Contents of the requested register |
Definition at line 98 of file LTC4245.cpp.
| int8_t LTC4245_write | ( | uint8_t | i2c_address, |
| uint8_t | command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC4245.
| command | LTC4245 I2C ADDRESS |
| code | Register address to be written into Data to be written into the register |
Definition at line 90 of file LTC4245.cpp.