![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC3676: Power management solution for application processors. More...
LTC3676: Power management solution for application processors.
The LTC3676 is a complete power management solution for advanced portable application processor-based systems. The device contains four synchronous step-down DC/DC converters for core, memory, I/O, and system on-chip (SoC) rails and three 300mA LDO regulators for low noise analog supplies. The LTC3676-1 has a 1.5A buck regulator configured to support DDR termination plus a VTTR reference output. An I2C serial port is used to control regulator enables, power-down sequencing, output voltage levels, dynamic voltage scaling, operating modes and status reporting. Regulator start-up is sequenced by connecting outputs to enable pins in the desired order or via the I2C port. System power-on, power-off and reset functions are controlled by pushbutton interface, pin inputs, or I2C. The LTC3676 supports i.MX, PXA and OMAP processors with eight independent rails at appropriate power levels. Other features include interface signals such as the VSTB pin that toggles between programmed run and standby output voltages on up to four rails simultaneously. The device is available in a 40-lead 6mm x 6mm QFN package. I2C DATA FORMAT (MSB FIRST);
http://www.linear.com/product/LTC3676
http://www.linear.com/product/LTC3676#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Library Header File for LTC3676: Power management solution for application processors
Definition in file LTC3676.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC3676_register_read (uint8_t i2c_address, uint8_t register_address, uint8_t *register_data) |
| Reads an 8-bit register from the LTC3676 using the standard repeated start format. More... | |
| int8_t | LTC3676_register_write (uint8_t i2c_address, uint8_t register_address, uint8_t register_data) |
| Writes to an 8-bit register inside the LTC3676 using the standard I2C repeated start format. More... | |
| int8_t | LTC3676_bit_set (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number) |
| Sets any bit inside the LTC3676 using the standard I2C repeated start format. More... | |
| int8_t | LTC3676_bit_clear (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number) |
| Clears any bit inside the LTC3676 using the standard I2C repeated start format. More... | |
| int8_t | LTC3676_bit_write (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number, uint8_t bit_data) |
| Writes any bit inside the LTC3676 using the standard I2C repeated start format. More... | |
| uint8_t | LTC3676_bit_is_set (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number) |
| Reads the value of any bit in any register or the LTC3676. More... | |
| float | LTC3676_set_buck_output_voltage (uint8_t i2c_address, uint8_t register_address, float output_voltage) |
| Sets the output voltage of any buck. More... | |
| float | LTC3676_set_buck_fb_ref (uint8_t i2c_address, uint8_t register_address, float fb_ref_voltage) |
| Writes the Feedback Reference Voltage of any buck. More... | |
| float | LTC3676_buck_vout_max (uint8_t buck_number) |
| Calculates the maximum output voltage of any buck in mV based on the feedback resistors. More... | |
| float | LTC3676_buck_vout_min (uint8_t buck_number) |
| Calculates the minimum output voltage of any buck in mV based on the feedback resistors. More... | |
| int8_t | LTC3676_select_buck_reference (uint8_t i2c_address, uint8_t buck_number, int8_t ref_char) |
| Selects the reference for the specified buck regulator(s). More... | |
| int8_t | LTC3676_set_buck_mode (uint8_t i2c_address, uint8_t buck_number, uint8_t mode) |
| Sets the switching mode for the specified Buck regulator. More... | |
| int8_t | LTC3676_set_startup_mode (uint8_t i2c_address, uint8_t buck_number, uint8_t startup_bit) |
| Sets the start-up mode for all bucks. More... | |
| int8_t | LTC3676_set_buck_pgood_mask (uint8_t i2c_address, uint8_t buck_number, uint8_t pgood_bit) |
| Sets the PGOOD mask bit in the DVBxB register for all bucks. More... | |
| int8_t | LTC3676_set_uv_warning_threshold (uint8_t i2c_address, float uv_warning_threshold) |
| Writes a new UV warning threshold voltage in the CTRL register. More... | |
| int8_t | LTC3676_set_overtemp_warning_level (uint8_t i2c_address, uint8_t ot_warning_level) |
| Writes the UV warning threshold of any buck. More... | |
| int8_t | LTC3676_1_set_ldo4_voltage (uint8_t i2c_address, uint8_t ldo4_output_voltage_code) |
| Sets LDO4 output voltage on the LTC3676-1. More... | |
| int8_t | LTC3676_set_buck_sequence_down (uint8_t i2c_address, uint8_t buck_number, uint8_t sequence_phase) |
| Sets the Sequence Down bits for any buck in the SQD1 register. More... | |
| int8_t | LTC3676_set_ldo_sequence_down (uint8_t i2c_address, uint8_t ldo_number, uint8_t sequence_phase) |
| Sets the Sequence Down bits for any buck in the SQD1 register. More... | |
Macros | |
I2C_ADDRESSES | |
I2C address of the LTC3676 and LTC3676-1. | |
| #define | LTC3676_I2C_ADDRESS 0x3C |
| #define | LTC3676_1_I2C_ADDRESS 0x3D |
FEEDBACK RESISTORS | |
Feedback resistor values for the DC1976A-A in kOhm. | |
| #define | LTC3676_RES_BUCK1_RTOP 1000. |
| #define | LTC3676_RES_BUCK1_RBOT 280. |
| #define | LTC3676_RES_BUCK2_RTOP 1000. |
| #define | LTC3676_RES_BUCK2_RBOT 1100. |
| #define | LTC3676_RES_BUCK3_RTOP 1000. |
| #define | LTC3676_RES_BUCK3_RBOT 1100. |
| #define | LTC3676_RES_BUCK4_RTOP 1000. |
| #define | LTC3676_RES_BUCK4_RBOT 931. |
REGISTERS | |
| #define | LTC3676_REG_BUCK1 0x01 |
| #define | LTC3676_REG_BUCK2 0x02 |
| #define | LTC3676_REG_BUCK3 0x03 |
| #define | LTC3676_REG_BUCK4 0x04 |
| #define | LTC3676_REG_LDOA 0x05 |
| #define | LTC3676_REG_LDOB 0x06 |
| #define | LTC3676_REG_SQD1 0x07 |
| #define | LTC3676_REG_SQD2 0x08 |
| #define | LTC3676_REG_CNTRL 0x09 |
| #define | LTC3676_REG_DVB1A 0x0A |
| #define | LTC3676_REG_DVB1B 0x0B |
| #define | LTC3676_REG_DVB2A 0x0C |
| #define | LTC3676_REG_DVB2B 0x0D |
| #define | LTC3676_REG_DVB3A 0x0E |
| #define | LTC3676_REG_DVB3B 0x0F |
| #define | LTC3676_REG_DVB4A 0x10 |
| #define | LTC3676_REG_DVB4B 0x11 |
| #define | LTC3676_REG_MSKIRQ 0x12 |
| #define | LTC3676_REG_MSKPG 0x13 |
| #define | LTC3676_REG_USER 0x14 |
| #define | LTC3676_REG_IRQSTAT 0x15 |
| #define | LTC3676_REG_PGSTATL 0x16 |
| #define | LTC3676_REG_PGSTATRT 0x17 |
| #define | LTC3676_REG_HRST 0x1E |
| #define | LTC3676_REG_CLIRQ 0x1F |
LTC3676_REG_BUCKx SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_BUCKx registers. | |
| #define | LTC3676_BUCK_ENABLE 7 |
| #define | LTC3676_BUCK_STARTUP 4 |
| #define | LTC3676_BUCK_PHASE_SEL 3 |
| #define | LTC3676_BUCK_CLOCK_RATE 2 |
| #define | LTC3676_BUCK_KEEP_ALIVE 1 |
| #define | LTC3676_BUCK_SLEW 0 |
LTC3676_REG_LDOA SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_LDOA register. | |
| #define | LTC3676_LDO3_ENABLE 5 |
| #define | LTC3676_LDO3_STARTUP 4 |
| #define | LTC3676_LDO3_KEEP_ALIVE 3 |
| #define | LTC3676_LDO2_ENABLE 2 |
| #define | LTC3676_LDO2_STARTUP 1 |
| #define | LTC3676_LDO2_KEEP_ALIVE 0 |
LTC3676_REG_LDOB SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_LDOB register. | |
| #define | LTC3676_LDO4_ENABLE 2 |
| #define | LTC3676_LDO4_STARTUP 1 |
| #define | LTC3676_LDO4_KEEP_ALIVE 0 |
LTC3676_REG_CNTRL SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_CNTRL register. | |
| #define | LTC3676_PWR_ON 7 |
| #define | LTC3676_PB_RESET_TMR 6 |
| #define | LTC3676_SOFTWARE_CNTRL 5 |
LTC3676_REG_DVBxA SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_DVBxA registers. | |
| #define | LTC3676_BUCK_REF_SELECT 5 |
LTC3676_REG_DVBxB SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_DVBxB register. | |
| #define | LTC3676_BUCK_PG_MASK 5 |
LTC3676_REG_MSKIRQ SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_MSKIRQ register. | |
| #define | LTC3676_MASK_OT_SHUTDOWN 6 |
| #define | LTC3676_MASK_OT_WARNING 5 |
| #define | LTC3676_MASK_UV_SHUTDOWN 4 |
| #define | LTC3676_MASK_UV_WARNING 3 |
| #define | LTC3676_MASK_PG_TIMEOUT 2 |
| #define | LTC3676_MASK_PB_STATUS 0 |
LTC3676_REG_MSKPG SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_MSKPG register. | |
| #define | LTC3676_ENABLE_PG_LDO4 7 |
| #define | LTC3676_ENABLE_PG_LDO3 6 |
| #define | LTC3676_ENABLE_PG_LDO2 5 |
| #define | LTC3676_ENABLE_PG_BUCK4 3 |
| #define | LTC3676_ENABLE_PG_BUCK3 2 |
| #define | LTC3676_ENABLE_PG_BUCK2 1 |
| #define | LTC3676_ENABLE_PG_BUCK1 0 |
LTC3676_REG_USER SETTINGS | |
Bit position of single bit settings in the LTC3676_REG_USER register. | |
| #define | LTC3676_USER_7 7 |
| #define | LTC3676_USER_6 6 |
| #define | LTC3676_USER_5 5 |
| #define | LTC3676_USER_4 4 |
| #define | LTC3676_USER_3 3 |
| #define | LTC3676_USER_2 2 |
| #define | LTC3676_USER_1 1 |
| #define | LTC3676_USER_0 0 |
LTC3676_REG_IRQSTAT SETTINGS | |
Bit position of status bits in the LTC3676_REG_IRQSTAT register. | |
| #define | LTC3676_IRQ_OT_SHUTDOWN 6 |
| #define | LTC3676_IRQ_OT_WARNING 5 |
| #define | LTC3676_IRQ_UV_SHUTDOWN 4 |
| #define | LTC3676_IRQ_UV_WARNING 3 |
| #define | LTC3676_IRQ_PG_TIMEOUT 2 |
| #define | LTC3676_IRQ_HARD_RESET 1 |
| #define | LTC3676_IRQ_PB_STATUS 0 |
LTC3676_REG_PGSTATL SETTINGS | |
Bit position of status bits in the LTC3676_REG_PGSTATL register. | |
| #define | LTC3676_PGL_LDO4 7 |
| #define | LTC3676_PGL_LDO3 6 |
| #define | LTC3676_PGL_LDO2 5 |
| #define | LTC3676_PGL_LDO1 4 |
| #define | LTC3676_PGL_BUCK4 3 |
| #define | LTC3676_PGL_BUCK3 2 |
| #define | LTC3676_PGL_BUCK2 1 |
| #define | LTC3676_PGL_BUCK1 0 |
LTC3676_REG_PGSTATRT SETTINGS | |
Bit position of status bits in the LTC3676_REG_PGSTATRT register. | |
| #define | LTC3676_PGRT_LDO4 7 |
| #define | LTC3676_PGRT_LDO3 6 |
| #define | LTC3676_PGRT_LDO2 5 |
| #define | LTC3676_PGRT_LDO1 4 |
| #define | LTC3676_PGRT_BUCK4 3 |
| #define | LTC3676_PGRT_BUCK3 2 |
| #define | LTC3676_PGRT_BUCK2 1 |
| #define | LTC3676_PGRT_BUCK1 0 |
LTC3676 MASK SETTINGS | |
Bitwise AND with register data to determine present setting. | |
| #define | LTC3676_BUCK_SEQ_MASK(num) (0x03<<((num)*2)-2) |
| #define | LTC3676_LDO_SEQ_MASK(num) (0x03<<((num-2)*2)) |
| #define | LTC3676_BUCK_MODE_MASK 0x60 |
| #define | LTC3676_BUCK4_SEQ_MASK 0xC0 |
| #define | LTC3676_BUCK3_SEQ_MASK 0x30 |
| #define | LTC3676_BUCK2_SEQ_MASK 0x0C |
| #define | LTC3676_BUCK1_SEQ_MASK 0x03 |
| #define | LTC3676_LDO4_SEQ_MASK 0x30 |
| #define | LTC3676_LDO3_SEQ_MASK 0x0C |
| #define | LTC3676_LDO2_SEQ_MASK 0x03 |
| #define | LTC3676_UV_WARN_THRESH_MASK 0x1C |
| #define | LTC3676_OT_WARN_LEVEL_MASK 0x03 |
| #define | LTC3676_FB_REF_MASK 0x1F |
LTC3676-1 ONLY MASK SETTINGS | |
Bitwise AND with register data to determine present setting. | |
| #define | LTC3676_1_LDO4_VOLTAGE_MASK 0x18 |
| int8_t LTC3676_1_set_ldo4_voltage | ( | uint8_t | i2c_address, |
| uint8_t | ldo4_output_voltage_code | ||
| ) |
Sets LDO4 output voltage on the LTC3676-1.
| i2c_address | I2C address of the LTC3676-1. |
| ldo4_output_voltage_code | Voltage code for new LDO4 output voltage: 0=1.2V, 1=2.5V, 2=2.8V, 3=3.0V |
Definition at line 341 of file LTC3676.cpp.
| int8_t LTC3676_bit_clear | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number | ||
| ) |
Clears any bit inside the LTC3676 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC3676. |
| register_address | Address of the LTC3676 register to be overwritten. This is also known as the "command byte". |
| bit_number | Address of the bit to set within the register. |
Definition at line 108 of file LTC3676.cpp.
| uint8_t LTC3676_bit_is_set | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number | ||
| ) |
Reads the value of any bit in any register or the LTC3676.
| i2c_address | I2C address of the LTC3676. |
| register_address | Address of the LTC3676 register to be read. This is also known as the "command byte". |
| bit_number | Bit location (0-7) to be read. |
Definition at line 137 of file LTC3676.cpp.
| int8_t LTC3676_bit_set | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number | ||
| ) |
Sets any bit inside the LTC3676 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC3676. |
| register_address | Address of the LTC3676 register to be overwritten. This is also known as the "command byte". |
| bit_number | Bit location (0-7) to be written. |
Definition at line 95 of file LTC3676.cpp.
| int8_t LTC3676_bit_write | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number, | ||
| uint8_t | bit_data | ||
| ) |
Writes any bit inside the LTC3676 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC3676. |
| register_address | Address of the LTC3676 register to be written. |
| bit_number | Bit location (0-7) to be written. |
| bit_data | Bit data (0 or 1) to be written. |
Definition at line 122 of file LTC3676.cpp.
| float LTC3676_buck_vout_max | ( | uint8_t | buck_number | ) |
Calculates the maximum output voltage of any buck in mV based on the feedback resistors.
| buck_number | Number (1-4) of buck. |
Definition at line 191 of file LTC3676.cpp.
| float LTC3676_buck_vout_min | ( | uint8_t | buck_number | ) |
Calculates the minimum output voltage of any buck in mV based on the feedback resistors.
| buck_number | Number (1-4) of buck. |
Definition at line 212 of file LTC3676.cpp.
| int8_t LTC3676_register_read | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t * | register_data | ||
| ) |
Reads an 8-bit register from the LTC3676 using the standard repeated start format.
| i2c_address | I2C address of the LTC3676. |
| register_address | Address of the LTC3676 register to be read. This is also known as the "command byte". |
| register_data | returns 8-bit value read from the LTC3676 register. |
Definition at line 78 of file LTC3676.cpp.
| int8_t LTC3676_register_write | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | register_data | ||
| ) |
Writes to an 8-bit register inside the LTC3676 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC3676. |
| register_address | Address of the LTC3676 register to be overwritten. This is also known as the "command byte". |
| register_data | Value that will be written to the register. |
Definition at line 86 of file LTC3676.cpp.
| int8_t LTC3676_select_buck_reference | ( | uint8_t | i2c_address, |
| uint8_t | buck_number, | ||
| int8_t | ref_char | ||
| ) |
Selects the reference for the specified buck regulator(s).
| i2c_address | I2C address of the LTC3676. |
| buck_number | Number (1-4) of the buck whose reference will be selected. Enter 0xFF for all bucks. |
| ref_char | Reference to select (A or B). |
Definition at line 233 of file LTC3676.cpp.
| float LTC3676_set_buck_fb_ref | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| float | fb_ref_voltage | ||
| ) |
Writes the Feedback Reference Voltage of any buck.
| i2c_address | I2C address of the LTC3676. |
| register_address | Address of the LTC3676 Buck FB reference register to be written. |
| fb_ref_voltage | New Feedback Reference voltage to set in mV. Values between 412.5 and 800 are allowed. |
Definition at line 176 of file LTC3676.cpp.
| int8_t LTC3676_set_buck_mode | ( | uint8_t | i2c_address, |
| uint8_t | buck_number, | ||
| uint8_t | mode | ||
| ) |
Sets the switching mode for the specified Buck regulator.
| i2c_address | I2C address of the LTC3676. |
| buck_number | Number (1-4) of the buck to set. Enter 0xFF for all bucks. |
| mode | Switching mode to be set (0=pulse skipping, 1=burst, 2=forced continuous) |
Definition at line 255 of file LTC3676.cpp.
| float LTC3676_set_buck_output_voltage | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| float | output_voltage | ||
| ) |
Sets the output voltage of any buck.
| i2c_address | I2C address of the LTC3676. |
| register_address | Address of the LTC3676 Buck FB reference register to be written. |
| output_voltage | New output voltage to set, in mV. Assumes a valid voltage for the feedback resistors. |
Definition at line 147 of file LTC3676.cpp.
| int8_t LTC3676_set_buck_pgood_mask | ( | uint8_t | i2c_address, |
| uint8_t | buck_number, | ||
| uint8_t | pgood_bit | ||
| ) |
Sets the PGOOD mask bit in the DVBxB register for all bucks.
| i2c_address | I2C address of the LTC3676. |
| buck_number | Number (1-4) of the buck to set. |
| pgood_bit | Data to write to PGOOD bit (0=PGOOD low when slewing, 1=PGOOD not forced low when slewing) |
Definition at line 293 of file LTC3676.cpp.
| int8_t LTC3676_set_buck_sequence_down | ( | uint8_t | i2c_address, |
| uint8_t | buck_number, | ||
| uint8_t | sequence_phase | ||
| ) |
Sets the Sequence Down bits for any buck in the SQD1 register.
| i2c_address | I2C address of the LTC3676. |
| buck_number | Number (1-4) of the buck to sequence. |
| sequence_phase | Sequence down phase: 0=with WAKE, 1=WAKE+100ms, 2=WAKE+200ms, 3=WAKE+300ms. |
Definition at line 354 of file LTC3676.cpp.
| int8_t LTC3676_set_ldo_sequence_down | ( | uint8_t | i2c_address, |
| uint8_t | ldo_number, | ||
| uint8_t | sequence_phase | ||
| ) |
Sets the Sequence Down bits for any buck in the SQD1 register.
| i2c_address | I2C address of the LTC3676. |
| ldo_number | Number (2-4) of the LDO to sequence. |
| sequence_phase | Sequence down phase: 0=with WAKE, 1=WAKE+100ms, 2=WAKE+200ms, 3=WAKE+300ms. |
Definition at line 368 of file LTC3676.cpp.
| int8_t LTC3676_set_overtemp_warning_level | ( | uint8_t | i2c_address, |
| uint8_t | ot_warning_level | ||
| ) |
Writes the UV warning threshold of any buck.
| i2c_address | I2C address of the LTC3676. |
| ot_warning_level | New overtemp warning level to set, degrees C below Overtemperature fault level. Values 10, 20, 30, and 40 are allowed. |
Definition at line 326 of file LTC3676.cpp.
| int8_t LTC3676_set_startup_mode | ( | uint8_t | i2c_address, |
| uint8_t | buck_number, | ||
| uint8_t | startup_bit | ||
| ) |
Sets the start-up mode for all bucks.
| i2c_address | I2C address of the LTC3676. |
| buck_number | Number (1-4) of the buck to set. Enter 0xFF for all bucks. |
| startup_bit | Data to write to start-up bit (0=enable at any output, 1=enable only if output <300mV) |
Definition at line 276 of file LTC3676.cpp.
| int8_t LTC3676_set_uv_warning_threshold | ( | uint8_t | i2c_address, |
| float | uv_warning_threshold | ||
| ) |
Writes a new UV warning threshold voltage in the CTRL register.
| i2c_address | I2C address of the LTC3676. |
| uv_warning_threshold | New UV warning threshold to set, in volts. Values between 2.7 and 3.4 are allowed. |
Definition at line 311 of file LTC3676.cpp.