![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC3589: 8-Output Regulator with Sequencing and I2C. More...
Library for LTC3589: 8-Output Regulator with Sequencing and I2C.
Definition in file LTC3589.cpp.
Go to the source code of this file.
Functions | |
| int8_t | LTC3589_register_read (uint8_t i2c_address, uint8_t register_address, uint8_t *register_data) |
| Reads an 8-bit register from the LTC3589 using the standard repeated start format. More... | |
| int8_t | LTC3589_register_write (uint8_t i2c_address, uint8_t register_address, uint8_t register_data) |
| Writes to an 8-bit register inside the LTC3589 using the standard I2C repeated start format. More... | |
| int8_t | LTC3589_bit_set (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number) |
| Sets any bit inside the LTC3589 using the standard I2C repeated start format. More... | |
| int8_t | LTC3589_bit_clear (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number) |
| Clears any bit inside the LTC3589 using the standard I2C repeated start format. More... | |
| int8_t | LTC3589_bit_write (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number, uint8_t bit_data) |
| Writes any bit inside the LTC3589 using the standard I2C repeated start format. More... | |
| uint8_t | LTC3589_bit_is_set (uint8_t i2c_address, uint8_t register_address, uint8_t bit_number) |
| Reads the value of any bit in any register or the LTC3589. More... | |
| float | LTC3589_set_ldo2_output_voltage (uint8_t i2c_address, uint8_t register_address, float output_voltage) |
| Sets the output voltage of LDO2. More... | |
| float | LTC3589_set_buck_output_voltage (uint8_t i2c_address, uint8_t register_address, float output_voltage) |
| Sets the output voltage of any buck. More... | |
| float | LTC3589_set_ldo2_fb_ref (uint8_t i2c_address, uint8_t register_address, float fb_ref_voltage) |
| Writes the Feedback Reference Voltage of LDO2. More... | |
| float | LTC3589_set_buck_fb_ref (uint8_t i2c_address, uint8_t register_address, float fb_ref_voltage) |
| Writes the Feedback Reference Voltage of any buck. More... | |
| float | LTC3589_ldo2_vout_max () |
| Calculates the maximum output voltage of LDO2 in mV based on the feedback resistors. More... | |
| float | LTC3589_ldo2_vout_min () |
| Calculates the minimum output voltage of LDO2 mV based on the feedback resistors. More... | |
| float | LTC3589_buck_vout_max (uint8_t buck_number) |
| Calculates the maximum output voltage of any buck in mV based on the feedback resistors. More... | |
| float | LTC3589_buck_vout_min (uint8_t buck_number) |
| Calculates the minimum output voltage of any buck in mV based on the feedback resistors. More... | |
| int8_t | LTC3589_select_ldo2_reference (uint8_t i2c_address, int8_t ref_char) |
| Selects the reference for LDO2. More... | |
| int8_t | LTC3589_select_buck_reference (uint8_t i2c_address, uint8_t buck_number, int8_t ref_char) |
| Selects the reference for the specified buck regulator(s). More... | |
| int8_t | LTC3589_set_buck_mode (uint8_t i2c_address, uint8_t buck_number, uint8_t mode) |
| Sets the switching mode for the specified buck regulator(s). More... | |
| int8_t | LTC3589_set_buckboost_mode (uint8_t i2c_address, uint8_t mode) |
| Sets the switching mode for the buck-boost regulator. More... | |
| int8_t | LTC3589_set_startup_mode (uint8_t i2c_address, uint8_t startup_bit) |
| Sets the start-up mode for all regulators. More... | |
| int8_t | LTC3589_set_pgood_mask (uint8_t i2c_address, uint8_t pgood_bit) |
| Sets the PGOOD mask bit for all bucks and LDO2. More... | |
| int8_t | LTC3589_set_ldo4_voltage (uint8_t i2c_address, uint8_t ldo4_output_voltage_code) |
| Sets LDO4 output voltage on the LTC3589. More... | |
| int8_t | LTC3589_set_regulator_slew (uint8_t i2c_address, uint8_t regulator_mask, uint8_t slew_rate) |
| Sets the dynamnic reference slew rate for the regulator(s). More... | |
| int8_t | LTC3589_set_switch_dvdt_control (uint8_t i2c_address, uint8_t dvdt_control_bits) |
| Sets the switch DV/DT control for the buck regulators. More... | |
| int8_t | LTC3589_set_go_bits (uint8_t i2c_address) |
| Sets all of the GO bits in the VCCR register. More... | |
| int8_t LTC3589_bit_clear | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number | ||
| ) |
Clears any bit inside the LTC3589 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 register to be overwritten. This is also known as the "command byte". |
| bit_number | Address of the bit to set within the register. |
Definition at line 113 of file LTC3589.cpp.
| uint8_t LTC3589_bit_is_set | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number | ||
| ) |
Reads the value of any bit in any register or the LTC3589.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 register to be read. This is also known as the "command byte". |
| bit_number | Bit location (0-7) to be read. |
Definition at line 140 of file LTC3589.cpp.
| int8_t LTC3589_bit_set | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number | ||
| ) |
Sets any bit inside the LTC3589 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 register to be overwritten. This is also known as the "command byte". |
| bit_number | Bit location (0-7) to be written. |
Definition at line 100 of file LTC3589.cpp.
| int8_t LTC3589_bit_write | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bit_number, | ||
| uint8_t | bit_data | ||
| ) |
Writes any bit inside the LTC3589 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 register to be written. |
| bit_number | Bit location (0-7) to be written. |
| bit_data | Bit data (0 or 1) to be written. |
Definition at line 126 of file LTC3589.cpp.
| float LTC3589_buck_vout_max | ( | uint8_t | buck_number | ) |
Calculates the maximum output voltage of any buck in mV based on the feedback resistors.
| buck_number | Number (1-3) of buck. |
Definition at line 229 of file LTC3589.cpp.
| float LTC3589_buck_vout_min | ( | uint8_t | buck_number | ) |
Calculates the minimum output voltage of any buck in mV based on the feedback resistors.
| buck_number | Number (1-3) of buck. |
Definition at line 246 of file LTC3589.cpp.
| float LTC3589_ldo2_vout_max | ( | ) |
Calculates the maximum output voltage of LDO2 in mV based on the feedback resistors.
Definition at line 217 of file LTC3589.cpp.
| float LTC3589_ldo2_vout_min | ( | ) |
Calculates the minimum output voltage of LDO2 mV based on the feedback resistors.
Definition at line 223 of file LTC3589.cpp.
| int8_t LTC3589_register_read | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t * | register_data | ||
| ) |
Reads an 8-bit register from the LTC3589 using the standard repeated start format.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 register to be read. This is also known as the "command byte". |
| register_data | returns 8-bit value read from the LTC3589 register. |
Definition at line 84 of file LTC3589.cpp.
| int8_t LTC3589_register_write | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | register_data | ||
| ) |
Writes to an 8-bit register inside the LTC3589 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 register to be overwritten. This is also known as the "command byte". |
| register_data | Value that will be written to the register. |
Definition at line 92 of file LTC3589.cpp.
| int8_t LTC3589_select_buck_reference | ( | uint8_t | i2c_address, |
| uint8_t | buck_number, | ||
| int8_t | ref_char | ||
| ) |
Selects the reference for the specified buck regulator(s).
| i2c_address | I2C address of the LTC3589. |
| buck_number | Number (1-3) of the buck whose reference will be selected. Enter 0xFF for all bucks. |
| ref_char | Reference to select (A or B). |
Definition at line 275 of file LTC3589.cpp.
| int8_t LTC3589_select_ldo2_reference | ( | uint8_t | i2c_address, |
| int8_t | ref_char | ||
| ) |
Selects the reference for LDO2.
| i2c_address | I2C address of the LTC3589. |
| ref_char | Reference to select (A or B). |
Definition at line 263 of file LTC3589.cpp.
| float LTC3589_set_buck_fb_ref | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| float | fb_ref_voltage | ||
| ) |
Writes the Feedback Reference Voltage of any buck.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 Buck FB reference register to be written. |
| fb_ref_voltage | New Feedback Reference voltage to set in mV. Values between 362.5 and 750 are allowed. |
Definition at line 202 of file LTC3589.cpp.
| int8_t LTC3589_set_buck_mode | ( | uint8_t | i2c_address, |
| uint8_t | buck_number, | ||
| uint8_t | mode | ||
| ) |
Sets the switching mode for the specified buck regulator(s).
| i2c_address | I2C address of the LTC3589. |
| buck_number | Number (1-3) of the buck to set. Enter 0xFF for all bucks. |
| mode | Switching mode to be set (0=pulse skipping, 1=burst, 2=forced continuous) |
Definition at line 294 of file LTC3589.cpp.
| float LTC3589_set_buck_output_voltage | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| float | output_voltage | ||
| ) |
Sets the output voltage of any buck.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 Buck FB reference register to be written. |
| output_voltage | New output voltage to set, in mV. Assumes a valid voltage for the feedback resistors. |
Definition at line 164 of file LTC3589.cpp.
| int8_t LTC3589_set_buckboost_mode | ( | uint8_t | i2c_address, |
| uint8_t | mode | ||
| ) |
Sets the switching mode for the buck-boost regulator.
| i2c_address | I2C address of the LTC3589. |
| mode | Switching mode to be set (0=pulse skipping, 1=burst, 2=forced continuous) |
Definition at line 313 of file LTC3589.cpp.
| int8_t LTC3589_set_go_bits | ( | uint8_t | i2c_address | ) |
Sets all of the GO bits in the VCCR register.
| i2c_address | I2C address of the LTC3589. |
Definition at line 392 of file LTC3589.cpp.
| float LTC3589_set_ldo2_fb_ref | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| float | fb_ref_voltage | ||
| ) |
Writes the Feedback Reference Voltage of LDO2.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 LDO2 FB reference register to be written. |
| fb_ref_voltage | New Feedback Reference voltage to set in mV. Values between 362.5 and 750 are allowed. |
Definition at line 187 of file LTC3589.cpp.
| float LTC3589_set_ldo2_output_voltage | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| float | output_voltage | ||
| ) |
Sets the output voltage of LDO2.
| i2c_address | I2C address of the LTC3589. |
| register_address | Address of the LTC3589 LDO2 FB reference register to be written. |
| output_voltage | New output voltage to set, in mV. Assumes a valid voltage for the feedback resistors. |
Definition at line 151 of file LTC3589.cpp.
| int8_t LTC3589_set_ldo4_voltage | ( | uint8_t | i2c_address, |
| uint8_t | ldo4_output_voltage_code | ||
| ) |
Sets LDO4 output voltage on the LTC3589.
| i2c_address | I2C address of the LTC3589. |
| ldo4_output_voltage_code | Voltage code for new LDO4 output voltage (varies by part option). |
Definition at line 347 of file LTC3589.cpp.
| int8_t LTC3589_set_pgood_mask | ( | uint8_t | i2c_address, |
| uint8_t | pgood_bit | ||
| ) |
Sets the PGOOD mask bit for all bucks and LDO2.
| i2c_address | I2C address of the LTC3589. |
| pgood_bit | Data to write to PGOOD bit (0=PGOOD low when slewing, 1=PGOOD not forced low when slewing) |
Definition at line 336 of file LTC3589.cpp.
| int8_t LTC3589_set_regulator_slew | ( | uint8_t | i2c_address, |
| uint8_t | regulator_mask, | ||
| uint8_t | slew_rate | ||
| ) |
Sets the dynamnic reference slew rate for the regulator(s).
| i2c_address | I2C address of the LTC3589. |
| regulator_mask | Mask of the regulator to set. Enter 0xFF for all regulators. |
| slew_rate | Slew rate code to set. |
Definition at line 359 of file LTC3589.cpp.
| int8_t LTC3589_set_startup_mode | ( | uint8_t | i2c_address, |
| uint8_t | startup_bit | ||
| ) |
Sets the start-up mode for all regulators.
| i2c_address | I2C address of the LTC3589. |
| startup_bit | Data to write to start-up bit (0=enable at any output, 1=enable only if output <300mV) |
Definition at line 322 of file LTC3589.cpp.
| int8_t LTC3589_set_switch_dvdt_control | ( | uint8_t | i2c_address, |
| uint8_t | dvdt_control_bits | ||
| ) |
Sets the switch DV/DT control for the buck regulators.
| i2c_address | I2C address of the LTC3589. |
| dvdt_control_bits | Two-bit DV/DT control code to set. |
Definition at line 380 of file LTC3589.cpp.