![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC3335: Nanopower Buck-Boost DC/DC with Integrated Coulomb Counter. More...
LTC3335: Nanopower Buck-Boost DC/DC with Integrated Coulomb Counter.
This header file contains the definitions that allow configuration of the LTC3335 driver. The definitions belong to two groups:
The LTC®3335 is a high efficiency, low quiescent current (680nA) buck-boost DC/DC converter with an integrated precision coulomb counter which monitors accumulated battery discharge in long life battery powered applications. The buck-boost can operate down to 1.8V on its input and provides eight pin-selectable output voltages with up to 50mA of output current. The coulomb counter stores the accumulated battery discharge in an internal register accessible via an I2C interface. The LTC3335 features a programmable discharge alarm threshold. When the threshold is reached, an interrupt is generated at the IRQ pin. To accommodate a wide range of battery types and sizes, the peak input current can be selected from as low as 5mA to as high as 250mA and the full-scale coulomb counter has a programmable range of 32,768:1.
http://www.linear.com/product/LTC3335
http://www.linear.com/product/LTC3335#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Configuration Header File for LTC3335: Nanopower Buck-Boost DC/DC with Integrated Coulomb Counter
Definition in file LTC3335_Config.h.
Go to the source code of this file.
Macros | |
| #define | LTC3335_IPEAK_CONFIGURATION LTC3335_IPEAK_CONFIGURATION_100MA |
| IPEAK setting from LTC3335_IPEAK_CONFIGURATION_TYPE in LTC3335.h. More... | |
| #define | LTC3335_OUTPUT_VOLTAGE LTC3335_OUTPUT_VOLTAGE_3_3V |
| VOUT setting from LTC3335_NUM_OUTPUT_VOLTAGES in LTC3335.h. More... | |
| #define | LTC3335_CAPACITY (2400) |
| in mAh, capacity of the battery More... | |
| #define | LTC3335_ALARM_CAPACITY 0.9*LTC3335_CAPACITY |
| in mAh, the capacity at which the alarm should be activated. More... | |
| #define | LTC3335_USE_CURRENT_MEASUREMENT true |
| Set to true to use the /IRQ pin to measure the battery current real time. More... | |
| #define | LTC3335_USE_SOFTWARE_CORRECTION false |
| Set to true to use software correction of coulomb count and current measurement. More... | |
| #define | LTC3335_VBAT_TYP 3600 |
| in mV, the nominal battery voltage expected for the majority of the battery discharge. More... | |
| #define | LTC3335_CORRECTION_FACTOR_TYP -487 |
| Value of LTC3335_Software_Correction_Table[VBAT_TO_TABLE_INDEX(LTC3335_VBAT_TYP)]. More... | |
Input Read Definitions | |
Macros to read LTC3335 Inputs, defined to interface to the Arduino. | |
| #define | LTC3335_PGOOD_READ() digitalRead(2) |
| #define | LTC3335_NIRQ_READ() digitalRead(5) |
Timing Definitions | |
Macro to get timing data from microprocessor, defined to interface to the Arduino function which uses ATMega328P Timer0. The timer resolution is specified in timer counts per sec. | |
| #define | LTC3335_TIMER_GET() micros() |
| #define | LTC3335_TIMER_COUNTS_PER_SEC 1000000 |
Counter Definitions | |
Macro to get hardware counter data from microprocess, defined to interface to function in ATmega_Counter.h which uses ATMega328P Timer1. The number of bits of the hardware timer is specified in number of bits. | |
| #define | LTC3335_COUNTER_GET() TCNT1 |
| #define | LTC3335_COUNTER_SIZE 16 |
Hardware Initialization | |
Macro to init micro hardware that is used by LTC3335 driver. | |
| #define | LTC3335_MICRO_INIT() |
| #define LTC3335_ALARM_CAPACITY 0.9*LTC3335_CAPACITY |
in mAh, the capacity at which the alarm should be activated.
Definition at line 98 of file LTC3335_Config.h.
| #define LTC3335_CAPACITY (2400) |
in mAh, capacity of the battery
Definition at line 97 of file LTC3335_Config.h.
| #define LTC3335_CORRECTION_FACTOR_TYP -487 |
Value of LTC3335_Software_Correction_Table[VBAT_TO_TABLE_INDEX(LTC3335_VBAT_TYP)].
Arduino compiler is not smart enough to lookup the value in the const table when optimizing and makes a lot of runtime code if you don't #define the value manually.
Definition at line 104 of file LTC3335_Config.h.
| #define LTC3335_COUNTER_GET | ( | ) | TCNT1 |
Definition at line 132 of file LTC3335_Config.h.
| #define LTC3335_COUNTER_SIZE 16 |
Definition at line 133 of file LTC3335_Config.h.
| #define LTC3335_IPEAK_CONFIGURATION LTC3335_IPEAK_CONFIGURATION_100MA |
IPEAK setting from LTC3335_IPEAK_CONFIGURATION_TYPE in LTC3335.h.
Definition at line 95 of file LTC3335_Config.h.
| #define LTC3335_MICRO_INIT | ( | ) |
Definition at line 139 of file LTC3335_Config.h.
| #define LTC3335_NIRQ_READ | ( | ) | digitalRead(5) |
Definition at line 117 of file LTC3335_Config.h.
| #define LTC3335_OUTPUT_VOLTAGE LTC3335_OUTPUT_VOLTAGE_3_3V |
VOUT setting from LTC3335_NUM_OUTPUT_VOLTAGES in LTC3335.h.
Definition at line 96 of file LTC3335_Config.h.
| #define LTC3335_PGOOD_READ | ( | ) | digitalRead(2) |
Definition at line 116 of file LTC3335_Config.h.
| #define LTC3335_TIMER_COUNTS_PER_SEC 1000000 |
Definition at line 125 of file LTC3335_Config.h.
| #define LTC3335_TIMER_GET | ( | ) | micros() |
Definition at line 124 of file LTC3335_Config.h.
| #define LTC3335_USE_CURRENT_MEASUREMENT true |
Set to true to use the /IRQ pin to measure the battery current real time.
Definition at line 100 of file LTC3335_Config.h.
| #define LTC3335_USE_SOFTWARE_CORRECTION false |
Set to true to use software correction of coulomb count and current measurement.
Definition at line 102 of file LTC3335_Config.h.
| #define LTC3335_VBAT_TYP 3600 |
in mV, the nominal battery voltage expected for the majority of the battery discharge.
Definition at line 103 of file LTC3335_Config.h.