![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2990: 14-bit ADC Quad I2C voltage, current, and temperature monitor. More...
LTC2990: 14-bit ADC Quad I2C voltage, current, and temperature monitor.
The LTC2990 is used to monitor system temperatures, voltages and currents.
Through the I2C serial interface, the four monitors can individually measure
supply voltages and can be paired for differential measurements of current sense
resistors or temperature sensing transistors. Additional measurements include
internal temperature and internal VCC. The internal 10ppm reference minimizes
the number of supporting components and area required. Selectable address and
configurable functionality give the LTC2990 flexibility to be incorporated in
various systems needing temperature, voltage or current data. The LTC2990 fits
well in systems needing sub-millivolt voltage resolution, 1% current measurement
and 1 degree Celsius temperature accuracy or any combination of the three.
I2C DATA FORMAT (MSB FIRST);
Data Out:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK X X X X C3 C2 C1 C0 SACK D7 D6 D5 D4 D3 D2 D1 D0 SACK STOP
Data In:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK X X X X C3 C2 C1 C0 SACK REPEAT START SA6 SA5 SA4 SA3 SA2 SA1 SA0 R SACK
Byte #4 Byte #5
MSB LSB
D15 D14 D13 D12 D11 D10 D9 D8 MACK D7 D6 D5 D4 D3 D2 D1 D0 MNACK STOP
START : I2C Start
REPEAT Start : I2C Repeat Start
STOP : I2C Stop
SACK : I2C Slave Generated Acknowledge (Active Low)
MACK : I2C Master Generated Acknowledge (Active Low)
MNACK : I2C Master Generated Not Acknowledge
SAx : I2C Address
W : I2C Write (0)
R : I2C Read (1)
Cx : Command Code
Dx : Data Bits
X : Don't care
Example Code:
Read single-ended voltage from V1.
// Enable Single-Ended Mode
ack |= LTC2990_register_set_clear_bits(LTC2990_I2C_ADDRESS, LTC2990_CONTROL_REG, LTC2990_V1_V2_V3_V4, LTC2990_VOLTAGE_MODE_MASK);
// Triggers a conversion by writing any value to the trigger register
ack |= LTC2990_register_write(LTC2990_I2C_ADDRESS, LTC2990_TRIGGER_REG, 0x00);
// Flush one ADC reading in case it is stale. Then, take a new fresh reading.
ack |= LTC2990_adc_read_new_data(LTC2990_I2C_ADDRESS, LTC2990_V1_MSB_REG, &code, &data_valid, LTC2990_TIMEOUT);
voltage = LTC2990_code_to_single_ended_voltage(code, LTC2990_SINGLE_ENDED_lsb);
Read current from V3-V4.
resistor = 1; // R_sense across V3-V4 in ohms
// Enables differential mode.
ack |= LTC2990_register_set_clear_bits(LTC2990_I2C_ADDRESS, LTC2990_CONTROL_REG, LTC2990_V1V2_V3V4, LTC2990_VOLTAGE_MODE_MASK);
// Triggers a conversion by writing any value to the trigger register
ack |= LTC2990_register_write(LTC2990_I2C_ADDRESS, LTC2990_TRIGGER_REG, 0x00);
// Flush one ADC reading in case it is stale. Then, take a new fresh reading.
ack |= LTC2990_adc_read_new_data(LTC2990_I2C_ADDRESS, LTC2990_V2_MSB_REG, &code, &data_valid, LTC2990_TIMEOUT);
voltage = LTC2990_code_to_differential_voltage(code, LTC2990_DIFFERENTIAL_lsb);
current = voltage / resistor; // Calculates current
Read temperature from diode connected to V1-V2.
// Enables temperature mode
ack |= LTC2990_register_set_clear_bits(LTC2990_I2C_ADDRESS, LTC2990_CONTROL_REG, LTC2990_TR1_TR2, LTC2990_VOLTAGE_MODE_MASK);
// Triggers a conversion by writing any value to the trigger register
ack |= LTC2990_register_write(LTC2990_I2C_ADDRESS, LTC2990_TRIGGER_REG, 0x00);
// Flush one ADC reading in case it is stale. Then, take a new fresh reading.
ack |= LTC2990_adc_read_new_data(LTC2990_I2C_ADDRESS, LTC2990_V1_MSB_REG, &adc_code, &data_valid, LTC2990_TIMEOUT);
// Check which temperature mode the LTC2990 in currently in
ack |= LTC2990_register_read(LTC2990_I2C_ADDRESS, LTC2990_CONTROL_REG, ®_data);
if (reg_data & LTC2990_KELVIN_ENABLE) isKelvin= true;
else isKelvin=false;
temperature = LTC2990_temperature(adc_code, LTC2990_TEMPERATURE_lsb, isKelvin);http://www.linear.com/product/LTC2990
http://www.linear.com/product/LTC2990#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Library Header File for LTC2990: 14-bit Quad I2C Voltage, Current, and Temperature Monitor
Definition in file LTC2990.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2990_adc_read (uint8_t i2c_address, uint8_t msb_register_address, int16_t *adc_code, int8_t *data_valid) |
| Reads a 14-bit adc_code from LTC2990. More... | |
| int8_t | LTC2990_adc_read_timeout (uint8_t i2c_address, uint8_t msb_register_address, int16_t *adc_code, int8_t *data_valid, uint16_t timeout, uint8_t status_bit) |
| Reads a 14-bit adc_code from the LTC2990 but enforces a maximum timeout. More... | |
| int8_t | LTC2990_adc_read_new_data (uint8_t i2c_address, uint8_t msb_register_address, int16_t *adc_code, int8_t *data_valid, uint16_t timeout) |
| Reads new data (even after a mode change) by flushing old data and waiting for the data_valid bit to be set. More... | |
| int8_t | LTC2990_register_read (uint8_t i2c_address, uint8_t register_address, uint8_t *register_data) |
| Reads an 8-bit register from the LTC2990 using the standard repeated start format. More... | |
| int8_t | LTC2990_register_write (uint8_t i2c_address, uint8_t register_address, uint8_t register_data) |
| Write one byte to an LTC2990 register. More... | |
| int8_t | LTC2990_register_set_clear_bits (uint8_t i2c_address, uint8_t register_address, uint8_t bits_to_set, uint8_t bits_to_clear) |
| Used to set and clear bits in a control register. More... | |
| float | LTC2990_code_to_single_ended_voltage (int16_t adc_code, float LTC2990_single_ended_lsb) |
| Calculates the LTC2990 single-ended input voltages. More... | |
| float | LTC2990_code_to_vcc_voltage (int16_t adc_code, float LTC2990_single_ended_lsb) |
| Calculates the LTC2990 Vcc voltage. More... | |
| float | LTC2990_code_to_differential_voltage (int16_t adc_code, float LTC2990_differential_lsb) |
| Calculates the LTC2990 differential input voltage. More... | |
| float | LTC2990_temperature (int16_t adc_code, float LTC2990_temperature_lsb, boolean unit) |
| Calculates the LTC2990 temperature. More... | |
| float | LTC2990_code_to_diode_voltage (int16_t adc_code, float LTC2990_diode_voltage_lsb) |
| Calculates the LTC2990 diode voltage. More... | |
Macros | |
I2C_Addresses | |
| #define | LTC2990_I2C_ADDRESS 0x4C |
| I2C address of the LTC2990. More... | |
| #define | LTC2990_I2C_GLOBAL_ADDRESS 0x77 |
| LTC2990 Global I2C Address. More... | |
REGISTERS | |
| #define | LTC2990_STATUS_REG 0x00 |
| Indicates BUSY state and conversion status. More... | |
| #define | LTC2990_CONTROL_REG 0x01 |
| Controls Mode, Single/Repeat, Celsius/Kelvin. More... | |
| #define | LTC2990_TRIGGER_REG 0x02 |
| Triggers a conversion. More... | |
| #define | LTC2990_TINT_MSB_REG 0x04 |
| Internal Temperature MSB. More... | |
| #define | LTC2990_TINT_LSB_REG 0x05 |
| Internal Temperature LSB. More... | |
| #define | LTC2990_V1_MSB_REG 0x06 |
| V1, V1-V2, or T_R1 T MSB. More... | |
| #define | LTC2990_V1_LSB_REG 0x07 |
| V1, V1-V2, or T_R1 T LSB. More... | |
| #define | LTC2990_V2_MSB_REG 0x08 |
| V2, V1-V2, or T_R2 Voltage MSB. More... | |
| #define | LTC2990_V2_LSB_REG 0x09 |
| V2, V1-V2, or T_R2 Voltage LSB. More... | |
| #define | LTC2990_V3_MSB_REG 0x0A |
| V3, V3-V4, or T_R2 T MSB. More... | |
| #define | LTC2990_V3_LSB_REG 0x0B |
| V3, V3-V4, or T_R2 T LSB. More... | |
| #define | LTC2990_V4_MSB_REG 0x0C |
| V4, V3-V4, or T_R2 Voltage MSB. More... | |
| #define | LTC2990_V4_LSB_REG 0x0D |
| V4, V3-V4, or T_R2 Voltage LSB. More... | |
| #define | LTC2990_VCC_MSB_REG 0x0E |
| Vcc MSB. More... | |
| #define | LTC2990_VCC_LSB_REG 0x0F |
| Vcc LSB. More... | |
LTC2990_CONTROL_REG SETTINGS | |
Bitwise OR settings, and write to LTC2990_CONTROL_REG to configure settings. Bitwise AND with value read from LTC2990_CONTROL_REG to determine present setting. | |
| #define | LTC2990_KELVIN_ENABLE 0x80 |
| Enable for Kelvin. More... | |
| #define | LTC2990_CELSIUS_ENABLE 0x00 |
| Enable for Celsius. More... | |
| #define | LTC2990_TEMP_FORMAT_MASK 0x80 |
| Use mask when changing temp formats. More... | |
| #define | LTC2990_SINGLE_ENABLE 0x40 |
| Enable for Single Acquisition. More... | |
| #define | LTC2990_REPEATED_ENABLE 0x00 |
| Enable for Repeated Acquisition Mode. More... | |
| #define | LTC2990_ACQUISITION_MASK 0x40 |
| Use mask when changing acquisition settings. More... | |
LTC2990_CONTROL_REG ENABLE | |
Bitwise AND 0xE7 then Bitwise OR settings, and write to LTC2990_CONTROL_REG to configure enable settings. Bitwise AND with value read from LTC2990_CONTROL_REG to determine present enable setting. | |
| #define | LTC2990_ENABLE_INT_TEMPERATURE 0x00 |
| Read only Internal Temperature. More... | |
| #define | LTC2990_ENABLE_V1 0x08 |
| Tr1, V1 or V1-V2 per Mode are enabled. More... | |
| #define | LTC2990_ENABLE_V2 0x10 |
| Tr2, V3 or V3-V4 per Mode are enabled. More... | |
| #define | LTC2990_ENABLE_ALL 0x18 |
| All measurements per Mode are enabled. More... | |
| #define | LTC2990_TEMP_MEAS_MODE_MASK 0x18 |
| Use mask when changing temp meas modes. More... | |
LTC2990_CONTROL_REG MODE | |
Bitwise AND 0xF8 then Bitwise OR settings, and write to LTC2990_CONTROL_REG to configure enable settings. Bitwise AND with value read from LTC2990_CONTROL_REG to determine present enable setting. | |
| #define | LTC2990_V1_V2_TR2 0x00 |
| Read V1, V2 and TR2. More... | |
| #define | LTC2990_V1V2_TR2 0x01 |
| Read V1-V2 and TR2. More... | |
| #define | LTC2990_V1V2_V3_V4 0x02 |
| Read V1-V2, V3 and V4. More... | |
| #define | LTC2990_TR1_V3_V4 0x03 |
| Read TR1, V3 and V4. More... | |
| #define | LTC2990_TR1_V3V4 0x04 |
| Read TR1 and V3-V4. More... | |
| #define | LTC2990_TR1_TR2 0x05 |
| Read TR1 and TR2. More... | |
| #define | LTC2990_V1V2_V3V4 0x06 |
| Read V1-V2 and V3-V4. More... | |
| #define | LTC2990_V1_V2_V3_V4 0x07 |
| Read V1, V2, V3 and V4. More... | |
| #define | LTC2990_VOLTAGE_MODE_MASK 0x07 |
| Use mode mask when changing modes. More... | |
| int8_t LTC2990_adc_read | ( | uint8_t | i2c_address, |
| uint8_t | msb_register_address, | ||
| int16_t * | adc_code, | ||
| int8_t * | data_valid | ||
| ) |
Reads a 14-bit adc_code from LTC2990.
| i2c_address | I2C address of the LTC2990. Configured by tying the ADR0, ADR1, and ADR2 pins high or low. See Table 1 of datasheet. |
| msb_register_address | Address of the LTC2990 MSB register to be read. This is also known as the "command byte". Two sequential 8-bit registers are read, starting with the msb_register_address. |
| adc_code | returns 14-bit value read from the ADC |
| data_valid | returns the status of the DATA_VALID bit. *data_valid=0 indicates stale data |
Definition at line 76 of file LTC2990.cpp.
| int8_t LTC2990_adc_read_new_data | ( | uint8_t | i2c_address, |
| uint8_t | msb_register_address, | ||
| int16_t * | adc_code, | ||
| int8_t * | data_valid, | ||
| uint16_t | timeout | ||
| ) |
Reads new data (even after a mode change) by flushing old data and waiting for the data_valid bit to be set.
This function simplifies ADC reads when modes are changing. For example, if V1-V2 changes from temperature mode to differential voltage mode, the data in the register may still correspond to the temperature reading immediately after the mode change. Flushing one reading and waiting for a new reading guarantees fresh data is received. If the timeout is reached without valid data (*data_valid=1) the function exits.
| i2c_address | I2C address of the LTC2990. Configured by tying the ADR0, ADR1, and ADR2 pins high or low. See Table 1 of datasheet. |
| msb_register_address | Address of the LTC2990 MSB register to be read. This is also known as the "command byte". Two sequential 8-bit registers will be read, starting with the msb_register_address. |
| adc_code | returns 14-bit value read from the ADC |
| data_valid | returns the status of the DATA_VALID bit. *data_valid=0 indicates stale data |
| timeout | maximum timeout in milliseconds. If at any time a NACK is received the function aborts. If the timeout is reached without valid data (*data_valid=1) the function exits. |
Definition at line 124 of file LTC2990.cpp.
| int8_t LTC2990_adc_read_timeout | ( | uint8_t | i2c_address, |
| uint8_t | msb_register_address, | ||
| int16_t * | adc_code, | ||
| int8_t * | data_valid, | ||
| uint16_t | timeout, | ||
| uint8_t | status_bit | ||
| ) |
Reads a 14-bit adc_code from the LTC2990 but enforces a maximum timeout.
Similar to LTC2990_adc_read except it repeats until the data_valid bit is set, it fails to receive an I2C acknowledge, or the timeout (in milliseconds) expires. It keeps trying to read from the LTC2990 every millisecond until the data_valid bit is set (indicating new data since the previous time this register was read) or until it fails to receive an I2C acknowledge (indicating an error on the I2C bus).
| i2c_address | I2C address of the LTC2990. Configured by tying the ADR0, ADR1, and ADR2 pins high or low. See Table 1 of datasheet. |
| msb_register_address | Address of the LTC2990 MSB register to be read. This is also known as the "command byte". Two sequential 8-bit registers will be read, starting with the msb_register_address. |
| adc_code | returns 14-bit value read from the ADC |
| data_valid | returns the status of the DATA_VALID bit. *data_valid=0 indicates stale data |
| timeout | maximum timeout in milliseconds. If at any time a NACK is received the function aborts. |
Definition at line 93 of file LTC2990.cpp.
| float LTC2990_code_to_differential_voltage | ( | int16_t | adc_code, |
| float | LTC2990_differential_lsb | ||
| ) |
Calculates the LTC2990 differential input voltage.
| adc_code | code read from the ADC (from a function such as LTC2990_adc_read) |
| LTC2990_differential_lsb | differential LSB weight. If not calibrated, use LTC2990_DIFFERENTIAL_LSB |
Definition at line 200 of file LTC2990.cpp.
| float LTC2990_code_to_diode_voltage | ( | int16_t | adc_code, |
| float | LTC2990_diode_voltage_lsb | ||
| ) |
Calculates the LTC2990 diode voltage.
| adc_code | code read from the ADC (from a function such as LTC2990_adc_read) |
| LTC2990_diode_voltage_lsb | diode voltage LSB weight. If not calibrated, use LTC2990_DIODE_VOLTAGE_LSB |
Definition at line 231 of file LTC2990.cpp.
| float LTC2990_code_to_single_ended_voltage | ( | int16_t | adc_code, |
| float | LTC2990_single_ended_lsb | ||
| ) |
Calculates the LTC2990 single-ended input voltages.
| adc_code | code read from the ADC (from a function such as LTC2990_adc_read) |
| LTC2990_single_ended_lsb | single-ended LSB weight. If not calibrated, use LTC2990_SINGLE_ENDED_LSB |
Definition at line 170 of file LTC2990.cpp.
| float LTC2990_code_to_vcc_voltage | ( | int16_t | adc_code, |
| float | LTC2990_single_ended_lsb | ||
| ) |
Calculates the LTC2990 Vcc voltage.
| adc_code | code read from the ADC (from a function such as LTC2990_adc_read) |
| LTC2990_single_ended_lsb | Vcc LSB weight. If not calibrated, use LTC2990_VCC_LSB |
Definition at line 185 of file LTC2990.cpp.
| int8_t LTC2990_register_read | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t * | register_data | ||
| ) |
Reads an 8-bit register from the LTC2990 using the standard repeated start format.
| i2c_address | I2C address of the LTC2990. Configured by tying the ADR0, ADR1, and ADR2 pins high or low. See Table 1 of datasheet. |
| register_address | Address of the LTC2990 register to be read. This is also known as the "command byte". |
| register_data | returns 8-bit value read from the LTC2990 register. |
Definition at line 137 of file LTC2990.cpp.
| int8_t LTC2990_register_set_clear_bits | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bits_to_set, | ||
| uint8_t | bits_to_clear | ||
| ) |
Used to set and clear bits in a control register.
bits_to_set will be bitwise OR'd with the register. bits_to_clear will be inverted and bitwise AND'd with the register so that every location with a 1 will result in a 0 in the register.
| i2c_address | I2C address of the LTC2990. Configured by tying the ADR0, ADR1, and ADR2 pins high or low. See Table 1 of datasheet. |
| register_address | Address of the LTC2990 register to be modified. |
| bits_to_set | bits_to_set will be bitwise OR'd with the register. |
| bits_to_clear | bits_to_clear will be inverted and bitwise AND'd with the register |
Definition at line 157 of file LTC2990.cpp.
| int8_t LTC2990_register_write | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | register_data | ||
| ) |
Write one byte to an LTC2990 register.
Writes to an 8-bit register inside the LTC2990 using the standard I2C repeated start format.
| i2c_address | I2C address of the LTC2990. Configured by tying the ADR0, ADR1, and ADR2 pins high or low. See Table 1 of datasheet. |
| register_address | Address of the LTC2990 register to be overwritten. This is also known as the "command byte". |
| register_data | Value that will be written to the register. |
Definition at line 147 of file LTC2990.cpp.
| float LTC2990_temperature | ( | int16_t | adc_code, |
| float | LTC2990_temperature_lsb, | ||
| boolean | unit | ||
| ) |
Calculates the LTC2990 temperature.
| adc_code | code read from the ADC (from a function such as LTC2990_adc_read). |
| LTC2990_temperature_lsb | temperature LSB weight. If not calibrated, use LTC2990_TEMPERATURE_LSB |
| unit | The temperature unit, true for Kelvin, false for Celsius |
Definition at line 214 of file LTC2990.cpp.
| #define LTC2990_ACQUISITION_MASK 0x40 |
| #define LTC2990_CONTROL_REG 0x01 |
| #define LTC2990_ENABLE_ALL 0x18 |
| #define LTC2990_ENABLE_INT_TEMPERATURE 0x00 |
| #define LTC2990_ENABLE_V1 0x08 |
| #define LTC2990_ENABLE_V2 0x10 |
| #define LTC2990_I2C_ADDRESS 0x4C |
| #define LTC2990_I2C_GLOBAL_ADDRESS 0x77 |
| #define LTC2990_REPEATED_ENABLE 0x00 |
| #define LTC2990_SINGLE_ENABLE 0x40 |
| #define LTC2990_STATUS_REG 0x00 |
| #define LTC2990_TEMP_FORMAT_MASK 0x80 |
| #define LTC2990_TEMP_MEAS_MODE_MASK 0x18 |
| #define LTC2990_TINT_LSB_REG 0x05 |
| #define LTC2990_TINT_MSB_REG 0x04 |
| #define LTC2990_V2_LSB_REG 0x09 |
| #define LTC2990_V2_MSB_REG 0x08 |
| #define LTC2990_V4_LSB_REG 0x0D |
| #define LTC2990_V4_MSB_REG 0x0C |