![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2946: 12-Bit Wide Range Power, Charge and Energy Monitor. More...
LTC2946: 12-Bit Wide Range Power, Charge and Energy Monitor.
The LTC®2946 is a rail-to-rail system monitor that measures
current, voltage, power, charge and energy. It features an
operating range of 2.7V to 100V and includes a shunt regulator
for supplies above 100V. The current measurement common mode
range of 0V to 100V is independent of the input supply.
A 12-bit ADC measures load current, input voltage and an
auxiliary external voltage. Load current and internally
calculated power are integrated over an external clock or
crystal or internal oscillator time base for charge and energy.
An accurate time base allows the LTC2946 to provide measurement
accuracy of better than ±0.6% for charge and ±1% for power and
energy. Minimum and maximum values are stored and an overrange
alert with programmable thresholds minimizes the need for software
polling. Data is reported via a standard I2C interface.
Shutdown mode reduces power consumption to 15uA.
I2C DATA FORMAT (MSB FIRST):
Data Out:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK X X C5 C4 C3 C2 C1 C0 SACK D7 D6 D5 D4 D3 D2 D1 D0 SACK STOP
Data In:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK X X C5 C4 C3 C2 C1 C0 SACK Repeat Start SA6 SA5 SA4 SA3 SA2 SA1 SA0 R SACK
Byte #4 Byte #5
MSB LSB
D15 D14 D13 D12 D11 D10 D9 D8 MACK D7 D6 D5 D4 D3 D2 D1 D0 MNACK STOP
START : I2C Start
Repeat Start: I2c Repeat Start
STOP : I2C Stop
SAx : I2C Address
SACK : I2C Slave Generated Acknowledge (Active Low)
MACK : I2C Master Generated Acknowledge (Active Low)
MNACK : I2c Master Generated Not Acknowledge
W : I2C Write (0)
R : I2C Read (1)
Cx : Command Code
Dx : Data Bits
X : Don't care
Example Code:
Read power, current, voltage, charge and energy.
CTRLA = LTC2946_CHANNEL_CONFIG_V_C_3|LTC2946_SENSE_PLUS|LTC2946_OFFSET_CAL_EVERY|LTC2946_ADIN_GND; //! Set Control A register to default value in continuous mode
ack |= LTC2946_write(LTC2946_I2C_ADDRESS, LTC2946_CTRLA_REG, CTRLA); //! Sets the LTC2946 to continuous mode
resistor = .02; // Resistor Value On Demo Board
ack |= LTC2946_read_24_bits(LTC2946_I2C_ADDRESS, LTC2946_POWER_MSB2_REG, &power_code); // Reads the ADC registers that contains V^2
power = LTC2946_code_to_power(power_code, resistor, LTC2946_Power_lsb); // Calculates power from power code, resistor value and power lsb
ack |= LTC2946_read_12_bits(LTC2946_I2C_ADDRESS, LTC2946_DELTA_SENSE_MSB_REG, ¤t_code); // Reads the voltage code across sense resistor
current = LTC2946_code_to_current(current_code, resistor, LTC2946_DELTA_SENSE_lsb); // Calculates current from current code, resistor value and current lsb
ack |= LTC2946_read_12_bits(LTC2946_I2C_ADDRESS, LTC2946_VIN_MSB_REG, &VIN_code); // Reads VIN voltage code
VIN = LTC2946_VIN_code_to_voltage(VIN_code, LTC2946_VIN_lsb); // Calculates VIN voltage from VIN code and lsb
ack |= LTC2946_read_32_bits(LTC2946_I2C_ADDRESS, LTC2946_ENERGY_MSB3_REG, &energy_code); // Reads energy code
energy = LTC2946_code_to_energy(energy_code,resistor,LTC2946_Power_lsb, LTC2946_INTERNAL_TIME_lsb); //Calculates Energy in Joules from energy_code, resistor, power lsb and time lsb
ack |= LTC2946_read_32_bits(LTC2946_I2C_ADDRESS, LTC2946_CHARGE_MSB3_REG, &charge_code); // Reads charge code
charge = LTC2946_code_to_coulombs(charge_code,resistor,LTC2946_DELTA_SENSE_lsb, LTC2946_INTERNAL_TIME_lsb); //Calculates charge in coulombs from charge_code, resistor, current lsb and time lsbhttp://www.linear.com/product/LTC2946
http://www.linear.com/product/ltc2946#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2946: 12-Bit Wide Range Power, Charge and Energy Monitor
Definition in file LTC2946.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2946_write (uint8_t i2c_address, uint8_t adc_command, uint8_t code) |
| Write an 8-bit code to the LTC2946. More... | |
| int8_t | LTC2946_write_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t code) |
| Write a 16-bit code to the LTC2946. More... | |
| int8_t | LTC2946_write_24_bits (uint8_t i2c_address, uint8_t adc_command, uint32_t code) |
| Write a 24-bit code to the LTC2946. More... | |
| int8_t | LTC2946_write_32_bits (uint8_t i2c_address, uint8_t adc_command, uint32_t code) |
| Write a 32-bit code to the LTC2946. More... | |
| int8_t | LTC2946_read (uint8_t i2c_address, uint8_t adc_command, uint8_t *adc_code) |
| Reads an 8-bit adc_code from LTC2946. More... | |
| int8_t | LTC2946_read_12_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 12-bit adc_code from LTC2946. More... | |
| int8_t | LTC2946_read_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 16-bit adc_code from LTC2946. More... | |
| int8_t | LTC2946_read_24_bits (uint8_t i2c_address, uint8_t adc_command, uint32_t *adc_code) |
| Reads a 24-bit adc_code from LTC2946. More... | |
| int8_t | LTC2946_read_32_bits (uint8_t i2c_address, uint8_t adc_command, uint32_t *adc_code) |
| Reads a 32-bit adc_code from LTC2946. More... | |
| float | LTC2946_VIN_code_to_voltage (uint16_t adc_code, float LTC2946_VIN_lsb) |
| Calculate the LTC2946 VIN voltage. More... | |
| float | LTC2946_ADIN_code_to_voltage (uint16_t adc_code, float LTC2946_ADIN_lsb) |
| Calculate the LTC2946 ADIN voltage. More... | |
| float | LTC2946_code_to_current (uint16_t adc_code, float resistor, float LTC2946_DELTA_SENSE_lsb) |
| Calculate the LTC2946 current with a sense resistor. More... | |
| float | LTC2946_code_to_power (int32_t adc_code, float resistor, float LTC2946_Power_lsb) |
| Calculate the LTC2946 power. More... | |
| float | LTC2946_code_to_energy (int32_t adc_code, float resistor, float LTC2946_Power_lsb, float LTC2946_TIME_lsb) |
| Calculate the LTC2946 energy. More... | |
| float | LTC2946_code_to_coulombs (int32_t adc_code, float resistor, float LTC2946_DELTA_SENSE_lsb, float LTC2946_Time_lsb) |
| Calculate the LTC2946 coulombs. More... | |
| float | LTC2946_code_to_time (float time_code, float LTC2946_Time_lsb) |
| Calculate the LTC2946 internal time base. More... | |
Macros | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
LTC2946 I2C Address Assignments | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Use table to select address
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_I2C_ADDRESS 0x6F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_I2C_MASS_WRITE 0xCC | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_I2C_ALERT_RESPONSE 0x19 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Registers | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CTRLA_REG 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CTRLB_REG 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ALERT1_REG 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_STATUS1_REG 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_FAULT1_REG 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_POWER_MSB2_REG 0x05 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_POWER_MSB1_REG 0x06 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_POWER_LSB_REG 0x07 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_POWER_MSB2_REG 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_POWER_MSB1_REG 0x09 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_POWER_LSB_REG 0x0A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_POWER_MSB2_REG 0x0B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_POWER_MSB1_REG 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_POWER_LSB_REG 0x0D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_POWER_THRESHOLD_MSB2_REG 0x0E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_POWER_THRESHOLD_MSB1_REG 0x0F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_POWER_THRESHOLD_LSB_REG 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_POWER_THRESHOLD_MSB2_REG 0x11 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_POWER_THRESHOLD_MSB1_REG 0x12 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_POWER_THRESHOLD_LSB_REG 0x13 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DELTA_SENSE_MSB_REG 0x14 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DELTA_SENSE_LSB_REG 0x15 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_DELTA_SENSE_MSB_REG 0x16 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_DELTA_SENSE_LSB_REG 0x17 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_DELTA_SENSE_MSB_REG 0x18 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_DELTA_SENSE_LSB_REG 0x19 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_DELTA_SENSE_THRESHOLD_MSB_REG 0x1A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_DELTA_SENSE_THRESHOLD_LSB_REG 0x1B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_DELTA_SENSE_THRESHOLD_MSB_REG 0x1C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_DELTA_SENSE_THRESHOLD_LSB_REG 0x1D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_VIN_MSB_REG 0x1E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_VIN_LSB_REG 0x1F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_VIN_MSB_REG 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_VIN_LSB_REG 0x21 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_VIN_MSB_REG 0x22 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_VIN_LSB_REG 0x23 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_VIN_THRESHOLD_MSB_REG 0x24 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_VIN_THRESHOLD_LSB_REG 0x25 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_VIN_THRESHOLD_MSB_REG 0x26 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_VIN_THRESHOLD_LSB_REG 0x27 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ADIN_MSB_REG 0x28 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ADIN_LSB_REG_REG 0x29 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_ADIN_MSB_REG 0x2A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_ADIN_LSB_REG 0x2B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_ADIN_MSB_REG 0x2C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_ADIN_LSB_REG 0x2D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_ADIN_THRESHOLD_MSB_REG 0x2E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_ADIN_THRESHOLD_LSB_REG 0x2F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_ADIN_THRESHOLD_MSB_REG 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_ADIN_THRESHOLD_LSB_REG 0x31 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ALERT2_REG 0x32 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO_CFG_REG 0x33 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_TIME_COUNTER_MSB3_REG 0x34 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_TIME_COUNTER_MSB2_REG 0x35 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_TIME_COUNTER_MSB1_REG 0x36 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_TIME_COUNTER_LSB_REG 0x37 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHARGE_MSB3_REG 0x38 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHARGE_MSB2_REG 0x39 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHARGE_MSB1_REG 0x3A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHARGE_LSB_REG 0x3B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENERGY_MSB3_REG 0x3C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENERGY_MSB2_REG 0x3D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENERGY_MSB1_REG 0x3E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENERGY_LSB_REG 0x3F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_STATUS2_REG 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_FAULT2_REG 0x41 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO3_CTRL_REG 0x42 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CLK_DIV_REG 0x43 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Voltage Selection Command | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DELTA_SENSE 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_VDD 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ADIN 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_SENSE_PLUS 0x18 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Command Codes | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ADIN_INTVCC 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ADIN_GND 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_OFFSET_CAL_LAST 0x60 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_OFFSET_CAL_128 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_OFFSET_CAL_16 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_OFFSET_CAL_EVERY 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHANNEL_CONFIG_SNAPSHOT 0x07 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHANNEL_CONFIG_V_C 0x06 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHANNEL_CONFIG_A_V_C_1 0x05 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHANNEL_CONFIG_A_V_C_2 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHANNEL_CONFIG_A_V_C_3 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHANNEL_CONFIG_V_C_1 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHANNEL_CONFIG_V_C_2 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CHANNEL_CONFIG_V_C_3 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_ALERT_CLEAR 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_SHUTDOWN 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_CLEARED_ON_READ 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_STUCK_BUS_RECOVER 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_ALERT_CLEAR 0x7F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_SHUTDOWN 0xBF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_CLEARED_ON_READ 0xDF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_STUCK_BUS_RECOVER 0xEF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ACC_PIN_CONTROL 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_ACC 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_ACC 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_RESET_ALL 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_RESET_ACC 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_AUTO_RESET 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_AUTO_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_POWER_MSB2_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_POWER_MSB2_RESET 0xFF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_DELTA_SENSE_MSB_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_DELTA_SENSE_MSB_RESET 0xFF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_VIN_MSB_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_VIN_MSB_RESET 0xFF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MAX_ADIN_MSB_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_MIN_ADIN_MSB_RESET 0xFF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_MAX_POWER_ALERT 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_MIN_POWER_ALERT 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_MAX_POWER_ALERT 0x7F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_MIN_POWER_ALERT 0xBF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_MAX_I_SENSE_ALERT 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_MIN_I_SENSE_ALERT 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_MAX_I_SENSE_ALERT 0xDF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_MIN_I_SENSE_ALERT 0xEF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_MAX_VIN_ALERT 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_MIN_VIN_ALERT 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_MAX_VIN_ALERT 0xF7 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_MIN_VIN_ALERT 0xFB | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_MAX_ADIN_ALERT 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_MIN_ADIN_ALERT 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_MAX_ADIN_ALERT 0xFD | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_MIN_ADIN_ALERT 0xFE | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_ADC_DONE_ALERT 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_ADC_DONE_ALERT 0x7F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_GPIO_1_ALERT 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_GPIO_1_ALERT 0xBF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_GPIO_2_ALERT 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_GPIO_2_ALERT 0xDF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_STUCK_BUS_WAKE_ALERT 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_STUCK_BUS_WAKE_ALERT 0xF7 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_ENERGY_OVERFLOW_ALERT 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_ENERGY_OVERFLOW_ALERT 0xFB | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_CHARGE_OVERFLOW_ALERT 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_CHARGE_OVERFLOW_ALERT 0xFD | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_ENABLE_COUNTER_OVERFLOW_ALERT 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_DISABLE_COUNTER_OVERFLOW_ALERT 0xFE | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO1_IN_ACTIVE_HIGH 0xC0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO1_IN_ACTIVE_LOW 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO1_OUT_HIGH_Z 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO1_OUT_LOW 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO2_IN_ACTIVE_HIGH 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO2_IN_ACTIVE_LOW 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO2_OUT_HIGH_Z 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO2_OUT_LOW 0x12 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO2_IN_ACC 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO3_IN_ACTIVE_HIGH 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO3_IN_ACTIVE_LOW 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO3_OUT_REG_42 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO3_OUT_ALERT 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO3_OUT_LOW 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO3_OUT_HIGH_Z 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO_ALERT_CLEAR 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Register Mask Command | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CTRLA_ADIN_MASK 0x7F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CTRLA_OFFSET_MASK 0x9F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CTRLA_VOLTAGE_SEL_MASK 0xE7 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CTRLA_CHANNEL_CONFIG_MASK 0xF8 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CTRLB_ACC_MASK 0xF3 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_CTRLB_RESET_MASK 0xFC | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIOCFG_GPIO1_MASK 0x3F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIOCFG_GPIO2_MASK 0xCF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIOCFG_GPIO3_MASK 0xF3 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIOCFG_GPIO2_OUT_MASK 0xFD | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2946_GPIO3_CTRL_GPIO3_MASK 0xBF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| float LTC2946_ADIN_code_to_voltage | ( | uint16_t | adc_code, |
| float | LTC2946_ADIN_lsb | ||
| ) |
Calculate the LTC2946 ADIN voltage.
| adc_code | The ADC value |
| LTC2946_ADIN_lsb | ADIN lsb weight |
Definition at line 203 of file LTC2946.cpp.
| float LTC2946_code_to_coulombs | ( | int32_t | adc_code, |
| float | resistor, | ||
| float | LTC2946_DELTA_SENSE_lsb, | ||
| float | LTC2946_Time_lsb | ||
| ) |
Calculate the LTC2946 coulombs.
| adc_code | The ADC value |
| resistor | The resistor value |
| LTC2946_DELTA_SENSE_lsb | Delta sense lsb weight |
| LTC2946_Time_lsb | Time lsb weight |
Definition at line 243 of file LTC2946.cpp.
| float LTC2946_code_to_current | ( | uint16_t | adc_code, |
| float | resistor, | ||
| float | LTC2946_DELTA_SENSE_lsb | ||
| ) |
Calculate the LTC2946 current with a sense resistor.
| adc_code | The ADC value |
| resistor | The resistor value |
| LTC2946_DELTA_SENSE_lsb | Delta sense lsb weight |
Definition at line 212 of file LTC2946.cpp.
| float LTC2946_code_to_energy | ( | int32_t | adc_code, |
| float | resistor, | ||
| float | LTC2946_Power_lsb, | ||
| float | LTC2946_TIME_lsb | ||
| ) |
Calculate the LTC2946 energy.
| adc_code | The ADC value |
| resistor | The resistor value |
| LTC2946_Power_lsb | Power lsb weight |
| LTC2946_TIME_lsb | Time lsb weight |
Definition at line 233 of file LTC2946.cpp.
| float LTC2946_code_to_power | ( | int32_t | adc_code, |
| float | resistor, | ||
| float | LTC2946_Power_lsb | ||
| ) |
Calculate the LTC2946 power.
| adc_code | The ADC value |
| resistor | The resistor value |
Definition at line 222 of file LTC2946.cpp.
| float LTC2946_code_to_time | ( | float | time_code, |
| float | LTC2946_Time_lsb | ||
| ) |
Calculate the LTC2946 internal time base.
| time_code | Time adc code |
| LTC2946_Time_lsb | Time lsb weight |
Definition at line 253 of file LTC2946.cpp.
| int8_t LTC2946_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t * | adc_code | ||
| ) |
Reads an 8-bit adc_code from LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| adc_code | Value that will be read from the register. |
Definition at line 130 of file LTC2946.cpp.
| int8_t LTC2946_read_12_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 12-bit adc_code from LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| adc_code | Value that will be read from the register. |
Definition at line 141 of file LTC2946.cpp.
| int8_t LTC2946_read_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 16-bit adc_code from LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| adc_code | Value that will be read from the register. |
Definition at line 155 of file LTC2946.cpp.
| int8_t LTC2946_read_24_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint32_t * | adc_code | ||
| ) |
Reads a 24-bit adc_code from LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| adc_code | Value that will be read from the register. |
Definition at line 166 of file LTC2946.cpp.
| int8_t LTC2946_read_32_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint32_t * | adc_code | ||
| ) |
Reads a 32-bit adc_code from LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| adc_code | Value that will be read from the register. |
Definition at line 180 of file LTC2946.cpp.
| float LTC2946_VIN_code_to_voltage | ( | uint16_t | adc_code, |
| float | LTC2946_VIN_lsb | ||
| ) |
Calculate the LTC2946 VIN voltage.
| adc_code | The ADC value |
| LTC2946_VIN_lsb | VIN lsb weight |
Definition at line 194 of file LTC2946.cpp.
| int8_t LTC2946_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| code | Value that will be written to the register. |
Definition at line 81 of file LTC2946.cpp.
| int8_t LTC2946_write_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t | code | ||
| ) |
Write a 16-bit code to the LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| code | Value that will be written to the register. |
Definition at line 93 of file LTC2946.cpp.
| int8_t LTC2946_write_24_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint32_t | code | ||
| ) |
Write a 24-bit code to the LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| code | Value that will be written to the register. |
Definition at line 103 of file LTC2946.cpp.
| int8_t LTC2946_write_32_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint32_t | code | ||
| ) |
Write a 32-bit code to the LTC2946.
| i2c_address | Register address for the LTC2946 |
| adc_command | The "command byte" for the LTC2946 |
| code | Value that will be written to the register. |
Definition at line 116 of file LTC2946.cpp.