![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2945: 12-Bit Wide Range Power Monitor. More...
LTC2945: 12-Bit Wide Range Power Monitor.
The LTC2945 is a rail-to-rail system monitor that measures current, voltage, and
power. It features an operating range of 2.7V to 80V and includes a shunt
regulator for supplies above 80V to allow flexibility in the selection of input
supply. The current measurement range of 0V to 80V is independent of the input
supply. An onboard 0.75% accurate 12-bit ADC measures load current, input
voltage and an auxiliary external voltage. A 24-bit power value is generated by
digitally multiplying the measured 12-bit load current and input voltage data.
Minimum and maximum values are stored and an overrange alert with programmable
thresholds minimizes the need for software polling. Data is reported via a
standard I2C interface. Shutdown mode reduces power consumption to 20uA.
standard I2C interface. Shutdown mode reduces power consumption to 20uA.
I2C DATA FORMAT (MSB FIRST):
Data Out:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK X X C5 C4 C3 C2 C1 C0 SACK D7 D6 D5 D4 D3 D2 D1 D0 SACK STOP
Data In:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK X X C5 C4 C3 C2 C1 C0 SACK Repeat Start SA6 SA5 SA4 SA3 SA2 SA1 SA0 R SACK
Byte #4 Byte #5
MSB LSB
D15 D14 D13 D12 D11 D10 D9 D8 MACK D7 D6 D5 D4 D3 D2 D1 D0 MNACK STOP
START : I2C Start
Repeat Start: I2c Repeat Start
STOP : I2C Stop
SAx : I2C Address
SACK : I2C Slave Generated Acknowledge (Active Low)
MACK : I2C Master Generated Acknowledge (Active Low)
MNACK : I2c Master Generated Not Acknowledge
W : I2C Write (0)
R : I2C Read (1)
Cx : Command Code
Dx : Data Bits
X : Don't care
Example Code:
Read power, current, and voltage.
adc_command = LTC2945_SENSE_MONITOR | LTC2945_CONTINUOUS_MODE; // Builds commands to set LTC2945 to continuous mode
ack |= LTC2945_write(LTC2945_I2C_ADDRESS, LTC2945_CONTROL_REG, adc_command); // Sets the LTC2945 to continuous mode
resistor = .02; // Resistor Value On Demo Board
ack |= LTC2945_read_24_bits(LTC2945_I2C_ADDRESS, LTC2945_POWER_MSB2_REG, &power_code); // Reads the ADC registers that contains V^2
power = LTC2945_code_to_power(power_code, resistor, LTC2945_Power_lsb); // Calculates power from power code, resistor value and power lsb
ack |= LTC2945_read_12_bits(LTC2945_I2C_ADDRESS, LTC2945_DELTA_SENSE_MSB_REG, ¤t_code); // Reads the voltage code across sense resistor
current = LTC2945_code_to_current(current_code, resistor, LTC2945_DELTA_SENSE_lsb); // Calculates current from current code, resistor value and current lsb
ack |= LTC2945_read_12_bits(LTC2945_I2C_ADDRESS, LTC2945_VIN_MSB_REG, &VIN_code); // Reads VIN voltage code
VIN = LTC2945_VIN_code_to_voltage(VIN_code, LTC2945_VIN_lsb); // Calculates VIN voltage from VIN code and lsbhttp://www.linear.com/product/LTC2945
http://www.linear.com/product/ltc2945#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2945: 12-bit Wide Range Power Monitor
Definition in file LTC2945.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2945_write (uint8_t i2c_address, uint8_t adc_command, uint8_t code) |
| Write an 8-bit code to the LTC2945. More... | |
| int8_t | LTC2945_write_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t code) |
| Write a 16-bit code to the LTC2945. More... | |
| int8_t | LTC2945_write_24_bits (uint8_t i2c_address, uint8_t adc_command, int32_t code) |
| Write a 24-bit code to the LTC2945. More... | |
| int8_t | LTC2945_read (uint8_t i2c_address, uint8_t adc_command, uint8_t *adc_code) |
| Reads an 8-bit adc_code from LTC2945. More... | |
| int8_t | LTC2945_read_12_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 12-bit adc_code from LTC2945. More... | |
| int8_t | LTC2945_read_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 16-bit adc_code from LTC2945. More... | |
| int8_t | LTC2945_read_24_bits (uint8_t i2c_address, uint8_t adc_command, int32_t *adc_code) |
| Reads a 24-bit adc_code from LTC2945. More... | |
| float | LTC2945_VIN_code_to_voltage (uint16_t adc_code, float LTC2945_VIN_lsb) |
| Calculate the LTC2945 VIN voltage. More... | |
| float | LTC2945_ADIN_code_to_voltage (uint16_t adc_code, float LTC2945_ADIN_lsb) |
| Calculate the LTC2945 ADIN voltage. More... | |
| float | LTC2945_code_to_current (uint16_t adc_code, float resistor, float LTC2945_DELTA_SENSE_lsb) |
| Calculate the LTC2945 current with a sense resistor. More... | |
| float | LTC2945_code_to_power (int32_t adc_code, float resistor, float LTC2945_Power_lsb) |
| Calculate the LTC2945 power. More... | |
| float | LTC2945_code_to_ADIN_power (int32_t adc_code, float resistor, float LTC2945_ADIN_DELTA_SENSE_lsb) |
| Calculate the LTC2945 power with the ADIN. More... | |
Macros | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
LTC2945 I2C Address Assignments | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Use table to select address
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_I2C_ADDRESS 0x6F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_I2C_MASS_WRITE 0xCC | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_I2C_ALERT_RESPONSE 0x19 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Registers | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_CONTROL_REG 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ALERT_REG 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_STATUS_REG 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_FAULT_REG 0x03 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_FAULT_CoR_REG 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_POWER_MSB2_REG 0x05 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_POWER_MSB1_REG 0x06 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_POWER_LSB_REG 0x07 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_POWER_MSB2_REG 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_POWER_MSB1_REG 0x09 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_POWER_LSB_REG 0x0A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_POWER_MSB2_REG 0x0B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_POWER_MSB1_REG 0x0C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_POWER_LSB_REG 0x0D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_POWER_THRESHOLD_MSB2_REG 0x0E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_POWER_THRESHOLD_MSB1_REG 0x0F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_POWER_THRESHOLD_LSB_REG 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_POWER_THRESHOLD_MSB2_REG 0x11 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_POWER_THRESHOLD_MSB1_REG 0x12 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_POWER_THRESHOLD_LSB_REG 0x13 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DELTA_SENSE_MSB_REG 0x14 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DELTA_SENSE_LSB_REG 0x15 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_DELTA_SENSE_MSB_REG 0x16 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_DELTA_SENSE_LSB_REG 0x17 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_DELTA_SENSE_MSB_REG 0x18 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_DELTA_SENSE_LSB_REG 0x19 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_DELTA_SENSE_THRESHOLD_MSB_REG 0x1A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_DELTA_SENSE_THRESHOLD_LSB_REG 0x1B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_DELTA_SENSE_THRESHOLD_MSB_REG 0x1C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_DELTA_SENSE_THRESHOLD_LSB_REG 0x1D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_VIN_MSB_REG 0x1E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_VIN_LSB_REG 0x1F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_VIN_MSB_REG 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_VIN_LSB_REG 0x21 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_VIN_MSB_REG 0x22 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_VIN_LSB_REG 0x23 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_VIN_THRESHOLD_MSB_REG 0x24 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_VIN_THRESHOLD_LSB_REG 0x25 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_VIN_THRESHOLD_MSB_REG 0x26 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_VIN_THRESHOLD_LSB_REG 0x27 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ADIN_MSB_REG 0x28 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ADIN_LSB_REG_REG 0x29 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_ADIN_MSB_REG 0x2A | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_ADIN_LSB_REG 0x2B | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_ADIN_MSB_REG 0x2C | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_ADIN_LSB_REG 0x2D | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_ADIN_THRESHOLD_MSB_REG 0x2E | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_ADIN_THRESHOLD_LSB_REG 0x2F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_ADIN_THRESHOLD_MSB_REG 0x30 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_ADIN_THRESHOLD_LSB_REG 0x31 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Selection Command | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DELTA_SENSE_SNAPSHOT 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_VIN_SNAPSHOT 0xA0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ADIN_SNAPSHOT 0xC0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Command Codes | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_CONTINUOUS_MODE 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_SHUTDOWN_MODE 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_TEST_MODE 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_RESET_ALL_FAULTS 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_SENSE_MULTIPLIER 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_SENSE_MONITOR 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_POWER_MSB2_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_POWER_MSB2_RESET 0xFF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_DELTA_SENSE_MSB_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_DELTA_SENSE_MSB_RESET 0xFF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_VIN_MSB_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_VIN_MSB_RESET 0xFF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MAX_ADIN_MSB_RESET 0x00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_MIN_ADIN_MSB_RESET 0xFF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ENABLE_MAX_POWER_ALERT 0x80 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ENABLE_MIN_POWER_ALERT 0x40 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DISABLE_MAX_POWER_ALERT 0x7F | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DISABLE_MIN_POWER_ALERT 0xBF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ENABLE_MAX_DELTA_SENSE_ALERT 0x20 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ENABLE_MIN_DELTA_SENSE_ALERT 0x10 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DISABLE_MAX_DELTA_SENSE_ALERT 0xDF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DISABLE_MIN_DELTA_SENSE_ALERT 0xEF | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ENABLE_MAX_VIN_ALERT 0x08 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ENABLE_MIN_VIN_ALERT 0x04 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DISABLE_MAX_VIN_ALERT 0xF7 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DISABLE_MIN_VIN_ALERT 0xFB | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ENABLE_MAX_ADIN_ALERT 0x02 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_ENABLE_MIN_ADIN_ALERT 0x01 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DISABLE_MAX_ADIN_ALERT 0xFD | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| #define | LTC2945_DISABLE_MIN_ADIN_ALERT 0xFE | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| float LTC2945_ADIN_code_to_voltage | ( | uint16_t | adc_code, |
| float | LTC2945_ADIN_lsb | ||
| ) |
Calculate the LTC2945 ADIN voltage.
| adc_code | The ADC value |
| LTC2945_ADIN_lsb | ADIN lsb weight |
Definition at line 171 of file LTC2945.cpp.
| float LTC2945_code_to_ADIN_power | ( | int32_t | adc_code, |
| float | resistor, | ||
| float | LTC2945_ADIN_DELTA_SENSE_lsb | ||
| ) |
Calculate the LTC2945 power with the ADIN.
| adc_code | The ADC value |
| resistor | The resistor value |
| LTC2945_ADIN_DELTA_SENSE_lsb | Power lsb weight |
Definition at line 200 of file LTC2945.cpp.
| float LTC2945_code_to_current | ( | uint16_t | adc_code, |
| float | resistor, | ||
| float | LTC2945_DELTA_SENSE_lsb | ||
| ) |
Calculate the LTC2945 current with a sense resistor.
| adc_code | The ADC value |
| resistor | The resistor value |
| LTC2945_DELTA_SENSE_lsb | Delta sense lsb weight |
Definition at line 180 of file LTC2945.cpp.
| float LTC2945_code_to_power | ( | int32_t | adc_code, |
| float | resistor, | ||
| float | LTC2945_Power_lsb | ||
| ) |
Calculate the LTC2945 power.
| adc_code | The ADC value |
| resistor | The resistor value |
| LTC2945_Power_lsb | Power lsb weight |
Definition at line 190 of file LTC2945.cpp.
| int8_t LTC2945_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t * | adc_code | ||
| ) |
Reads an 8-bit adc_code from LTC2945.
| i2c_address | Register address for the LTC2945 |
| adc_command | The "command byte" for the LTC2945 |
| adc_code | Value that will be read from the register. |
Definition at line 112 of file LTC2945.cpp.
| int8_t LTC2945_read_12_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 12-bit adc_code from LTC2945.
| i2c_address | Register address for the LTC2945 |
| adc_command | The "command byte" for the LTC2945 |
| adc_code | Value that will be read from the register. |
Definition at line 123 of file LTC2945.cpp.
| int8_t LTC2945_read_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 16-bit adc_code from LTC2945.
| i2c_address | Register address for the LTC2945 |
| adc_command | The "command byte" for the LTC2945 |
| adc_code | Value that will be read from the register. |
Definition at line 137 of file LTC2945.cpp.
| int8_t LTC2945_read_24_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| int32_t * | adc_code | ||
| ) |
Reads a 24-bit adc_code from LTC2945.
| i2c_address | Register address for the LTC2945 |
| adc_command | The "command byte" for the LTC2945 |
| adc_code | Value that will be read from the register. |
Definition at line 148 of file LTC2945.cpp.
| float LTC2945_VIN_code_to_voltage | ( | uint16_t | adc_code, |
| float | LTC2945_VIN_lsb | ||
| ) |
Calculate the LTC2945 VIN voltage.
| adc_code | The ADC value |
| LTC2945_VIN_lsb | VIN lsb weight |
Definition at line 162 of file LTC2945.cpp.
| int8_t LTC2945_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC2945.
| i2c_address | Register address for the LTC2945 |
| adc_command | The "command byte" for the LTC2945 |
| code | Value that will be written to the register. |
Definition at line 76 of file LTC2945.cpp.
| int8_t LTC2945_write_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t | code | ||
| ) |
Write a 16-bit code to the LTC2945.
| i2c_address | Register address for the LTC2945 |
| adc_command | The "command byte" for the LTC2945 |
| code | Value that will be written to the register. |
Definition at line 88 of file LTC2945.cpp.
| int8_t LTC2945_write_24_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| int32_t | code | ||
| ) |
Write a 24-bit code to the LTC2945.
| i2c_address | Register address for the LTC2945 |
| adc_command | The "command byte" for the LTC2945 |
| code | Value that will be written to the register. |
Definition at line 98 of file LTC2945.cpp.