![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC2944 Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement. More...
Library for LTC2944 Multicell Battery Gas Gauge with Temperature, Voltage and Current Measurement.
Definition in file LTC2944.cpp.
Go to the source code of this file.
Functions | |
| int8_t | LTC2944_write (uint8_t i2c_address, uint8_t adc_command, uint8_t code) |
| Write an 8-bit code to the LTC2944. More... | |
| int8_t | LTC2944_write_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t code) |
| Write a 16-bit code to the LTC2944. More... | |
| int8_t | LTC2944_read (uint8_t i2c_address, uint8_t adc_command, uint8_t *adc_code) |
| Reads an 8-bit adc_code from LTC2944. More... | |
| int8_t | LTC2944_read_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 16-bit adc_code from LTC2944. More... | |
| float | LTC2944_code_to_coulombs (uint16_t adc_code, float resistor, uint16_t prescalar) |
| Calculate the LTC2944 charge in Coulombs. More... | |
| float | LTC2944_code_to_mAh (uint16_t adc_code, float resistor, uint16_t prescalar) |
| Calculate the LTC2944 charge in mAh. More... | |
| float | LTC2944_code_to_voltage (uint16_t adc_code) |
| Calculate the LTC2944 SENSE+ voltage. More... | |
| float | LTC2944_code_to_current (uint16_t adc_code, float resistor) |
| Calculate the LTC2944 current with a sense resistor. More... | |
| float | LTC2944_code_to_kelvin_temperature (uint16_t adc_code) |
| Calculate the LTC2944 temperature. More... | |
| float | LTC2944_code_to_celcius_temperature (uint16_t adc_code) |
| Calculate the LTC2944 temperature. More... | |
| int8_t | LTC2944_register_set_clear_bits (uint8_t i2c_address, uint8_t register_address, uint8_t bits_to_set, uint8_t bits_to_clear) |
| float LTC2944_code_to_celcius_temperature | ( | uint16_t | adc_code | ) |
Calculate the LTC2944 temperature.
| adc_code | The RAW ADC value |
Definition at line 161 of file LTC2944.cpp.
| float LTC2944_code_to_coulombs | ( | uint16_t | adc_code, |
| float | resistor, | ||
| uint16_t | prescalar | ||
| ) |
Calculate the LTC2944 charge in Coulombs.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
| prescalar | The prescalar value |
Definition at line 120 of file LTC2944.cpp.
| float LTC2944_code_to_current | ( | uint16_t | adc_code, |
| float | resistor | ||
| ) |
Calculate the LTC2944 current with a sense resistor.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
Definition at line 145 of file LTC2944.cpp.
| float LTC2944_code_to_kelvin_temperature | ( | uint16_t | adc_code | ) |
Calculate the LTC2944 temperature.
| adc_code | The RAW ADC value |
Definition at line 153 of file LTC2944.cpp.
| float LTC2944_code_to_mAh | ( | uint16_t | adc_code, |
| float | resistor, | ||
| uint16_t | prescalar | ||
| ) |
Calculate the LTC2944 charge in mAh.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
| prescalar | The prescalar value |
Definition at line 129 of file LTC2944.cpp.
| float LTC2944_code_to_voltage | ( | uint16_t | adc_code | ) |
Calculate the LTC2944 SENSE+ voltage.
| adc_code | The RAW ADC value |
Definition at line 137 of file LTC2944.cpp.
| int8_t LTC2944_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t * | adc_code | ||
| ) |
Reads an 8-bit adc_code from LTC2944.
| i2c_address | Register address for the LTC2944 |
| adc_command | The "command byte" for the LTC2944 |
| adc_code | Value that will be read from the register. |
Definition at line 98 of file LTC2944.cpp.
| int8_t LTC2944_read_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 16-bit adc_code from LTC2944.
| i2c_address | Register address for the LTC2944 |
| adc_command | The "command byte" for the LTC2944 |
| adc_code | Value that will be read from the register. |
Definition at line 109 of file LTC2944.cpp.
| int8_t LTC2944_register_set_clear_bits | ( | uint8_t | i2c_address, |
| uint8_t | register_address, | ||
| uint8_t | bits_to_set, | ||
| uint8_t | bits_to_clear | ||
| ) |
Definition at line 171 of file LTC2944.cpp.
| int8_t LTC2944_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC2944.
| i2c_address | Register address for the LTC2944 |
| adc_command | The "command byte" for the LTC2944 |
| code | Value that will be written to the register. |
Definition at line 77 of file LTC2944.cpp.
| int8_t LTC2944_write_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t | code | ||
| ) |
Write a 16-bit code to the LTC2944.
| i2c_address | Register address for the LTC2944 |
| adc_command | The "command byte" for the LTC2944 |
| code | Value that will be written to the register. |
Definition at line 88 of file LTC2944.cpp.