![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2942: Battery Gas Gauge with Temperature, Voltage Measurement. More...
LTC2942: Battery Gas Gauge with Temperature, Voltage Measurement.
LTC2941: Battery Gas Gauge with I2C Interface.
The LTC®2942 measures battery charge state, battery
voltage and chip temperature in handheld PC and portable
product applications. Its operating range is perfectly suited
for single-cell Li-Ion batteries. A precision coulomb counter
integrates current through a sense resistor between the
battery’s positive terminal and the load or charger. Battery
voltage and on-chip temperature are measured with an
internal 14-bit No Latency ∆∑™ ADC. The three measured
quantities (charge, voltage and temperature) are stored in
internal registers accessible via the onboard SMBus/I2C
interface.
I2C DATA FORMAT (MSB FIRST):
Data Out:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C7 C6 C5 C4 C3 C2 C1 C0 SACK D7 D6 D5 D4 D3 D2 D1 D0 SACK STOP
Data In:
Byte #1 Byte #2 Byte #3
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C7 C6 C5 C4 C3 C2 C1 C0 SACK Repeat Start SA6 SA5 SA4 SA3 SA2 SA1 SA0 R SACK
Byte #4 Byte #5
MSB LSB
D15 D14 D13 D12 D11 D10 D9 D8 MACK D7 D6 D5 D4 D3 D2 D1 D0 MNACK STOP
START : I2C Start
Repeat Start: I2c Repeat Start
STOP : I2C Stop
SAx : I2C Address
SACK : I2C Slave Generated Acknowledge (Active Low)
MACK : I2C Master Generated Acknowledge (Active Low)
MNACK : I2c Master Generated Not Acknowledge
W : I2C Write (0)
R : I2C Read (1)
Cx : Command Code
Dx : Data Bits
X : Don't care
Example Code:
Read charge, current, and voltage.
adc_command = LTC2942_SENSE_MONITOR | LTC2942_AUTOMATIC_MODE; // Builds commands to set LTC2942 to automatic mode
ack |= LTC2942_write(LTC2942_I2C_ADDRESS, LTC2942_CONTROL_REG, adc_command); // Sets the LTC2942 to automatic mode
resistor = .1; // Resistor Value On Demo Board
ack |= LTC2942_read_16_bits(LTC2942_I2C_ADDRESS, LTC2942_CHARGE_MSB_REG, &charge_code); // Reads the ADC registers that contains charge value
charge = LTC2942_code_to_coulombs(charge_code, resistor, prescalarValue); // Calculates charge from charge code, resistor and prescalar
ack |= LTC2942_read_16_bits(LTC2942_I2C_ADDRESS, LTC2942_CURRENT_MSB_REG, ¤t_code); // Reads the voltage code across sense resistor
current = LTC2942_code_to_current(current_code, resistor); // Calculates current from current code, resistor value.
ack |= LTC2942_read_16_bits(LTC2942_I2C_ADDRESS, LTC2942_VOLTAGE_MSB_REG, &voltage_code); // Reads voltage voltage code
VIN = LTC2942_VIN_code_to_voltage(voltage_code); // Calculates VIN voltage from VIN code and lsbhttp://www.linear.com/product/LTC2942 http://www.linear.com/product/LTC2941
http://www.linear.com/product/LTC2942#demoboards http://www.linear.com/product/LTC2941#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2942: Battery Gas Gauge with Temperature, Voltage Measurement
Definition in file LTC2942.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2942_write (uint8_t i2c_address, uint8_t adc_command, uint8_t code) |
| Write an 8-bit code to the LTC2942. More... | |
| int8_t | LTC2942_write_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t code) |
| Write a 16-bit code to the LTC2942. More... | |
| int8_t | LTC2942_read (uint8_t i2c_address, uint8_t adc_command, uint8_t *adc_code) |
| Reads an 8-bit adc_code from LTC2942. More... | |
| int8_t | LTC2942_read_16_bits (uint8_t i2c_address, uint8_t adc_command, uint16_t *adc_code) |
| Reads a 16-bit adc_code from LTC2942. More... | |
| float | LTC2942_code_to_coulombs (uint16_t adc_code, float resistor, uint16_t prescalar) |
| Calculate the LTC2942 charge in Coulombs. More... | |
| float | LTC2942_code_to_mAh (uint16_t adc_code, float resistor, uint16_t prescalar) |
| Calculate the LTC2942 charge in mAh. More... | |
| float | LTC2942_code_to_voltage (uint16_t adc_code) |
| Calculate the LTC2942 SENSE+ voltage. More... | |
| float | LTC2942_code_to_kelvin_temperature (uint16_t adc_code) |
| Calculate the LTC2942 temperature. More... | |
| float | LTC2942_code_to_celcius_temperature (uint16_t adc_code) |
| Calculate the LTC2942 temperature. More... | |
Macros | |||||||||||||||||||||||||||||||||||
LTC2942 I2C Address | |||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||
| #define | LTC2942_I2C_ADDRESS 0x64 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_I2C_ALERT_RESPONSE 0x0C | ||||||||||||||||||||||||||||||||||
Registers | |||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||
| #define | LTC2942_STATUS_REG 0x00 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_CONTROL_REG 0x01 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_ACCUM_CHARGE_MSB_REG 0x02 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_ACCUM_CHARGE_LSB_REG 0x03 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_CHARGE_THRESH_HIGH_MSB_REG 0x04 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_CHARGE_THRESH_HIGH_LSB_REG 0x05 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_CHARGE_THRESH_LOW_MSB_REG 0x06 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_CHARGE_THRESH_LOW_LSB_REG 0x07 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_VOLTAGE_MSB_REG 0x08 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_VOLTAGE_LSB_REG 0x09 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_VOLTAGE_THRESH_HIGH_REG 0x0A | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_VOLTAGE_THRESH_LOW_REG 0x0B | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_TEMPERATURE_MSB_REG 0x0C | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_TEMPERATURE_LSB_REG 0x0D | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_TEMPERATURE_THRESH_HIGH_REG 0x0E | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_TEMPERATURE_THRESH_LOW_REG 0x0F | ||||||||||||||||||||||||||||||||||
Command Codes | |||||||||||||||||||||||||||||||||||
| |||||||||||||||||||||||||||||||||||
| #define | LTC2942_AUTOMATIC_MODE 0xC0 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_MANUAL_VOLTAGE 0x80 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_MANUAL_TEMPERATURE 0x40 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_SLEEP_MODE 0x00 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_PRESCALAR_M_1 0x00 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_PRESCALAR_M_2 0x08 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_PRESCALAR_M_4 0x10 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_PRESCALAR_M_8 0x18 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_PRESCALAR_M_16 0x20 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_PRESCALAR_M_32 0x28 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_PRESCALAR_M_64 0x30 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_PRESCALAR_M_128 0x38 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_ALERT_MODE 0x04 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_CHARGE_COMPLETE_MODE 0x02 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_DISABLE_ALCC_PIN 0x00 | ||||||||||||||||||||||||||||||||||
| #define | LTC2942_SHUTDOWN_MODE 0x01 | ||||||||||||||||||||||||||||||||||
Variables | |||||||||||||
Conversion Constants | |||||||||||||
| |||||||||||||
| const float | LTC2942_CHARGE_lsb = 0.085E-3 | ||||||||||||
| const float | LTC2942_VOLTAGE_lsb = .3662E-3 | ||||||||||||
| const float | LTC2942_TEMPERATURE_lsb = 0.25 | ||||||||||||
| const float | LTC2942_FULLSCALE_VOLTAGE = 6 | ||||||||||||
| const float | LTC2942_FULLSCALE_TEMPERATURE = 600 | ||||||||||||
| float LTC2942_code_to_celcius_temperature | ( | uint16_t | adc_code | ) |
Calculate the LTC2942 temperature.
| adc_code | The RAW ADC value |
Definition at line 148 of file LTC2942.cpp.
| float LTC2942_code_to_coulombs | ( | uint16_t | adc_code, |
| float | resistor, | ||
| uint16_t | prescalar | ||
| ) |
Calculate the LTC2942 charge in Coulombs.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
| prescalar | The prescalar value |
Definition at line 114 of file LTC2942.cpp.
| float LTC2942_code_to_kelvin_temperature | ( | uint16_t | adc_code | ) |
Calculate the LTC2942 temperature.
| adc_code | The RAW ADC value |
Definition at line 140 of file LTC2942.cpp.
| float LTC2942_code_to_mAh | ( | uint16_t | adc_code, |
| float | resistor, | ||
| uint16_t | prescalar | ||
| ) |
Calculate the LTC2942 charge in mAh.
| adc_code | The RAW ADC value |
| resistor | The sense resistor value |
| prescalar | The prescalar value |
Definition at line 123 of file LTC2942.cpp.
| float LTC2942_code_to_voltage | ( | uint16_t | adc_code | ) |
Calculate the LTC2942 SENSE+ voltage.
| adc_code | The RAW ADC value |
Definition at line 131 of file LTC2942.cpp.
| int8_t LTC2942_read | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t * | adc_code | ||
| ) |
Reads an 8-bit adc_code from LTC2942.
| i2c_address | Register address for the LTC2942 |
| adc_command | The "command byte" for the LTC2942 |
| adc_code | Value that will be read from the register. |
Definition at line 92 of file LTC2942.cpp.
| int8_t LTC2942_read_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t * | adc_code | ||
| ) |
Reads a 16-bit adc_code from LTC2942.
| i2c_address | Register address for the LTC2942 |
| adc_command | The "command byte" for the LTC2942 |
| adc_code | Value that will be read from the register. |
Definition at line 103 of file LTC2942.cpp.
| int8_t LTC2942_write | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint8_t | code | ||
| ) |
Write an 8-bit code to the LTC2942.
| i2c_address | Register address for the LTC2942 |
| adc_command | The "command byte" for the LTC2942 |
| code | Value that will be written to the register. |
Definition at line 71 of file LTC2942.cpp.
| int8_t LTC2942_write_16_bits | ( | uint8_t | i2c_address, |
| uint8_t | adc_command, | ||
| uint16_t | code | ||
| ) |
Write a 16-bit code to the LTC2942.
| i2c_address | Register address for the LTC2942 |
| adc_command | The "command byte" for the LTC2942 |
| code | Value that will be written to the register. |
Definition at line 82 of file LTC2942.cpp.