![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2607: 16-Bit, Dual Rail-to-Rail DACs with I2C Interface. More...
LTC2607: 16-Bit, Dual Rail-to-Rail DACs with I2C Interface.
LTC2609: Quad 16-/14-/12-Bit Rail-to-Rail DACs with I²C Interface. LTC2606: 16-Bit Rail-to-Rail DACs with I²C Interface.
The LTC2607/LTC2617/LTC2627 are dual 16-, 14- and 12-bit, 2.7V to 5.5V
rail-to-rail voltage output DACs in a 12-lead DFN package. They have built-in
high performance output buffers and are guaranteed monotonic.
These parts establish new board-density benchmarks for 16- and 14-bit DACs and
advance performance standards for output drive and load regulation in single-
supply, voltage-output DACs.
The parts use a 2-wire, I2C compatible serial interface. The
LTC2607/LTC2617/LTC2627 operate in both the standard mode (clock rate of 100kHz)
and the fast mode (clock rate of 400kHz). An asynchronous DAC update pin (LDAC)
is also included.
The LTC2607/LTC2617/LTC2627 incorporate a power-on reset circuit. During power-
up, the voltage outputs rise less than 10mV above zero scale; and after power-
up, they stay at zero scale until a valid write and update take place. The
power-on reset circuit resets the LTC2607-1/LTC2617-1/ LTC2627-1 to mid-scale.
The voltage outputs stay at midscale until a valid write and update takes place.
I2C DATA FORMAT (MSB First):
Byte #1 Byte #2 Byte #3 Byte #4
START SA6 SA5 SA4 SA3 SA2 SA1 SA0 W SACK C3 C2 C1 C0 A3 A2 A1 A0 SACK D15 D14 D13 D12 D11 D10 D9 D8 SACK D7 D6 D5 D4 D3 D2 D1 D0 SACK STOP
SACK : Slave Acknowlege
SAx : I2C Address
W : I2C Write (0)
R : I2C Read (1)
SACK : I2C Slave Generated Acknowledge (Active Low)
Cx : DAC Command Code
Ax : DAC Address
Dx : DAC Data Bits
X : Don't care
Example Code:
Set DAC A to Full Scale.
dac_code = 0x0FFFF; // Set dac code to full scale
// Write dac code to the LTC2607 and update dac
ack = LTC2607_write(LTC2607_I2C_GLOBAL_ADDRESS, LTC2607_WRITE_UPDATE_COMMAND, LTC2607_DAC_A, dac_code);http://www.linear.com/product/LTC2607 http://www.linear.com/product/LTC2609 http://www.linear.com/product/LTC2606
http://www.linear.com/product/LTC2607#demoboards http://www.linear.com/product/LTC2609#demoboards http://www.linear.com/product/LTC2606#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header File for LTC2607: 16-Bit, Dual Rail-to-Rail DACs with I2C Interface
Definition in file LTC2607.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2607_write (uint8_t i2c_address, uint8_t dac_command, uint8_t dac_address, uint16_t dac_code) |
| Writes command, DAC address, and DAC code to the LTC2607. More... | |
| uint16_t | LTC2607_voltage_to_code (float dac_voltage, float LTC2607_lsb, int32_t LTC2607_offset) |
| Calculates an LTC2607 DAC code for the desired output voltage. More... | |
| void | LTC2607_calibrate (uint16_t dac_code1, uint16_t dac_code2, float voltage1, float voltage2, float *LTC2607_lsb, int32_t *LTC2607_offset) |
| Calculates the LTC2607 offset and lsb voltage given two measured voltages and their corresponding DAC codes. More... | |
Macros | |
I2C_Addresses | |
| #define | LTC2607_I2C_ADDRESS 0x10 |
| I2C address of the LTC2607. More... | |
| #define | LTC2607_I2C_GLOBAL_ADDRESS 0x73 |
| LTC2607 Global I2C Address. More... | |
DAC Command | |
| #define | LTC2607_WRITE_COMMAND 0x00 |
| Command to write to internal register of LTC2607, but not update output voltage yet. More... | |
| #define | LTC2607_UPDATE_COMMAND 0x10 |
| Command to update (and power up) LTC2607. More... | |
| #define | LTC2607_WRITE_UPDATE_COMMAND 0x30 |
| Command to write and update (and power up) the LTC2607. More... | |
| #define | LTC2607_POWER_DOWN_COMMAND 0x40 |
| Command to power down the LTC2607. More... | |
DAC Address | |
| #define | LTC2607_DAC_A 0x00 |
| Command (and DAC code) will modify DAC A. More... | |
| #define | LTC2607_DAC_B 0x01 |
| Command (and DAC code) will modify DAC B. More... | |
| #define | LTC2607_ALL_DACS 0x0F |
| Command (and DAC code) will modify both DAC A and DAC B. More... | |
Variables | |
| const float | LTC2607_TYPICAL_lsb = 7.6295109E-5 |
| The LTC2607 typical least significant bit value with 5V full-scale. More... | |
| const float | LTC2607_TYPICAL_OFFSET = 0 |
| The LTC2607 typical offset voltage. More... | |
| void LTC2607_calibrate | ( | uint16_t | dac_code1, |
| uint16_t | dac_code2, | ||
| float | voltage1, | ||
| float | voltage2, | ||
| float * | LTC2607_lsb, | ||
| int32_t * | LTC2607_offset | ||
| ) |
Calculates the LTC2607 offset and lsb voltage given two measured voltages and their corresponding DAC codes.
Prior to calling this function, write two DAC codes to the LTC2607, and measure the output voltage for each DAC code. When passed the DAC codes and measured voltages as parameters, this function calculates the calibrated lsb and offset values.
| dac_code1 | DAC Code 1. |
| dac_code2 | DAC Code 2. |
| voltage1 | Measured output voltage corresponding to DAC Code 1. |
| voltage2 | Measured output voltage corresponding to DAC Code 2. |
| LTC2607_lsb | Overwritten with new calculated lsb voltage. |
| LTC2607_offset | Overwritten with new calculated offset voltage. |
Definition at line 127 of file LTC2607.cpp.
| uint16_t LTC2607_voltage_to_code | ( | float | dac_voltage, |
| float | LTC2607_lsb, | ||
| int32_t | LTC2607_offset | ||
| ) |
Calculates an LTC2607 DAC code for the desired output voltage.
Based on the desired output voltage, the offset, and lsb parameters, return the corresponding DAC code that should be written to the LTC2607.
| dac_voltage | Desired DAC output voltage. |
| LTC2607_lsb | The LSB weight. Use calibrated value for best results, otherwise use typical value from datasheet. |
| LTC2607_offset | The offset voltage. Use calibrated value for best results, otherwise use typical value from datasheet. |
Definition at line 110 of file LTC2607.cpp.
| int8_t LTC2607_write | ( | uint8_t | i2c_address, |
| uint8_t | dac_command, | ||
| uint8_t | dac_address, | ||
| uint16_t | dac_code | ||
| ) |
Writes command, DAC address, and DAC code to the LTC2607.
Configures command (write, update, power down, etc.), address (DAC A, DAC B, or BOTH), and 16-bit dac_code for output voltage.
| i2c_address | I2C address of the LTC2607. Configured by CA0, CA1, and CA2 pins. See Table 1 of datasheet. |
| dac_command | DAC command (4-bits) that will be written to LTC2607. (Write, update, power down, etc.) |
| dac_address | DAC address (4-bits) that will be written to LTC2607. Configures DAC A, DAC B, or both. |
| dac_code | DAC code that will be written to LTC2607. This configures the output voltage. |
Definition at line 100 of file LTC2607.cpp.
| #define LTC2607_ALL_DACS 0x0F |
| #define LTC2607_DAC_A 0x00 |
| #define LTC2607_DAC_B 0x01 |
| #define LTC2607_I2C_ADDRESS 0x10 |
| #define LTC2607_I2C_GLOBAL_ADDRESS 0x73 |
| #define LTC2607_POWER_DOWN_COMMAND 0x40 |
| #define LTC2607_UPDATE_COMMAND 0x10 |
| #define LTC2607_WRITE_COMMAND 0x00 |
| #define LTC2607_WRITE_UPDATE_COMMAND 0x30 |
| const float LTC2607_TYPICAL_lsb = 7.6295109E-5 |