![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC2460: 24-Bit, 16-Channel Delta Sigma ADCs with Selectable Speed/Resolution. More...
Library for LTC2460: 24-Bit, 16-Channel Delta Sigma ADCs with Selectable Speed/Resolution.
Definition in file LTC2460.cpp.
Go to the source code of this file.
Functions | |
| void | LTC2460_read (uint8_t cs, uint8_t adc_command, int32_t *adc_code) |
| float | LTC2460_code_to_voltage (int32_t adc_code, float vref) |
| Calculates the voltage corresponding to an adc code, given the reference (in volts) More... | |
| float LTC2460_code_to_voltage | ( | int32_t | adc_code, |
| float | vref | ||
| ) |
Calculates the voltage corresponding to an adc code, given the reference (in volts)
| adc_code | Code read from adc |
| vref | VRef (in volts) |
Definition at line 86 of file LTC2460.cpp.
| void LTC2460_read | ( | uint8_t | cs, |
| uint8_t | adc_command, | ||
| int32_t * | adc_code | ||
| ) |
Reads from LTC2460.
| cs | Chip select |
| adc_command | 1 byte command written to LTC2460 |
| adc_code | 4 byte conversion code read from LTC2460 |
Definition at line 77 of file LTC2460.cpp.