![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2449: 24-Bit, 16-Channel Delta Sigma ADCs with Selectable Speed/Resolution. More...
LTC2449: 24-Bit, 16-Channel Delta Sigma ADCs with Selectable Speed/Resolution.
LTC2442: 24-Bit, 4-Channel Delta Sigma ADC with Integrated Amplifier LTC2448: 24-Bit, 8-/16-Channel Delta Sigma ADCs with Selectable Speed/Resolution
The LTC2444/LTC2445/LTC2448/LTC2449 are 8-/16-channel (4-/8-differential)
high speed 24-bit No Latency Delta Sigma ADCs. They use a proprietary
delta-sigma architecture enabling variable speed/resolution. Through a
simple 4-wire serial interface, ten speed/resolution combinations
6.9Hz/280nVRMS to 3.5kHz/25uVRMS (4kHz with external oscillator) can be
selected with no latency between conversion results or shift in DC accuracy
(offset, full-scale, linearity, drift). Additionally, a 2X speed mode can
be selected enabling output rates up to 7kHz (8kHz if an external
oscillator is used) with one cycle latency.
SPI DATA FORMAT (MSB First):
Byte #1 Byte #2
Data Out : !EOC DMY SIG D28 D27 D26 D25 D24 D23 D22 D21 D20 D19 D18 D17 D16
Data In : 1 0 EN SGL OS S2 S1 S0 OSR3 OSR2 OSR1 OSR1 SPD X X X
Byte #3 Byte #4
D15 D14 D13 D12 D11 D10 D9 D8 D7 D6 D5 D4 *D3 *D2 *D1 *D0
X X X X X X X X X X X X X X X X
!EOC : End of Conversion Bit (Active Low)
DMY : Dummy Bit (Always 0)
SIG : Sign Bit (1-data positive, 0-data negative)
Dx : Data Bits
*Dx : Data Bits Below lsb
EN : Enable Bit (0-keep previous mode, 1-change mode)
SGL : Enable Single-Ended Bit (0-differential, 1-single-ended)
OS : ODD/Sign Bit
Sx : Address Select Bit
0SRX : Over Sampling Rate Bits
SPD : Double Output Rate Select Bit (0-Normal rate, auto-calibration on, 2x rate, auto_calibration off)
Command Byte #1
1 0 EN SGL OS S2 S1 S0 Comments
1 0 0 X X X X X Keep Previous Mode
1 0 1 0 X X X X Differential Mode
1 0 1 1 X X X X Single-Ended Mode
| Coversion Rate | RMS | ENOB | OSR | Latency
Command Byte #2 |Internal | External | Noise | | |
| 9MHz | 10.24MHz | | | |
OSR3 OSR2 OSR1 OSR1 SPD | Clock | Clock | | | |
0 0 0 0 0 Keep Previous Speed/Resolution
0 0 0 1 0 3.52kHz 4kHz 23uV 17 64 none
0 0 1 0 0 1.76kHz 2kHz 3.5uV 20.1 128 none
0 0 1 1 0 880Hz 1kHz 2uV 21.3 256 none
0 1 0 0 0 440Hz 500Hz 1.4uV 21.8 512 none
0 1 0 1 0 220Hz 250Hz 1uV 22.4 1024 none
0 1 1 0 0 110Hz 125Hz 750nV 22.9 2048 none
0 1 1 1 0 55Hz 62.5Hz 510nV 23.4 4096 none
1 0 0 0 0 27.5Hz 31.25Hz 375nV 24 8192 none
1 0 0 1 0 13.75Hz 15.625Hz 250nV 24.4 16384 none
1 1 1 1 0 6.87kHz 7.8125Hz 200nV 24.6 32768 none
0 0 0 0 1 Keep Previous Speed/Resolution
OSR3 OSR2 OSR1 OSR1 1 2X Mode *all clock speeds double
Example Code:
Read Channel 0 in Single-Ended with OSR of 65536
uint16_t miso_timeout = 1000;
adc_command = LTC2449_CH0 | LTC2449_OSR_32768 | LTC2449_SPEED_2X; // Build ADC command for channel 0
// OSR = 32768*2 = 65536
if(LTC2449_EOC_timeout(LTC2449_CS, miso_timeout)) // Check for EOC
return; // Exit if timeout is reached
LTC2449_read(LTC2449_CS, adc_command, &adc_code); // Throws out last reading
if(LTC2449_EOC_timeout(LTC2449_CS, miso_timeout)) // Check for EOC
return; // Exit if timeout is reached
LTC2449_read(LTC2449_CS, adc_command, &adc_code); // Obtains the current reading and stores to adc_code variable
// Convert adc_code to voltage
adc_voltage = LTC2449_code_to_voltage(adc_code, LTC2449_lsb, LTC2449_offset_code);http://www.linear.com/product/LTC2449 http://www.linear.com/product/LTC2442 http://www.linear.com/product/LTC2448
http://www.linear.com/product/LTC2449#demoboards http://www.linear.com/product/LTC2442#demoboards http://www.linear.com/product/LTC2448#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Header for LTC2449: 24-Bit, 16-Channel Delta Sigma ADCs with Selectable Speed/Resolution
Definition in file LTC2449.h.
Go to the source code of this file.
Functions | |
| int8_t | LTC2449_EOC_timeout (uint8_t cs, uint16_t miso_timeout) |
| Checks for EOC with a specified timeout. More... | |
| void | LTC2449_read (uint8_t cs, uint16_t adc_command, uint32_t *adc_code) |
| Reads from LTC2449. More... | |
| float | LTC2449_code_to_voltage (int32_t adc_code, float LTC2449_lsb, int32_t LTC2449_offset_code) |
| Calculates the voltage corresponding to an adc code, given lsb weight (in volts) and the calibrated ADC offset code (zero code that is subtracted from adc_code). More... | |
| void | LTC2449_cal_voltage (int32_t zero_code, int32_t fs_code, float zero_voltage, float fs_voltage, float *LTC2449_lsb, int32_t *LTC2449_offset_code) |
| Calculate the lsb weight and offset code given a full-scale code and a measured zero-code. More... | |
Macros | |
| #define | LTC2449_CS QUIKEVAL_CS |
| Define the SPI CS pin. More... | |
Mode Configuration | |
| #define | LTC2449_KEEP_PREVIOUS_MODE 0x8000 |
| #define | LTC2449_KEEP_PREVIOUS_SPEED_RESOLUTION 0x0000 |
| #define | LTC2449_SPEED_1X 0x0000 |
| #define | LTC2449_SPEED_2X 0x0008 |
Single-Ended Channels Configuration | |
| #define | LTC2449_CH0 0xB000 |
| #define | LTC2449_CH1 0xB800 |
| #define | LTC2449_CH2 0xB100 |
| #define | LTC2449_CH3 0xB900 |
| #define | LTC2449_CH4 0xB200 |
| #define | LTC2449_CH5 0xBA00 |
| #define | LTC2449_CH6 0xB300 |
| #define | LTC2449_CH7 0xBB00 |
| #define | LTC2449_CH8 0xB400 |
| #define | LTC2449_CH9 0xBC00 |
| #define | LTC2449_CH10 0xB500 |
| #define | LTC2449_CH11 0xBD00 |
| #define | LTC2449_CH12 0xB600 |
| #define | LTC2449_CH13 0xBE00 |
| #define | LTC2449_CH14 0xB700 |
| #define | LTC2449_CH15 0xBF00 |
Differential Channel Configuration | |
| #define | LTC2449_P0_N1 0xA000 |
| #define | LTC2449_P1_N0 0xA800 |
| #define | LTC2449_P2_N3 0xA100 |
| #define | LTC2449_P3_N2 0xA900 |
| #define | LTC2449_P4_N5 0xA200 |
| #define | LTC2449_P5_N4 0xAA00 |
| #define | LTC2449_P6_N7 0xA300 |
| #define | LTC2449_P7_N6 0xAB00 |
| #define | LTC2449_P8_N9 0xA400 |
| #define | LTC2449_P9_N8 0xAC00 |
| #define | LTC2449_P10_N11 0xA500 |
| #define | LTC2449_P11_N10 0xAD00 |
| #define | LTC2449_P12_N13 0xA600 |
| #define | LTC2449_P13_N12 0xAE00 |
| #define | LTC2449_P14_N15 0xA700 |
| #define | LTC2449_P15_N14 0xAF00 |
Oversample Ratio (OSR) Commands | |
| #define | LTC2449_OSR_64 0xA010 |
| #define | LTC2449_OSR_128 0xA020 |
| #define | LTC2449_OSR_256 0xA030 |
| #define | LTC2449_OSR_512 0xA040 |
| #define | LTC2449_OSR_1024 0xA050 |
| #define | LTC2449_OSR_2048 0xA060 |
| #define | LTC2449_OSR_4096 0xA070 |
| #define | LTC2449_OSR_8192 0xA080 |
| #define | LTC2449_OSR_16384 0xA090 |
| #define | LTC2449_OSR_32768 0xA0F0 |
| void LTC2449_cal_voltage | ( | int32_t | zero_code, |
| int32_t | fs_code, | ||
| float | zero_voltage, | ||
| float | fs_voltage, | ||
| float * | LTC2449_lsb, | ||
| int32_t * | LTC2449_offset_code | ||
| ) |
Calculate the lsb weight and offset code given a full-scale code and a measured zero-code.
| zero_code | Measured code with the inputs shorted to ground |
| fs_code | Measured code at nearly full-scale |
| zero_voltage | Measured zero voltage |
| fs_voltage | Voltage measured at input (with voltmeter) when fs_code was read from adc |
| LTC2449_lsb | Overwritten with lsb weight (in volts) |
| LTC2449_offset_code | Overwritten with offset code (zero code) |
Definition at line 136 of file LTC2449.cpp.
| float LTC2449_code_to_voltage | ( | int32_t | adc_code, |
| float | LTC2449_lsb, | ||
| int32_t | LTC2449_offset_code | ||
| ) |
Calculates the voltage corresponding to an adc code, given lsb weight (in volts) and the calibrated ADC offset code (zero code that is subtracted from adc_code).
| adc_code | Code read from adc |
| LTC2449_lsb | LSB weight (in volts) |
| LTC2449_offset_code | The calibrated offset code (This is the adc code zero code that will be subtraced from adc_code) |
Definition at line 127 of file LTC2449.cpp.
| int8_t LTC2449_EOC_timeout | ( | uint8_t | cs, |
| uint16_t | miso_timeout | ||
| ) |
Checks for EOC with a specified timeout.
Checks for EOC with a specified timeout.
| cs | Chip Select pin |
| miso_timeout | Timeout (in milliseconds) |
Definition at line 86 of file LTC2449.cpp.
| void LTC2449_read | ( | uint8_t | cs, |
| uint16_t | adc_command, | ||
| uint32_t * | adc_code | ||
| ) |
Reads from LTC2449.
| cs | Chip Select pin |
| adc_command | 2 byte command written to LTC2449 |
| adc_code | 4 byte conversion code read from LTC2449 |
Definition at line 107 of file LTC2449.cpp.
| #define LTC2449_CS QUIKEVAL_CS |