![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC2422: 1-/2-Channel 20-Bit uPower No Latency Delta-Sigma ADC in MSOP-10. More...
LTC2422: 1-/2-Channel 20-Bit uPower No Latency Delta-Sigma ADC in MSOP-10.
The LTC2421/LTC2422 are 1- and 2-channel 2.7V to 5.5V micropower 20-bit analog-
to-digital converters with an integrated oscillator, 8ppm INL and 1.2ppm RMS
noise. These ultrasmall devices use delta-sigma technology and a new digital
filter architecture that settles in a single cycle. This eliminates the latency
found in conventional delta-sigma converters and simplifies multiplexed
applications. Through a single pin, the LTC2421/LTC2422 can be configured for
better than 110dB rejection at 50Hz or 60Hz +/-2%, or can be driven by an
external oscillator for a user defined rejection frequency in the range 1Hz to
120Hz. The internal oscillator requires no external frequency setting
components.
SPI DATA FORMAT (MSB First):
Byte #1 Byte #2
Data Out : !EOC CH SIG EXR D19 D18 D17 D16 D15 D14 D13 D12 D11 D10 D9 D8
Data In : X X X X X X X X X X X X X X X X
Byte #3
D7 D6 D5 D4 D3 D2 D1 D0
X X X X X X X X
!EOC : End of Conversion Bit (Active Low)
CH : Channel Indicator Bit (0 - CH0 , 1 - CH1)
SIG : Sign Bit (1-data positive, 0-data negative)
EXR : Extebded Input Range Indicator Bit
Dx : Data Bits
Example Code:
Read Channel 0.
uint16_t miso_timeout = 1000;
if(LTC2422_EOC_timeout(LTC2422_CS, miso_timeout)) // Check for EOC
return; // Handle exception if timeout exceeded without EOC
LTC2422_adc_read(LTC2422_CS, &adc_channel, &adc_code); // Read ADC
if(adc_channel != 0)
{
if(LTC2422_EOC_timeout(LTC2422_CS, miso_timeout)) // Check for EOC
return; // Handle exception if timeout exceeded without EOC
LTC2422_adc_read(LTC2422_CS, &adc_channel, &adc_code); // Reads the ADC again if the first reading was not CH0
}
adc_voltage = LTC2422_code_to_voltage(adc_code, LTC2422_lsb);http://www.linear.com/product/LTC2422
http://www.linear.com/product/LTC2422#demoboard
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Library Header File for LTC2422: 1-/2-Channel 20-Bit uPower No Latency Delta-Sigma ADC in MSOP-10
Definition in file LTC2422.h.
Go to the source code of this file.
Functions | |
| uint8_t | LTC2422_EOC_timeout (uint8_t cs, uint16_t miso_timeout) |
| Checks for EOC with a specified timeout. More... | |
| void | LTC2422_adc_read (uint8_t cs, uint8_t *adc_channel, int32_t *code) |
| Read ADC code from the LTC2422. More... | |
| float | LTC2422_code_to_voltage (int32_t adc_code, float LTC2422_lsb) |
| Calculates the voltage given the ADC code and lsb weight. More... | |
| void | LTC2422_calculate_lsb (float LTC2422_reference_voltage, float *LTC2422_lsb) |
| Calculates the lsb weight from the given reference voltage. More... | |
Macros | |
| #define | LTC2422_CS QUIKEVAL_CS |
| Define the SPI CS pin. More... | |
Variables | |
| const float | LTC2422_TYPICAL_lsb = 4.7683761E-6 |
| The LTC2422 typical least significant bit value with 5V full-scale. More... | |
| void LTC2422_adc_read | ( | uint8_t | cs, |
| uint8_t * | adc_channel, | ||
| int32_t * | code | ||
| ) |
Read ADC code from the LTC2422.
Does not wait for end-of-conversion. To automatically wait for conversion to complete, use the LTC2422_EOC_timeout before this function.
| cs | Chip Select pin |
| adc_channel | Returns channel number read. |
| code | Returns the ADC code read. |
Definition at line 98 of file LTC2422.cpp.
| void LTC2422_calculate_lsb | ( | float | LTC2422_reference_voltage, |
| float * | LTC2422_lsb | ||
| ) |
Calculates the lsb weight from the given reference voltage.
| LTC2422_reference_voltage | Measured reference voltage. |
| LTC2422_lsb | Overwritten with the lsb weight in volts. |
Definition at line 128 of file LTC2422.cpp.
| float LTC2422_code_to_voltage | ( | int32_t | adc_code, |
| float | LTC2422_lsb | ||
| ) |
Calculates the voltage given the ADC code and lsb weight.
| adc_code | ADC code read from LTC2422. |
| LTC2422_lsb | LSB weight (determined by reference voltage). |
Definition at line 119 of file LTC2422.cpp.
| uint8_t LTC2422_EOC_timeout | ( | uint8_t | cs, |
| uint16_t | miso_timeout | ||
| ) |
Checks for EOC with a specified timeout.
| cs | Chip Select pin |
| miso_timeout | Timeout (ms) |
Definition at line 76 of file LTC2422.cpp.
| #define LTC2422_CS QUIKEVAL_CS |