![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC2418: 16-Channel 24-Bit No Latency Delta-Sigma ADC. More...
Library for LTC2418: 16-Channel 24-Bit No Latency Delta-Sigma ADC.
Definition in file LTC2418.cpp.
Go to the source code of this file.
Functions | |
| int8_t | LTC2418_EOC_timeout (uint8_t cs, uint16_t miso_timeout) |
| Checks for EOC with a specified timeout. More... | |
| void | LTC2418_read (uint8_t cs, uint8_t adc_command, uint32_t *adc_code) |
| Reads the LTC2418 result and programs the configuration for the next conversion. More... | |
| float | LTC2418_code_to_voltage (int32_t adc_code, float LTC2418_lsb, int32_t LTC2418_offset_code) |
| Calculates the LTC2418 input bipolar voltage. More... | |
| void | LTC2418_cal_voltage (int32_t zero_code, int32_t fs_code, float zero_voltage, float fs_voltage, float *LTC2418_lsb, int32_t *LTC2418_offset_code) |
| Calibrate the lsb. More... | |
| void LTC2418_cal_voltage | ( | int32_t | zero_code, |
| int32_t | fs_code, | ||
| float | zero_voltage, | ||
| float | fs_voltage, | ||
| float * | LTC2418_lsb, | ||
| int32_t * | LTC2418_offset_code | ||
| ) |
Calibrate the lsb.
| zero_code | Offset (Code) |
| fs_code | Code measured with full-scale input applied |
| zero_voltage | Measured zero voltage |
| fs_voltage | Measured full-scale voltage |
| LTC2418_lsb | Returns LSB value (volts) |
| LTC2418_offset_code | Returns Offset (Code) |
Definition at line 117 of file LTC2418.cpp.
| float LTC2418_code_to_voltage | ( | int32_t | adc_code, |
| float | LTC2418_lsb, | ||
| int32_t | LTC2418_offset_code | ||
| ) |
Calculates the LTC2418 input bipolar voltage.
| adc_code | Raw ADC code |
| LTC2418_lsb | LSB value (volts) |
| LTC2418_offset_code | Offset (Code) |
Definition at line 107 of file LTC2418.cpp.
| int8_t LTC2418_EOC_timeout | ( | uint8_t | cs, |
| uint16_t | miso_timeout | ||
| ) |
Checks for EOC with a specified timeout.
| cs | Chip Select pin |
| miso_timeout | Timeout (ms) |
Definition at line 73 of file LTC2418.cpp.
| void LTC2418_read | ( | uint8_t | cs, |
| uint8_t | adc_command, | ||
| uint32_t * | adc_code | ||
| ) |
Reads the LTC2418 result and programs the configuration for the next conversion.
| cs | Chip Select pin |
| adc_command | Command byte |
| adc_code | Returns raw 32-bit code read from ADC |
Definition at line 92 of file LTC2418.cpp.