![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LTC2412: 2-Channel Differential Input 24-Bit No Latency Delta Sigma ADC. More...
Library for LTC2412: 2-Channel Differential Input 24-Bit No Latency Delta Sigma ADC.
Definition in file LTC2412.cpp.
Go to the source code of this file.
Functions | |
| int8_t | LTC2412_EOC_timeout (uint8_t cs, uint16_t miso_timeout) |
| Checks for EOC with a specified timeout. More... | |
| void | LTC2412_read (uint8_t cs, uint32_t *adc_code) |
| Reads the LTC2412 result. More... | |
| float | LTC2412_code_to_voltage (int32_t adc_code, float LTC2412_lsb, int32_t LTC2412_offset_code) |
| Calculates the LTC2412 input voltage. More... | |
| float LTC2412_code_to_voltage | ( | int32_t | adc_code, |
| float | LTC2412_lsb, | ||
| int32_t | LTC2412_offset_code | ||
| ) |
Calculates the LTC2412 input voltage.
| adc_code | Raw ADC code |
| LTC2412_lsb | LSB value (volts) |
| LTC2412_offset_code | Offset (Code) |
Definition at line 113 of file LTC2412.cpp.
| int8_t LTC2412_EOC_timeout | ( | uint8_t | cs, |
| uint16_t | miso_timeout | ||
| ) |
Checks for EOC with a specified timeout.
| cs | Chip Select pin |
| miso_timeout | Timeout (ms) |
Definition at line 79 of file LTC2412.cpp.
| void LTC2412_read | ( | uint8_t | cs, |
| uint32_t * | adc_code | ||
| ) |
Reads the LTC2412 result.
| cs | Chip Select pin |
| adc_code | Returns raw 32-bit code read from ADC |
Definition at line 98 of file LTC2412.cpp.