![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Library for LT3965 Octal Matrix LED Bypass Switch. More...
Library for LT3965 Octal Matrix LED Bypass Switch.
Definition in file LT3965.cpp.
Go to the source code of this file.
Functions | |
| int8_t | i2c_acwrite (uint8_t address, uint8_t value) |
| ACMODE Write Command to write a "value" byte to device at "address". More... | |
| int8_t | i2c_acread (uint8_t address, uint8_t *values) |
| ACMODE Read Command to read 3 data bytes from device at "address". More... | |
| int8_t | i2c_scwriteshort (uint8_t address, uint8_t channel, uint8_t data_SCMREG) |
| SCMODE Write Command Short Format to write a "value" byte to device at "address". More... | |
| int8_t | i2c_scwritelong (uint8_t address, uint8_t channel, uint8_t data_SCMREG, uint8_t dimming_value) |
| SCMODE Write Command Long Format to write 2 "value" bytes to device at "address". More... | |
| int8_t | i2c_scwriteshort_scread (uint8_t address, uint8_t channel, uint8_t data_SCMREG, uint8_t *values) |
| SCMODE Write Short + SCMODE Read Command. More... | |
| int8_t | i2c_bcread (uint8_t *value) |
| BCMODE Read Command. More... | |
| int8_t i2c_acread | ( | uint8_t | address, |
| uint8_t * | values | ||
| ) |
ACMODE Read Command to read 3 data bytes from device at "address".
Definition at line 83 of file LT3965.cpp.
| int8_t i2c_acwrite | ( | uint8_t | address, |
| uint8_t | value | ||
| ) |
ACMODE Write Command to write a "value" byte to device at "address".
Definition at line 73 of file LT3965.cpp.
| int8_t i2c_bcread | ( | uint8_t * | value | ) |
BCMODE Read Command.
Definition at line 135 of file LT3965.cpp.
| int8_t i2c_scwritelong | ( | uint8_t | address, |
| uint8_t | channel, | ||
| uint8_t | data_SCMREG, | ||
| uint8_t | dimming_value | ||
| ) |
SCMODE Write Command Long Format to write 2 "value" bytes to device at "address".
Definition at line 107 of file LT3965.cpp.
| int8_t i2c_scwriteshort | ( | uint8_t | address, |
| uint8_t | channel, | ||
| uint8_t | data_SCMREG | ||
| ) |
SCMODE Write Command Short Format to write a "value" byte to device at "address".
Definition at line 93 of file LT3965.cpp.
| int8_t i2c_scwriteshort_scread | ( | uint8_t | address, |
| uint8_t | channel, | ||
| uint8_t | data_SCMREG, | ||
| uint8_t * | values | ||
| ) |
SCMODE Write Short + SCMODE Read Command.
Definition at line 121 of file LT3965.cpp.